Using the motion sensor
| A |
Current lux value. |
| B |
Current temperature. |
| C |
Current state of the device connected to the motion sensor
and the instruction to operate it.
|
| D |
Current state of the motion sensor. |
| E |
Option to create a schedule. |
| F |
Option to monitor the history of motion detection and temperature. |
| G |
Tap to add the device to the Favorite devices section in the Home screen. When you add it to your Favourites. To know more about Favourites, refer to the Managing Favourites topic in the respective System User Guide. |
| H |
Option to access the Device Details screen to update the motion sensor configuration. |