DUG_ARGUS Motion Sensor Outdoor 360_WH-03

About Quick Home Connect

Quick Home Connect is a wireless connectivity solution for Zigbee® devices without the need for a Hub or smartphone application. Quick Home Connect is your starting point for wireless home automation.
It performs functions like switching, dimming via a Zigbee® network. You can connect a Wiser Micro Module Dimmer, Wiser Micro Module Light Switch or Wiser Multiwire Micro Module LED Dimmer (hereafter referred as micro module) to the sensor.
When the motion sensor is triggered, it sends a signal to the connected micro modules. You can pair up to three micro modules with the sensor.

Supported devices

  • Wiser Micro Module LED Dimmer

  • Wiser Micro Module Light Switch

  • Wiser Multiwire Micro Module LED Dimmer

Limitations

  • You can connect maximum of 3 micro modules with 1 motion sensor via Quick Home Connect.

  • You can connect maximum of 5 motion sensors to 1 micro module via Quick Home Connect.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?