DUG_Exxact - ZB Thermostat 16 A_WH-01

About the device

The Connected Thermostat Room/Floor 16 A (hereinafter referred to as cFMT/thermostat) is mainly used for electric underfloor heating or electric radiators, but could also be used to control mains powered motorized valves or circulating pumps for water-based heating.

Thermostat features

  • Measure & control the room temperature.

  • Dot-matrix displays.

  • Boost mode for ease and comfort.

  • Child lock.

  • Valve protection.

  • Measure energy consumption.

  • Smart schedule and control through Wiser app.

Operating elements

  1. Dot-matrix display

    • Wireless connectivity LED ()

    • Heat demand LED ()

    TIP: All LED indications are explained in the LED behavior chapter.
  2. Touch buttons

    • +/–: to increase / decrease the value

    • O: function button

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?