DUG_Exxact - ZB Thermostat 16 A_WH-01

Setting the room temperature using the app

Using the Wiser Home app, you can adjust the room temperature.
To adjust the room temperature:
  1. On the Control tab, tap All devices or a room tab where the thermostat is located.
  2. To select a thermostat, tap .
  3. Use the slider control and set the room temperature for heating.
    NOTE:
    • The indicates that the room temperature is below the desired temperature (set point), so the heating is on.

    • The indicates that the room temperature is above the desired temperature (set point), so the heating is off.

    TIP: You can also adjust the set-point temperature:
    • By tapping or of the heating section on the Control tab.

    TIP: Tapping you can set the boost time and turns it off.
    IMPORTANT:
    • Once the boost time is set, the set-point temperature automatically increases by 2° C for the set boost time. After the boost time is over, the set-point temperature returns to the current scheduled event or to the previous set-point temperature.

    • Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?