DUG_Exxact - ZB Thermostat 16 A_WH-01

Resetting the device

You can manually reset the thermostat to factory settings or perform a soft reset.

To perform a Soft reset :


  • Press and hold the O touch button for more than 20 seconds.

  • The thermostat flashes Sr, indicating soft reset, and it is selected when the button is released.

  • The Sr will flash to confirm the soft rest.



NOTE: To cancel the soft reset, press and hold the O button for more than 30 seconds. This reverts the thermostat's UI back to its previous state before the touch button is pressed, with no change in a functional state.


A soft reset will:

  • Delete all Zigbee connection details.

  • Delete all cloud and account details maintained by the device to allow re-registration.

  • Revert to the default setpoint in manual control.

  • Maintain all Factory settings e.g. MAC address.

  • Retains installer configuration to ensure proper functioning after rejoining or re-registration.

To perform a Factory reset :


  • Press and hold the O touch button for more than 25 seconds until thermostat flashes Fr

  • Release the button when Fr flashes on the Dot-matrix display to confirm the factory reset.

  • The thermostat resets to factory defaults and returns to the preset selection screen after 5 seconds.

.
NOTE: To cancel the factory reset, press and hold the O button for more than 30 seconds. This restores the thermostat’s UI to its previous state without changing its functional settings.

A factory reset will:

  • Delete all Zigbee connection details.

  • Delete all configuration data.

  • Delete all schedules information.

  • Revert to the default setpoint in manual control.

  • Maintain all Factory settings e.g. MAC address.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?