DUG_Exxact - ZB Thermostat 16 A_WH-01

Troubleshooting

Symptom

Possible cause

Solution

Thermostat temperature measurement is not accurate.

Check the installation location for possible air flow in conduit box or installation tube.

Make sure there is proper sealing of the conduit box or installation tube, to prevent airflow from affecting sensor performance.

The thermostat has gone offline.

  • The thermostat is not On.

  • The thermostat is no longer in signal range of the Hub.

  • Turn the thermostat Off and On.

  • Move the Wiser Hub closer to the thermostat.

NOTE: If the problem persists, tap Help & Support to visit Wiser Support pages.

Unable to join to the Wiser Hub (blinking red LED)

Poor signal between the Wiser Hub and thermostat.

The devices have no power (Thermostat/ Wiser Hub/Wi-Fi® network).

  • Rejoin the thermostat in the app.

  • Turn on the devices' power (Thermostat/ Wiser Hub/Wi-Fi® network).

Unable to set the room temperature by the app.

Wiser Hub signal is weak or not connected to the Wi-Fi® network.

Check for a Wi-Fi® signal.

Find and Bind

 

When the user press and holds the O button for more than 8 seconds, "Fb" LED is displayed on the thermostat matrix display.
It is a Zigbee function, can be ignored.

X mark is displayed on LED matrix

Device is lock and LED matrix displays “X”.

Hold O button for 5 seconds to exit the menu.

is displayed along the device on the Control screen.

  • The floor sensor is reporting a fault.

  • The thermostat is reporting a fault.

  • The room temperature is detected by the floor sensor, while other sensors are available in the room.

  • The room contains multiple flush mount thermostats that are configured differently.

  • If the floor sensor is reporting a fault, replace the floor sensor.

    NOTE: You can not control the temperature in the concerned room using the Wiser Home app, until you replace the floor sensor.
  • If the thermostat is reporting a fault, contact your installer.

  • If the room temperature is detected by the floor sensor, while other sensors are available in the room, remove all other sensors from the room.

  • If the room contains multiple flush mount thermostats that are configured differently, reassign the thermostats to other rooms.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?