DUG_Exxact - ZB Thermostat 16 A_WH-01

Turning on/off the device manually

When thermostat is not in use, you can turn on/off the device manually
NOTE: Make sure to disable childlock before turning off the device.

Press for more than 10 seconds to turn off.

When thermostat is fully off:

  • The LED does not display room temperature.

  • The thermostat does not control room temperature.

  • Outputs remain off

  • On initial interaction, the display shows “X” to indicate the device is off.


To turn on the thermostat:

Press /O/+ once, thermostat Dot-matrix display shows X and then press /O/+ button for more than 5 seconds to power on the thermostat..

When the thermostat is turned on, it returns to its last state.

NOTE: When the thermostat is turned on/off manually, its status is not displayed in the Wiser Home app.
IMPORTANT: If your thermostat is Off, your home is not protected against frost. Using the current version of the Wiser Home app, you can not switch back a thermostat On. It can only be turned On manually.
Hence, If you are leaving for holidays, do not turn the thermostat Off. Instead, lower the setpoint to the minimum frost protection level.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?