DUG_PowerTag-E_WH-09

Creating an automation

The following is an example of creating an automation when Grid is importing more than 0.5 kW, then send a notification.
  1. On the Home screen, tap the .
  2. Tap Automation > to create an automation.
  3. Tap and choose an icon that best represents your automation.
  4. Enter a name of the automation (A) and select any of the following conditions to meet (B).
    • All conditions: All conditions must be met to trigger an automation
    • Any condition: Any one of the condition must be met to trigger an automation.
  5. Tap Add conditions (C) and select any of the following (D):
    • Device status change (Select the device)
    • Away Mode (Enable or Disable)
    NOTE: Maximum 10 conditions can be added.
  6. Select a device that will set the condition. In this example, select Grid.
  7. Tap more than (E) and enter a power value in field (F).
  8. Tap Set (G).
    NOTE: To remove an added condition, swipe left and tap .

  9. To add an action, tap Then > Add an action and select any of the following (H):
    NOTE: Maximum 10 actions can be added.
    • Control a device: Select a device that you want to trigger.
    • Send notification: Turn on the notification for the automation.
    • Activate a moment: Select the moment that you want to trigger.
    • Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.
  10. Tap Notify me (I) and then tap Save.
  11. The saved Automation is displayed on the Automation page. Tap the toggle switch (J) to enable/disable the Automation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?