0611CT1001 R09/24

Trip Units

Available Trip Units

PowerPacT H-, J-, and L-frame circuit breakers offer a range of thermal-magnetic and MicroLogic electronic trip units in interchangeable cases. Thermal-magnetic trip units are designed to open automatically under overload or short circuit. H-frame and J-frame thermal-magnetic circuit breakers contain individual thermal (overload) and instantaneous (short circuit) sensing elements in each pole.

MicroLogic electronic trip units provide intelligent operation, with wide setting ranges make installation upgrades easier. Designed with processing capabilities, MicroLogic trip units can provide measurement information and device operating assistance to supply all of the information required to manage the electrical installation and optimize energy use.

MicroLogic trip units offer excellent measurement accuracy, using a new generation of current transformers combining “iron-core” sensors for self-powered electronics and “air-core” sensors (Rogowski coils) for measurements. The protection functions are managed by an ASIC component that is independent of the measurement functions. This independence ensures immunity to conducted and radiated disturbances and a high level of reliability.

An LED on the front of the electronic trip unit indicates the result of the self-test running continuously on the measurement system and the tripping release. When the green LED is flashing, the links between the CTs, the processing electronics and the Mitop release are operational. The circuit breaker is ready to protect. A minimum current of 15 to 50 A, depending on the device, is required for this function.

The dual adjustment for protection functions on MicroLogic 5/6 consists of:
— an adjustment using rotary switches to set the maximum value
— an adjustment using the keypad or remote controls to fine-tune the setting. This setting may not exceed the first one. It can be read directly on the MicroLogic screen, to within one ampere and a fraction of a second.

NOTE: All the trip units have a transparent sealable cover that protects access to the adjustment rotary switches.

For MicroLogic trip unit features, see PowerPacT H-, J-, and L-frame Circuit Breaker Trip Units.

Understanding the Names of MicroLogic Electronic Trip Units

 

Protection

Frame

Measurements

Applications

1: I

3: LI or LSI

5: LSI

6: LSIG

H- and J-frame

A: Ammeter

DIstribution or M: Motors

L: Long time

S: Short time

I: Instantaneous

G: Ground fault

L-frame

E: Energy

Example Trip Unit Names

MicroLogic 1.3 M Trip Unit

Instantaneous only

400 or 600 A

Motor

MicroLogic 3.3 Trip Unit

LI

250, 400, or 600 A

Distribution

MicroLogic 3.2S Trip Unit

LSI

60, 100, 150, or 250 A

Distribution

MicroLogic 5.2A Trip Unit

LSI—Ammeter

60, 100, 150, or 250 A

Distribution

lr = long-time pickup

The current level at which the circuit breaker long-time delay function begins timing.

tr = long-time delay

The length of time the circuit breaker will carry a sustained overcurrent (greater than the long-time pickup) before initiating a trip signal.

lsd = short-time pickup

The current level at which the circuit breaker short-time delay function begins timing.

tsd = short-time delay

The length of time the circuit breaker will carry a short circuit (current greater than the short-time pickup) before initiating a trip signal.

li = instantaneous pickup

The current level at which the circuit breaker will trip with no intentional time delay.

lg = ground-fault pickup

The level of ground-fault current at which the trip system begins timing.

Trip Unit Availability

Trip Unit Type

Trip Unit

H-, J-Frame

Trip Unit

L-Frame

Distribution Protection Thermal-Magnetic

T-M

N/A

Distribution Protection
LI

MicroLogic 3.2 and
3.2-W

MicroLogic 3.3 and
3.3-W

Distribution Protection
LSI
Fixed ST and LT delays

MicroLogic 3.2S and
3.2-SW

MicroLogic 3.3S and
3.3-SW

Distribution Protection
LSI + Ammeter

MicroLogic 5.2 A and
5.2 A-W

MicroLogic 5.3 A and
5.3 A-W

Distribution Protection
LSI + Energy Monitoring

MicroLogic 5.2 E and
5.2 E-W

MicroLogic 5.3 E and
5.3 E-W

Distribution Protection
LSIG + Ammeter

MicroLogic 6.2 A and
6.2 A-W

MicroLogic 6.3 A and
6.3 A-W

Distribution Protection
LSIG + Energy Monitoring

MicroLogic 6.2 E and
6.2 E-W

MicroLogic 6.3 E and
6.3 E-W

Motor Circuit Protection Magnetic Only

M

N/A

 

Motor Protection MicroLogic 1 M

N/A

MicroLogic 1.3M

Motor Protection MicroLogic 2 M

MicroLogic 2.2 M

MicroLogic 2.3 M

W = mission critical trip unit.

Protection of Distribution Systems

Thermal-Magnetic Trip Units

TM thermal-magnetic trip units can be used on PowerPacT H and J-frame circuit breakers with interrupting levels D/G/J/L. Thermal-magnetic trip units are available in factory sealed or field-interchangeable constructions.

H-Frame Trip Curve
(ln) Fixed threshold thermal protection against overload
(li) Fixed threshold  instantaneous protection against short circuits

 

H-Frame and J-Frame Three-Pole Field-Installable Thermal-Magnetic Trip Unit

15–60 A H-Frame

70–150 A H-Frame

150–250 A J-Frame

H-Frame Trip Unit

Cat No.

Amperage

Cat No.

Amperage

Cat. No.

J-Frame Trip Unit
Amperage

15 A

HT3015

70 A

HT3070

150 A

JT3150

20 A

HT3020

80 A

HT3080

175 A

JT3175

25 A

HT3025

90 A

HT3090

200 A

JT3200

30 A

HT3030

100 A

HT3100

225 A

JT3225

35 A

HT3035

110 A

HT3110

250 A

JT3250

40 A

HT3040

125 A

HT3125

45 A

HT3045

150 A

HT3150

50 A

HT3050

60 A

HT3060

MicroLogic 3 Trip Units

MicroLogic 3 trip units can be used on PowerPacT H-, J-, and L-Frame circuit breakers with performance levels D/G/J/L.

They provide:

  • standard protection of distribution cables

  • indication of:

    • overloads (using LEDs)

    • overload tripping (using the SDx relay module)

Circuit breakers equipped with MicroLogic 3 trip units can be used to protect distribution systems supplied by transformers.

Protection

Settings are made using the adjustment rotary switches.

Overloads: Long time protection (Ir)

Inverse time protection against overloads with an adjustable current pick-up Ir set using a rotary switch and an adjustable time delay tr.

Neutral protection

  • On three-pole L-frame circuit breakers, neutral protection is not possible.

  • On four-pole L-frame circuit breakers, neutral protection may be set using a three-position switch:

    • switch position 4P 3D: neutral unprotected

    • switch position 4P 3D + N/2: neutral protection at half the value of the phase pick-up, (0.5 x Ir)

    • switch position 4P 4D: neutral fully protected at Ir

Front indicators

  • The green “Ready” LED blinks slowly when the electronic trip unit is ready to provide protection. It indicates the trip unit is operating correctly.

  • Overload pre-alarm LED: steady on when I > 90% Ir

  • Overload LED: steady on when I > 105% Ir

Remote indicators

An overload trip signal can be remotely checked by installing an SDx relay module inside the circuit breaker. This module receives the signal from the MicroLogic electronic trip unit through an optical link and makes it available on the terminal block. The signal is cleared when the circuit breaker is reclosed. See SDx Module.

MicroLogic 3 Trip Units

Ratings

In at 104°F (40°C)*

60 A

100 A

150 A

250 A

400 A

600 A

Circuit Breaker

H-frame

X

X

X

J-frame

X

L-frame

X

X

X

MicroLogic 3.2 / 3.3 trip units*

L Long-time protection

Pick-Up (A)
Tripping between 1.05 and 1.20 Ir

Ir

Value depending on sensor rating (In) and setting on rotary switch

In =60 A

Ir =

15

20

25

30

35

40

45

50

60

In = 100 A

Ir =

35

40

45

50

60

70

80

90

100

In = 150 A

Ir =

50

60

70

80

90

100

110

125

150

In = 250 A

Ir =

70

80

100

125

150

175

200

225

250

In = 400 A

Ir =

125

150

175

200

225

250

300

350

400

In = 600 A

Ir =

200

225

250

300

350

400

450

500

600

Time Delay (s)
Accuracy 0 to -20%

tr

0.5

1

2

4

8

16

1.5 x Ir

15

25

50

100

200

400

6 x Ir

0.5

1

2

4

8

16

7.2 x Ir

0.35

0.7

1.4

2.8

5.5

11

Thermal memory

20 minutes before and after tripping

I Instantaneous

Pick-up (A) accuracy ± 15%

Ii x

60 A, 100 A

1.5

2

3

4

6

8

10

12

15

150 A

1.5

2

3

4

6

8

10

12

15

250 A

1.5

2

3

4

5

6

8

10

12

400 A

1.5

2

3

4

5

6

8

10

12

600 A

1.5

2

3

4

5

6

8

10

11

Non-tripping time
Maximum break time

10 ms 50 ms for I > 1.5 Ii

MicroLogic 3.2S / 3.3S trip units*

L Long-time protection

Pick-Up (A) Tripping between 1.05 and 1.20 Ir

Ir

Value depending on sensor rating (In) and setting on rotary switch

In =60 A

Ir =

15

20

25

30

35

40

45

50

60

In = 100 A

Ir =

35

40

45

50

60

70

80

90

100

In = 150 A

Ir =

50

60

70

80

90

100

110

125

150

In = 250 A

Ir =

70

80

100

125

150

175

200

225

250

In = 400 A

Ir =

125

150

175

200

225

250

300

350

400

In = 600 A

Ir =

200

225

250

300

350

400

450

500

600

Time Delay (s)
Accuracy 0 to -20%

tr

non-adjustable

1.5 x Ir

400

6 x Ir

16

7.2 x Ir

11

Thermal memory

20 minutes before and after tripping

S Short-time protection

Pick-up (A) accuracy ± 10%

Isd - Ir x...

1.5

2

3

4

5

6

7

8

10

Time delay (ms)

tsd

non-adjustable

Non-tripping time
Maximum break time

20
80

I Instantaneous

Pick-up (A)
accuracy ± 15%

Ii x

60 A, 100 A

1.5

2

3

4

6

8

10

12

15

150 A

1.5

2

3

4

6

8

10

12

15

250 A

1.5

2

3

4

5

6

8

10

12

400 A

1.5

2

3

4

5

6

8

10

12

600 A

1.5

2

3

4

5

6

8

10

11

Non-tripping time
Maximum break time

10 ms
50 ms for I > 1.5 Ii

MicroLogic 5/6 A or E Trip Units

MicroLogic 5/6 A (Ammeter) or E (Energy) trip units can be used on PowerPacT H-, J-, and L-frame circuit breakers with performance levels D, G, J, or L. They all have a front display module. They offer basic LSI protection (MicroLogic 5 trip unit) or LSI and ground-fault protection G (MicroLogic 6 trip unit). They also offer measurement, alarm and energy values.

The capabilities of MicroLogic 5/6 A and E trip units come into full play with the front display module. When the two are connected using a simple cable with RJ45 connectors, the combination offers full Power Meter capabilities and all the measurements required to monitor the electrical installation.

MicroLogic 5/6 A or E Trip Units

Trip Unit

Measurements

Operating and Maintenance Assistance

Communication Network

Ammeter (MicroLogic A Trip Unit)

Current measurements

  • Phase and neutral currents IA, IB, IC, IN

  • Average current of the 3 phases Iavg

  • Highest current of the three phases Imax

  • Ground-fault current Ig (MicroLogic 6.2 / 6.3 A) trip units

  • Maximum and minimum current measured

Indicators, alarms and histories

  • Fault types

  • Alarms for high/low alarm thresholds linked to I measurements

  • Trip, alarm and operating histories

  • Time-stamped tables for settings and maximum current

Maintenance indicators

  • Operation, trip and alarm counters

  • Operating hours counter

  • Contact wear

  • Load profile and thermal image

Modbus with add-on module

Energy (MicroLogic E Trip Unit)

Current measurements

  • Phase and neutral currents IA, IB, IC, IN

  • Average current of the 3 phases Iavg

  • Highest current of the three phases Imax

  • Ground-fault current Ig (MicroLogic 6.2 / 6.3 A trip units)

  • Maximum and minimum current measured

  • Current unbalance between phases

Voltage measurements

  • Phase-to-phase (V) and phase-to-neutral (U) voltages

  • Average voltages Vavg, Uavg

  • Ph-Ph (V) and Ph-N (U) voltage unbalance

Frequency measurements

  • Frequency (f)

Power-quality indicators

  • Total harmonic distortion (THD) for current and voltage

Power measurements

  • Active, reactive and apparent power, total and per phase

  • Power factor and cos φ

Maximum and minimum

  • For all I, V, f, P, E measurements

Demand current and power measurements

  • Demand values, total and per phase

  • Maximum demand

Energy metering

  • Active, reactive and apparent energy, total and per phase

Indicators, alarms and histories

  • Fault types

  • Alarms for high/low thresholds linked to I, V, f, P, E measurements

  • Trip, alarm and operating histories

  • Time-stamped tables for settings and I, V, f, P, E maximum values

Maintenance indicators

  • Operation, trip and alarm counters

  • Operating hours counter

  • Contact wear

  • Load profile and thermal image

Modbus with add-on module

Power Requirements

The amount of current needed to power the trip unit is printed in the upper left hand corner of the trip unit by the Ready LED.

Trip Unit Power Requirements

Frame

Power-Up Requirement

H-Frame, 60 A

60 A

>15 A

100 A

>15 A

150 A

>30 A

J-Frame, 250 A

250 A

>30 A

L-Frame, 600 A

400 A

>50 A

600 A

>50 A

Protection

Settings can be adjusted in two ways, using the rotary switches and/or the keypad.

  • The keypad can be used to make fine adjustments in 1 A steps below the maximum value defined by the setting on the rotary switch.

  • Access to setting modifications using the keypad is protected by a locking function displayed on the screen and controlled by a microswitch.

  • The lock is activated automatically if the keypad is not used for 5 minutes.

  • Access to the microswitch is protected by a transparent, sealable cover.

  • With the cover closed, it is still possible to display the various settings and measurements using the keypad.

Overloads: Long-Time Protection (Ir)

Inverse time protection against overloads with an adjustable current pick-up Ir is set using a rotary switch or the keypad for fine adjustments. The time delay tr is set using the keypad.

Short-Circuits: Short-Time Protection (Isd)

Short-circuit protection with an adjustable pick-up Isd and adjustable time delay tsd, with the possibility of including a portion of an inverse time curve (I2t On).

Short-Circuits: Instantaneous Protection (Ii)

Instantaneous protection with adjustable pick-up Ii.

Additional Ground Fault Protection (Ig) on MicroLogic 6 Trip Units

Residual type ground-fault protection with an adjustable pick-up Ig and adjustable time delay tg. Possibility of including a portion of an inverse time curve (I2t On).

Neutral Protection

  • On four-pole circuit breakers, this protection can be set using the keypad:

    • Off: neutral unprotected

    • 0.5: neutral protection at half the value of the phase pick-up (0.5 x Ir)

    • 1.0: neutral fully protected at Ir

    • OSN: Oversized neutral protection at 1.6 times the value of the phase pick-up.
      Used when there is a high level of 3rd order harmonics (or orders that are multiples of 3) that accumulate in the neutral and create a high current. In this case, the device must be limited to Ir = 0.63 x In for the maximum neutral protection setting of 1.6 x Ir.

  • With three-pole circuit breakers, the neutral can be protected by installing an external neutral sensor with the output (T1, T2) connected to the trip unit.

Zone Selective Interlocking (ZSI)

A ZSI terminal block may be used to interconnect a number of MicroLogic trip units to provide zone selective interlocking for short-time (Isd) and ground-fault (Ig) protection, without a time delay. For PowerPacT H- and J-frame circuit breakers, the ZSI function is available only in relation to the upstream circuit breaker (ZSI out). For PowerPacT L-frame circuit breakers, the ZSI function is available in relation to the upstream circuit breaker (ZSI out) and downstream circuit breakers (ZSI in).

Display of Type of Fault

On a fault trip, the type of fault (Ir, Isd, Ii, Ig), the phase concerned and the interrupted current are displayed. An external power supply is required.

Indicators

Front Indicators

  • The green “Ready” LED blinks slowly when the electronic trip unit is ready to provide protection. It indicates the trip unit is operating correctly.

  • Orange overload pre-alarm LED stays on when I > 90% Ir

  • Red overload LED stays on when I > 105% Ir

Remote Indicators

An SDx relay module installed inside the circuit breaker can be used to remote the following information:

  • overload trip

  • overload prealarm (MicroLogic 5 trip units) or ground fault trip (MicroLogic 6 trip units)

This module receives the signal from the MicroLogic electronic trip unit through an optical link and makes it available on the terminal block. The signal is cleared when the circuit breaker is closed.

Note: all the trip units have a transparent sealable cover.

These outputs can be reprogrammed to be assigned to other types of tripping or that protects access to the adjustment rotary switch. The module is described in detail in the section dealing with accessories.

MicroLogic 5/6 Trip Unit Ratings

MicroLogic 5/6 Trip Unit—L Long-Time Protection

Ratings

In at 104°F (40°C)*

60 A

100 A

150 A

250 A

400 A

600 A

Circuit Breaker*

H-frame

X

X

X

     

J-frame

     

X

   

L-frame

       

X

X

Pick-up (A) tripping between 1.05 and 1.20 Ir

Ir

Rotary switch 

Value depending on the trip unit rating (In) and setting on rotary switch

In = 60 A

Ir = 

15

20

25

30

35

40

45

50

60

In = 100 A

Ir = 

35

40

45

50

60

70

80

90

100

In = 150 A

Ir = 

50

60

70

80

90

100

110

125

150

In = 250 A

Ir = 

70

80

100

125

150

175

200

225

250

In = 400 A

Ir = 

125

150

175

200

225

250

300

350

400

In = 600 A

Ir = 

200

225

250

300

350

400

450

500

600

   

Keypad setting

Fine adjustment in 1 A steps below maximum value set on rotary switch

Time Delay (s) Accuracy 0 to -20%

tr =

Keypad setting

0.5

1

2

4

8

16

1.5 x Ir

15

25

50

100

200

400

6 x Ir

0.5

1

2

4

8

16

7.2 x Ir

0.35

0.7

1.4

2.8

5.5

11

Thermal memory

20 minutes before and after tripping

MicroLogic 5/6 Trip Unit—S Short-Time Protection

Ratings

In at 104°F (40°C)*

60 A

100 A

150 A

250 A

400 A

600 A

Circuit Breaker*

H-frame

X

X

X

     

J-frame

     

X

   

L-frame

       

X

X

Pick-up (A) accuracy ± 10%

Isd

Keypad setting

1.5

2

2.5

3

3.5

4

4.5

5

5.5

6

6.5

7

7.5

8

8.5

9

9.5

10

Fine adjustment in 0.5 x Ir steps using the keypad 

Time delay

tsd =

Keypad setting

I2t Off

0

0.1 s

0.2 s

0.3 s

0.4 s

I2t On

0.1 s

0.2 s

0.3 s

0.4 s

Non-tripping time (ms)
Maximum break time (ms)

20
80

80
140

140
200

230
320

350 ms
500 ms

MicroLogic 5/6 Trip Unit— Instantaneous

Ratings

In at 104°F (40°C)*

60 A

100 A

150 A

250 A

400 A

600 A

Circuit Breaker*

H-frame

X

X

X

     

J-frame

     

X

   

L-frame

       

X

X

Pick-up (A) accuracy ± 15%

Ii = In x

Rotary Switch

60 A

1.5

2

0.3

4

6

8

10

12

15

100 A

1.5

2

0.3

4

6

8

10

12

15

150 A

1.5

2

0.3

4

6

8

10

12

15

250 A

1.5

2

0.3

4

5

6

8

10

12

400 A

1.5

2

0.3

4

5

6

8

10

12

600 A

1.5

2

0.3

4

5

6

8

10

11

Non-tripping time
Maximum break time

10 ms
50 ms for I > Ii

MicroLogic 5/6 Trip Unit—G Ground Fault Protection for MicroLogic 6 A or E Trip Units

Ratings

In at 104°F (40°C)*

60 A

100 A

150 A

250 A

400 A

600 A

Circuit Breaker*

H-frame

X

X

X

     

J-frame

     

X

   

L-frame

       

X

X

Pick-up (A) accuracy ± 10%

Ig

Keypad Setting

 

In= 60 A

Ig =

0.3

0.35

0.4

0.45

0.5

0.55

0.6

0.65

0.7

0.75

0.8

0.85

0.9

0.95

1

   

In= 100–600 A

Ig =

0.2

2.5

0.3

0.35

0.4

0.45

0.5

0.55

0.6

0.65

0.7

0.75

0.8

0.85

0.9

0.95

1

Time delay (s)

tg =

Keypad setting

I2t Off

0

0.1

0.2

0.3

0.4

I2t On

0.1

0.2

0.3

0.4

Non-tripping time
Maximum break time

20
80

80
140

140
200

230
320

350
500

Test

Ig function

Built in

Field-Installable Trip Units

MicroLogic 3 Field-Installable Trip Units

Circuit Breaker*

Trip Unit Type

Catalog No.

Frame

Standard

Poles

Rating

H-Frame

UL/CSA/NOM

3

60 A 

MicroLogic 3.2 

HE3060U31X

MicroLogic 3.2S 

HE3060U33X

100 A 

MicroLogic 3.2 

HE3100U31X

MicroLogic 3.2S 

HE3100U33X

150 A 

MicroLogic 3.2 

HE3150U31X

MicroLogic 3.2S 

HE3150U33X

J-Frame

UL/CSA/NOM

3

250 A 

MicroLogic 3.2 

JE3250U31X

MicroLogic 3.2S 

JE3250U33X

L-Frame

UL/CSA/NOM

3

250 A 

MicroLogic 3.3 

LE3250U31X

MicroLogic 3.3S

LE3250U33X

400 A 

MicroLogic 3.3 

LE3400U31X

MicroLogic 3.3S

LE3400U33X

600 A 

MicroLogic 3.3 

LE3600U31X

MicroLogic 3.3S 

LE3600U33X

4

250 A 

MicroLogic 3.3 

LE4250U31X

MicroLogic 3.3S

LE4250U33X

400 A 

MicroLogic 3.3 

LE4400U31X

MicroLogic 3.3S

LE4400U33X

600 A 

MicroLogic 3.3 

LE4600U31X

MicroLogic 3.3S 

LE4600U33X

MicroLogic 5 and 6 Field-Installable Trip Units

Circuit Breaker *

Trip Unit Type

Catalog No.

Frame

Standard

Poles

Rating

H-Frame

UL/CSA/NOM

3

60 A

MicroLogic 5.2 A

HE3060U43X

MicroLogic 6.2 A

HE3060U44X

MicroLogic 5.2 E

HE3060U53X

MicroLogic 6.2 E

HE3060U54X

100 A

MicroLogic 5.2 A

HE3060U43X

MicroLogic 6.2 A

HE3100U44X

MicroLogic 5.2 E

HE3100U53X

MicroLogic 6.2 E

HE3100U54X

150 A

MicroLogic 5.2 A

HE3150U43X

MicroLogic 6.2 A

HE3150U44X

MicroLogic 5.2 E

HE3150U53X

MicroLogic 6.2 E

HE3150U54X

J-Frame

UL/CSA/NOM

3

250 A

MicroLogic 5.2 A

JE3250U43X

MicroLogic 6.2 A

JE3250U44X

MicroLogic 5.2 E

JE3250U53X

MicroLogic 6.2 E

JE3250U54X

L-Frame

UL/CSA/NOM

3

400 A

MicroLogic 5.3 A

LE3400U43X

MicroLogic 6.3 A

LE3400U44X

MicroLogic 5.3 E

LE3400U53X

MicroLogic 6.3 E

LE3400U54X

600 A

MicroLogic 5.3 A

LE3600U43X

MicroLogic 6.3 A

LE3600U44X

MicroLogic 5.3 E

LE3600U53X

MicroLogic 6.3 E

LE3600U54X

UL/CSA/NOM

4

400 A

MicroLogic 5.3 A

LE4400U43X

MicroLogic 6.3 A

LE4400U44X

MicroLogic 5.3 E

LE4400U53X

MicroLogic 6.3 E

LE4400U54X

600 A

MicroLogic 5.3 A

LE4600U43X

MicroLogic 6.3 A

LE4600U44X

MicroLogic 5.3 E

LE4600U53X

MicroLogic 6.3 E

LE4600U54X

MicroLogic Trip Unit Spare Parts

Spare Parts

Description

Frame

Trip Unit

Catalog No.

LCD Display

H/J/L

MicroLogic 5

S429483

MicroLogic 6

S429484

Trip Unit Cover-Transparent

H/J

MicroLogic 3

S429481

L

S432461

H/J

MicroLogic 5/6

S429478

L

S432459

Trip Unit Wire Seal

H

MicroLogic 3/5/6

MICROTUSEAL

Smart System Communication Wiring System

Wiring System ULP

The wiring system is designed for low-voltage power switchboards. Installation does not require special tools or training. The prefabricated wiring ensures both data transmission (Modbus protocol) and 24 Vdc power distribution for the communications modules on the MicroLogic trip units.

A. FDM128 display for 8 LV devices
B. IFE Ethernet interface for LV circuit breaker and gateway
C. IFM Modbus-SL interface for LV circuit breaker
D. FDM121 display for LV circuit breaker
E. IO input/output interface module for LV circuit breaker
F. MasterPacT NT/NW circuit breaker

G. PowerPacT H-, J-, or L-frame circuit breaker
H. ULP line terminator
I. ULP cable
J. Breaker ULP cord
K. NSX cord
L. PowerPacT P/R or ComPacT NS

Smart System Communication Wiring System Modbus Direct

A

B

C

D

E

F

IFE (LV434001 / LV434002)

IFM (LV434000)

Modbus SL hub (S434224)

Drawout MasterPacTMTZ1 / MTZ2 / MTZ3

Fixed MasterPacT MTZ1/MTZ2/MTZ3

ComPacT NSX/PowerPacT H-, J-, L-Frame

G

H

I

J

K

BSCM MBSL/ULP (S434220)

Ethernet

BSCM MBSL cord (S434221 / S434222 / S434223)

Modbus cord

ULP cord

Four Functional Levels

All PowerPacT H-, J-, and L-frame circuit breakers devices can be equipped with the communication function using a pre-wired connection system and a Modbus communication interface module. The interface module can be connected directly or through the front display module (FDM121).

The PowerPacT H-, J-, and L-frame circuit breakers can be integrated in a Modbus communication network. Four functional levels can be used separately or combined to adapt to all supervision requirements.

Level

Function

Communication of status indications

Compatible with PowerPacT H-, J- and L-frame circuit breakers and automatic switches. Use the BSCM module to access the following information:

  • ON/OFF position

  • trip indication

  • fault-trip indication

Communication of commands

Available on all circuit breakers and automatic switches with communicating motor operators, the remote control can be used to:

  • open

  • closed

  • reset

Communication of measurements with MicroLogic 5/6 A or E trip unit

This level provides access to:

  • instantaneous and demand values

  • maximums/minimums

  • energy metering

  • demand current and power

  • power quality

Communication of operating assistance with MicroLogic 5/6 A or E trip unit

This level also provides access to:

  • protection and alarm settings

  • time-stamped histories and event tables

  • maintenance indicators

Modbus Principle

The Modbus RS 485 (RTU protocol) system is an open bus on which communicating Modbus devices (PowerPacT and MasterPacT circuit breakers, Power Meter PM700, PM800, etc.) are installed. All types of PLCs and microcomputers may be connected to the bus.

Number of Devices

The maximum number of devices that may be connected to the Modbus bus depends on the type of device (PowerPacT circuit breaker with Modbus COM, PM700, PM800, MasterPacT circuit breaker, etc.), the baud rate (19200 is recommended), the volume of data exchanged and the desired response time. The RS 485 physical layer offers up to thirty-two connection points on the bus (one client, thirty-one servers).

Length of Bus

The maximum recommended length for the Modbus bus is 3940 feet (1200 meters).

Bus Power Source

A 24 Vdc power supply is required (less than 20% ripple, insulation class II).

Ethernet Principle

Ethernet is a data link and physical layer protocol defined by IEEE 802 10 and 100 Mbps specifications that connects computer or other Ethernet devices. Ethernet is an asynchronous Carrier Sense Multiple Access with Collision detection (referred as CSMA/CD) protocol. Carrier Sense means that the hosts can detect whether the medium (coaxial cable) is idle or busy.

Multiple Access means that multiple hosts can be connected to the common medium. Collision Detection means a host detects whether its transmission has collided with the transmission of another host (or hosts).

IFE Ethernet interface can be connected to a PC or a laptop over Ethernet. The maximum length of Ethernet cable is 325 feet (100 meters). IFE Ethernet interface + gateway provides a Modbus TCP/IP gateway over Ethernet to enable Modbus TCP communication from a Modbus TCP client to any Modbus server devices connected to it. The maximum number of active TCP client connections is twelve.

IFE Ethernet interface has an embedded web server (web page).

IFE Ethernet Interface

IFE Interface, IFE Interface + Gateway Description

 

IFE Interface

 

IFE Interface + Gateway

Introduction

The IFE interface and IFE interface + gateway enable low-voltage circuit breakers such as MasterPacT and PowerPacT to be connected to an Ethernet network.

IFE Interface

Provides Ethernet access to a single low-voltage circuit breaker.

Function: Interface - one circuit breaker is connected to the IFE interface using its ULP port.

IFE Interface + Gateway

Provides Ethernet access to one or several low-voltage circuit breakers.

Functions:

  • Interface - one circuit breaker is connected to the IFE interface using its ULP port.

  • Gateway: several circuit breakers on a Modbus network are connected using the IFE interface + gateway client Modbus port.

IFE Interface, IFE Interface + Gateway Features

  • Dual 10/100 Mbps Ethernet port for simple daisy chain connection.

  • Device profile web service for discovery of the IFE interface, IFE interface + gateway on the LAN.

  • Ethernet interface for MasterPacT and PowerPacT circuit breakers.

  • Gateway for Modbus-SL connected devices (IFE interface + gateway only).

  • Embedded set-up web pages.

  • Embedded monitoring web pages.

  • Embedded control web pages.

  • Built-in e-mail alarm notification.

IFE Interface, IFE Interface + Gateway Screen

Mounting

The IFE interface and IFE interface + gateway are DIN rail mounting devices. A stacking accessory enables the user to connect several IFMs (ULP to Modbus interfaces) to an IFE interface + gateway without additional wiring.

24 Vdc Power Supply

The IFE interface and the IFE interface + gateway must always be supplied with 24 Vdc.

The IFMs stacked to an IFE interface + gateway have power supplied by the IFE interface + gateway, thus it is not necessary to supply them separately. It is recommended to use a UL listed and recognized limited voltage/limited current or a class 2 power supply with a 24 Vdc, 3 A maximum.

Required Circuit Breaker Communication Modules

The connection to an IFE interface or IFE interface + gateway requires a communication module embedded into the circuit breaker:

  • PowerPacT and ComPacT (fixed or drawout) circuit breakers: BSCM communication module

  • Drawout PowerPacT and ComPacT circuit breakers: BSCM and its respective I/O (Input/Output) application module.

All connection configurations for PowerPacT and ComPacT circuit breakers require the circuit breaker ULP cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac. When the second ULP RJ45 connector is not used, it must be closed with a ULP terminator (TRV00880).

Network Communication Interface

Characteristic

Value

Type of interface module

Modbus RTU, RS485 serial connection

Modbus TCP/IP Ethernet

Transmission

Modbus RS485

  • Transfer rate: 9,600–19,200 Baud

  • Medium Double shielded twisted pair

  • Impedance 120 Ω

Ethernet

Transfer rate: 10/100 Mbps

Medium STP, Cat5e, straight cable

Structure

Type

Modbus, Ethernet

Method

Client/Server

Device type

Modbus

Client

Ethernet

Server

Turnaround time

Modbus

10 ms

Ethernet

1 ms

Maximum length of cable

Modbus

1000 m

Ethernet

100 m

Type of bus connector

Modbus

4-pin connector

Ethernet

RJ45 (Shielded)

IFE Ethernet Interface Characteristics—Web Page Description

Monitoring Web Page
Real time data X
Device logging X
Control Web Page
Single device control X
Diagnostics Web Page
Statistics X
Device information X
IMU (circuit breaker) information X
Read device registers X
Communication check X
Maintenance Web Page
Maintenance log X
Maintenance counters X
Setup Web Page
Device localization/name X
Ethernet configuration (dual port) X
IP configuration X
Modbus TCP/IP filtering X
Serial port X
Date and time X
E-mail server configuration X
Alarms to be e-mailed X
Device list X
Device logging X
Device log export X
SNMP parameters X
Documentation links X
Preferences X
Advanced services control X
User accounts X

IFE Ethernet Interface—General Characteristics

Environmental Characteristics

Conforming to standards

UL 508, UL 60950, IEC 60950, 60947-6-2

Certification

cUIUs, FCC, CE

Ambient temperature

Storage: -40 to +185°F (-40 to +85°C)

Operation: -13 to +158°F (-25 to +70°C)

Protective treatment

ULVO, conforming to IEC 60068-2-30

Pollution

Level 3

Mechanical Characteristics

Shock resistance

Conforming to IEC 60068-2-27 15g/11ms, 1/2 sinusoidal

Resistance to sinusoidal vibrations

Conforming to IEC 60068-2-6

Electrical Characteristics

Power supply

24 Vdc, -20%/+10% (19.2 to 26.4 Vdc)

Consumption

Typical: 4 Vdc, 120 mA at 68°F (20°C)

Maximum with gateway: 26.4 Vdc, 3 A at 140°F (60°C)

Physical Characteristics

Dimensions

2.83 x 4.13 x 2.79 in. (72 x 105 x 71 mm)

Mounting

Mounting DIN rail

Weight

182.5 g (0.41 lb)

Degree of protection of the installed module

On the front panel (wall mounted enclosure): IP4x

Connectors: IP2x

Other parts: IP3x

Connections

Screw type terminal blocks

Technical Characteristics - 24 Vdc Power Supply

Power supply type

Regulated switch type

Rated power

72 W

Input voltage

100–120 Vac for single phase

200–500 Vac phase-to-phase

PFC filter

With IEC 61000-3-2

Output voltage

24 Vdc

Power supply out current

3:00 AM

IFE Ethernet Interface Characteristics

NOTE: Use a UL Listed/UL Recognized limited voltage/limited current or a Class 2 power supply with a 24 Vdc, 3 A maximum.

A. Ethernet 1 and Ethernet 2 communication port

B. 24 Vdc power supply terminal block

C. Ethernet communication LEDs:

  • yellow: 10 Mb

  • green: 100 Mb

D. Module status LED:

  • steady off: no power

  • steady green: device operational

  • steady red: major fault

  • flashing green: standby

  • flashing red: minor fault

  • flashing green/red: self-test

E. Network status LED:

  • steady power off: no power/no valid IP address

  • steady green: connected, valid IP address

  • steady orange: default IP address Z

  • steady red: duplicated IP address

  • flashing green/red: self-test

F. Sealable transparent cover

G. ULP status LED

H. Test button (accessible closed cover)

I. Locking pad

J. Modbus traffic status LED (IFE Interface + Gateway only)

K. Device name label

L. ULP ports

IFM Modbus Communication Interface

Function

IFM Modbus Communication Interface. Ref.: TRV00210

An IFM Modbus communication interface is required for connection of a MasterPacT or PowerPacT circuit breaker to a Modbus network as long as this circuit breaker is provided with a ULP (Universal Logic Plug) port. The port is available on the BSCM.

Once connected, the circuit breaker is considered as a server by the Modbus client. Its electrical values, alarm status, open/close signals can be monitored or controlled by a Programmable Logic Controller or any other system.

Characteristics

ULP Port

Two RJ45 sockets, internal parallel wiring.

  • Connection of a single circuit breaker.

  • A ULP line terminator or an FDM121 display unit must be connected to the second RJ45 ULP socket.

  • The RJ45 sockets deliver a 24 Vdc supply fed from the Modbus socket.

  • Built-in test function, for checking the correct connection to the circuit breaker and FDM121 display unit.

Modbus Server Port

  • Top socket for screw-clamp connector, providing terminals for:

    • 24 Vdc input supply (0 V, +24 V)

    • Modbus line (D1, D2, Gnd) 2-wire Modbus system.

  • Lateral socket, for DIN-rail stackable connector. Both top and lateral sockets are internally parallel wired.

  • Multiple IFMs can be stacked, thus sharing a common power supply and Modbus line without individual wiring.

  • On the front face:

    • Modbus address setting (1 to 99): 2 coded rotary switches

    • Modbus locking pad: enables or disable the circuit breaker remote control and modification of IFM parameters.

  • Self-adjusting communication format (Baud rate, parity).

Technical Characteristics

IFM Modbus Communication Interface

Dimensions

0.71 x 2.83 x 3.78 in. (18 x 72 x 96 mm)

Maximum number of stacked IFM

12

Degree of protection of the installed module

Part projecting beyond the escutcheon

IP4x

Other module parts

IP3x

Connectors

IP2x

Operating temperature

-13 to 158°F (-25 to +70°C)

Power supply voltage

24 Vdc -20%/+10% (19.2–26.4 Vdc)

Consumption

Typical

21 mA/24 Vdc at 68°F (20°C)

Maximum

30 mA/19.2 Vdc at 140°F (60°C)

Certification

CE

IEC/EN 60947-1

UL

UL 508 - Industrial Control Equipment

CSA

No. 142-M1987 - Process Control Equipment

  • CAN/CSA C22.2 No. 0-M91 - General requirements - Canadian Electrical Code Part

  • CAN/CSA C22.2 No. 14-05 - Industrial Control Equipment

Simplified IFM Installation

Stacking an IFM

Stacking Accessories

Up to Twelve Stacked IFMs

Stacking an IFE Interface + Gateway with IFMs

I/O Application Module

Description

I/O Application Module

The I/O (Input/Output) application module for a low-voltage circuit breaker is part of an ULP system with built-in functions and applications to enhance the application needs. The ULP system architecture can be built without any restrictions using the wide range of circuit breakers.

The I/O application module is compliant with the ULP system specifications.

Two I/O application modules can be connected in the same ULP network.

The ranges of low-voltage circuit breakers enhanced by the I/O application module are:

  • MasterPacT NW

  • MasterPacT NT

  • PowerPacT R-Frame

  • PowerPacT P-Frame

  • PowerPacT H-Frame

  • PowerPacT J-Frame

  • PowerPacT L-Frame

I/O (Input/Output) Application Module for Low-Voltage Circuit Breaker

The I/O application module resources are:

  • Six digital inputs that are self powered for either NO and NC dry contact or pulse counter.

  • Three digital outputs that are a bistable relay (5 A maximum).

  • One analog input for PT100 temperature sensor.

Pre-Defined Application

The pre-defined application adds new functions to the I/O application module by:

  • Selection by the application rotary switch on the I/O application module, defining the application with pre-defined input/output assignment and wiring diagram.

  • No additional setting with the customer engineering tool required.

The resources not assigned to the pre-defined application are free for additional user-defined applications:

  • cradle management

  • circuit breaker operation

  • cradle management + ERMS (Energy Reduction Maintenance Setting)

    NOTE: Use only MicroLogic P or H trip units with the blue ERMS label for energy reduction maintenance setting systems. Review the I/O module user guide 0613IB1317 and ERMS installation instructions NHA37346 for details on installation, testing, and operation of the ERMS system.


  • light and load control

  • custom

User-Defined Applications

User-defined applications are processed by the I/O application module in addition to the pre-defined application selected.

The user-defined applications are available depending on:

  • the pre-defined application selected

  • the I/O application module resources (inputs and outputs) not used by the application.

The resources required by user-defined applications are assigned using the customer engineering tool:

  • protection

  • control

  • energy management

  • monitoring.

Mounting

The I/O application module is a DIN rail mounted device. Install on a steel DIN rail that is properly grounded near the device.

Application Rotary Switch

The application rotary switch enables the selection of the pre-defined application. It has nine positions and each position is assigned to a pre-defined application. The factory set position of the switch is pre-defined application one.

Setting Locking Pad

The setting locking pad on the front panel of the I/O application module enables the setting of the I/O application module by the customer engineering tool.

I/O Module Characteristics

I/O Module Characteristics

General Characteristics

Environmental Characteristics

Conforming to standards

UL 508, UL 60950, IED 60950, 60947-6-2

Certification

cULus, EAC, FCC, CE

Ambient temperature

Storage: -40 to +185°F (-40 to +85°C)
Operation: -13 to +158°F (-25 to +70°C)

Protective Treatment

ULVO, conforming to IEC 60068-2-30

Pollution

Level 3

Mechanical Characteristics

Shock resistance

Conforming to IEC 60068-2-27 15g/11ms, 1/2 sinusoidal

Resistance to sinusoidal vibrations

Conforming to IEC 60068-2-6

Electrical Characteristics

Power Supply

24 Vdc, -20%/+10% (19.2 to 26.4 Vdc)

Consumption

Typical: 24 Vdc, 165 mA at 20°C
Maximum with gateway: 26.4 Vdc,
420 mA at 60°C

Physical Characteristics

Dimensions

2.83 x 4.52 X 2.79 in. (72 x 115 x 71 mm)

Mounting

DIN rail

Weight

0.51 lb. (229.5 g)

Degree of protection of the installed I/O application module

On the front panel (wall mounted enclosure): IP4x
I/O parts: IP3x
Connectors: IP2x

Connections

Screw type terminal blocks

Technical Characteristics
24 Vdc power supply (A)

Power supply type

Regulated switch type

Rated power

72 W

Input voltage

100–120 Vac for single phase
200–500 Vac phase-to-phase maximum

PFC filter

With IEC 61000-3-2

Output voltage

24 Vdc

Power supply out current

3 A

NOTE: It is recommended to use a UL Listed / UL Recognized limited voltage / limited current or a class 2 power supply with a 24 Vdc, 3 A maximum.
  1. 24 Vdc power supply terminal block

  2. Digital input terminal block:

    • 6 inputs, 3 commons and 1 shield

  3. 6 input status LEDs

  4. Analog input status LED

  5. 3 output status LEDs

  6. I/O application module identification labels

  7. Sealable transparent cover

  8. Analog input terminal block

  9. Digital output terminal blocks

  10. ULP status LED

  11. Test/reset button (accessible with cover closed)

  12. Setting locking pad.

  13. Application rotary switch: 1 to 9

  14. Switch for I/O addressing (IO 1 or IO 2)

  15. ULP connectors

Digital Inputs (B)
6 inputs, 3 commons and 1 shield.

Digital input type

Self powered digital input with current limitations as per IEC 61131-2 type 2 standards (7 mA)

Input limit values at state 1 (close)

19.8–25.2 Vdc, 6.1–8.8 mA

Input limit values at state 0 (open)

0–19.8 Vdc, 0 mA

Maximum cable length

33 ft (10 m)

NOTE: For a length greater than 10 m (33 ft) and up to 300 m (1,000 ft), it is mandatory to use a shielded twisted cable. The shield cable is connected to the I/O functional ground of the I/O application module.

Digital Outputs

Digital output type

Bistable relay

Rated load

5 A at 250 Vac

Rated carry current

5 A

Maximum switching voltage

380 Vac, 125 Vdc

Maximum switch current

5 A

Maximum switching power

1250 VA, 150 W

Minimum permissible load

10 mA at 5 Vdc

Contact resistance

30 mΩ

Maximum operating frequency

18000 operations/hr (Mechanical)
1800 operations/hr (Electrical)

Digital output relay protection by an external fuse

External fuse of 5 A or less

Maximum cable length

10 m (33 ft)

Analog Inputs

The I/O application module analog input can be connected to a Pt100 temperature sensor

Range

-22 to 392°F (-30 to 200°C)

Accuracy

-22 to 68°F (-30 to 20°C): ±3.6°F (2°C)
68 to 284°F (20 to 140°C): ±1.8°F (1°C)
284 to 392°F (140 to 200°C): ±3.6°F (2°C)

Refresh interval

5 s

EcoStruxure Power Commission Software

Introduction

EcoStruxure Power Commission is an intuitive, feature-rich tool that can help electrical professionals more effectively and efficiently setup, test and report, commission, and maintain MV/LV circuit breakers and digital switchboards. EcoStruxure Power Commission helps you avoid errors and rework while simplifying your workload. Intuitive, browser-based, you can become proficient with it quickly.

Compatible Devices (Configuration and Device Management)

The software is compatible with a wide range of devices including:

Low Voltage Circuit Breakers:

  • ComPacT NSX/NSXm

  • MasterPacT NT/NW

  • MasterPacT MTZ (IEC and UL)

  • PowerPacT

  • TeSys GV4PB

  • TeSys GV4PEM

Medium Voltage Circuit Breakers

  • BM100

  • PTM100

  • EvoPacT

Download the software from our website:EcoStruxure Power Commission

https://www.se.com/us/en/product-range/62980-ecostruxure-power-commission/#overview

Features

Most of EPC’s features are free to use. The tool provides even more value with the Circuit Breaker Advanced Testing or Switchboard Advanced Commissioning Efficiency modules, which are both accessible through a paid subscription.

With EcoStruxure Power Commission, users can:

  • Discover all connected devices in the electrical panel.

  • Confirm electrical settings and upgrade firmware for power meters and gateways.

  • Test the communication wiring, troubleshoot issues, and generate reports as part of the Factory Acceptance Tests (FAT) or Site Acceptance Tests (SAT).

  • Use batch operations feature to speed up settings configuration for several devices at the same time (in-app purchase).

  • Discover all circuit breakers in the electrical panel.

  • Confirm electrical settings and upgrade firmware for all LV circuit breakers.

  • Test and report on low-voltage circuit breakers and their trip curve behavior during installation and maintenance and generate a report (in-app purchase).

  • Routine checks.

  • Secondary injection testing.

  • Preparation for primary injection testing.

  • Zone selective interlocking testing.

  • Create unique QR codes that identify each switchboard and its installed assets, which enables traceability for product upgrades, recalls, inventory audits, etc.

  • Provide digitized project documentation for your customers retrievable via the switchboard QR code for fast, efficient, and paperless project handover and reference.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.