0611CT1001 R09/24

Energy Management

Energy Management Using the Smart System

Use the Smart System to connect your building to real savings in three steps:

  1. Measure

    Embedded and stand-alone metering and control

  2. Connect

    • Integrated communication interfaces

    • Ready to connect to energy management platforms

  3. Save

    • Data-driven energy efficiency actions

    • Real-time monitoring and control

    • Access to energy and site information through on-line services

Measure

Smart System communications mean visible information.

Grouping most of the electrical protection, command and metering components, the switchboards are now significant sources of data locally displayed and sent via communication networks.

Connect

Smart Systems use reliable, simple-to-install-and-use displays, and Ethernet and Modbus interfaces.

Information is safely transmitted through the most efficient networks:

  • Modbus SL inside switchboards, between components

  • Ethernet, on cable or WiFi, inside the building and connecting switchboards and computers

  • Ethernet or GPRS, for access to on-line services by Schneider Electric

  • Energy experts, no matter where they are located, can now provide advice based on the updated data of the building.

Save

On-Site Real-Time Monitoring

The FDM128 touch screen display connected to the Ethernet:

  • shows essential electrical information and alarms concerning the electrical network

  • allows control (open, close, reset) of various equipment

The FDM128 touch screen provides real-time value checking and control, directly on the front panel of the main switchboard. On a PC display with common browser:

  • shows monitoring web pages hosted into the local Ethernet interface

  • alarm events generate automatic email notifications

  • allows control (open, close, reset) of various equipment

The data is displayed graphically or recorded into files for optimizing the use of energy in the building. As an example, the data can help validate the change of temperature settings, time scheduling in a Building Management System or other automated devices.

On-Line Energy Management Services

StruXureWare Energy Operation automates data collection using an open, scalable, and secure energy management information system.

With the help of the Schneider Electric energy management services team, data is turned into information to enable customers to understand their facilities’ performance on an ongoing basis.

Energy Operation leverages companies’ current investments in their existing systems, and can be used to communicate advanced results and performance to a broad audience for a shared understanding throughout an organization.

Smart System Communication Components

PowerPacT Circuit Breakers with MicroLogic Trip Units

Trip Unit

Ammeter A

  • MicroLogic 5 A selective protection

  • MicroLogic 6 A selective + ground-fault protection

Energy E

  • MicroLogic 5 E selective protection

  • MicroLogic 6 E selective + ground-fault protection

Displays

Power Meter

FDM121

Operating Assistance Functions

FDM128

Power Meter Functions

In addition to protection functions, MicroLogic A/E trip units offer all the functions of Power Meter products as well as operating assistance for the circuit breaker.

MicroLogic A/E trip unit measurement functions are made possible by the MicroLogic trip unit’s intelligence and the accuracy of the sensors. They are handled by a microprocessor that operates independent of protection functions.

Display Functions

MicroLogic Trip Unit LCD

Trip Unit LCD

The user can display all the protection settings and the main measurements on the LCD screen of the trip unit.

  • MicroLogic A trip unit: instantaneous rms current measurements

  • MicroLogic E trip unit: voltage, frequency and power measurements and energy metering, in addition to the measurements offered by MicroLogic A

To make the display available under all conditions and increase operating comfort, an external power supply is recommended for MicroLogic A trip unit. It is required to:

  • display faults and interrupted current measurements

  • use all the functions of MicroLogic E trip unit (such as metering of low power and energy values)

  • ensure operation of the communication network

The external power supply can be shared by several devices. For description, see 24 Vdc Power Supply.

FDM121 Display Unit (One to One)

Display Function

The FDM121 switchboard display unit can be connected to a communication (COM) option (Breaker Communication Module [BSCM]) using a circuit breaker ULP cord to display all measurements on a screen. The LCD screen is 3.78 x 3.78 in. (96 x 96 mm). The FMD121 display unit requires a 24 Vdc power supply. The COM option (BSCM) unit is supplied by the same power supply via the circuit breaker ULP cord connecting it to the FDM121. See FDM121 Display for more information.

FDM121 Display Navigation

FDM121 Display Current

FDM121 Display: Voltage

FDM121 Display: Power

FDM121 Display: Consumption

FDM128 Display Unit (One to Eight)

The FDM128 display unit uses an IFE Ethernet interface for low-voltage circuit breakers.

FDM128 Display Navigation

FDM128 Display Current

FDM128 Display: Voltage

FDM128 Display: Power

FDM128 Display: Consumption

For all FDM, in addition to the information displayed on the MicroLogic trip unit LCD, the FDM screen shows demand, power quality, and maximum/minimum ammeter values along with histories and maintenance indicators.

Measurement Functions

Instantaneous RMS Measurements

Measurement Function

The MicroLogic trip unit continuously displays the RMS value of the highest current of the three phases and neutral (Imax). The navigation buttons can be used to scroll through the main measurements.

In the event of a fault trip, the trip cause is displayed.

The MicroLogic A trip unit measures phase, neutral, and ground fault currents.

MicroLogic E trip units offer voltage, power, frequency, and energy metering in addition to the measurements provided by MicroLogic A trip units.

Maximum / Minimum Ammeter

Every instantaneous measurement provided by MicroLogic A/E trip units can be associated with a maximum/minimum ammeter. The maximum for the highest current of the three phases, neutral, and demand current can be reset using the MicroLogic trip unit keypad, FDM display unit, or the communication system.

Energy Metering

The MicroLogic E trip units also measures the energy consumed since the last reset of the meter. The active energy meter can be reset using the MicroLogic trip unit keypad, the FDM display unit, or the communication system.

Demand and Maximum Demand Values

MicroLogic E trip units also calculate demand current and power values. These calculations can be made using a block or sliding interval that can be set from five to sixty minutes in steps of one minute. The window can be synchronised with a signal sent through the communication system. Whatever the calculation method, the calculated values can be recovered on a PC through the communication network.

Ordinary spreadsheet software can be used to provide trend curves and forecasts based on this data. They provide a basis for load shedding and reconnection operations used to adjust consumption to the subscribed power.

Power Quality

The MicroLogic E trip unit calculates power quality indicators taking into account the presence of harmonics up to the fifteenth harmonic, including the total harmonic distortion (THD) of current and voltage.

MicroLogic 5/6 Trip Units Integrated Power Meter Functions

 

Type

Display

A

E

Trip Unit LCD

Front Display Module

Display of Protection Settings

Pick-ups (A) and delays

All settings can be displayed

Ir, tr, Isd, tsd, Ii, Ig, tg

X

X

X

Instantaneous rms measurements

Currents

Phase and neutral

IA, IB, IC, IN

X

X

X

X

Average of phases

Iavg = (IA + IB + IC) / 3

X

X

X

Highest current of the 3 phases and neutral

Imax of IA, IB, IC, IN

X

X

X

X

Ground fault (MicroLogic 6 trip unit)

% Ig (pick-up setting)

X

X

X

X

Current unbalance between phases

% Iavg

X

X

Voltage

Phase-to-phase

VAB, VBC, VCA

X

X

X

Phase-to-neutral

UAN, UBN, UCN

X

X

X

Average of phase-to-phase voltages

Vavg = (VAB + VAC + VBC) / 3

X

X

Average of phase-to-neutral voltages

Uavg = (UAN + UBN + UCN) / 3

X

X

Ph-Ph and Ph-N voltage unbalance

% Vavg and % Uavg

X

X

Phase sequence

1-2-3, 1-3-2

X

X

X

Frequency (Hz)

Power Systems

f

X

X

X

Power

Active (kW)

P, total/per phase

X

X

X

Reactive (kVAR)

Q, total/per phase

X

X

X

Apparent (kVA)

S, total/per phase

X

X

X

Power factor and cos φ (fundamental)

PF and cos φ, total and per phase

X

X

Maximum, minimum (MAX/MIN)

 

Associated with instantaneous rms measurements

Reset with MicroLogic trip unit or front display module

X

X

X

Energy metering

Energy

Active (kWh), reactive (kVAR), apparent (kVA)

Total since last reset

X

X

X

Absolute or signed mode*

X

X

X

Demand and maximum demand values

Demand current (A)

Phases and neutral

Present value on the selected window

X

X

Maximum demand since last reset

X

X

Demand power

Active (kWh), reactive (kVAR), apparent (kVA)

Present value on the selected window

X

X

Maximum demand since last reset

X

X

Calculation window

 

Adjustable from 5 to 60 minutes in 1 minute steps

X

*

Power quality

Total harmonic distortion THD (%)

Of voltage with respect to rms value

THDU, THDV of the Ph-Ph and Ph-N voltage

X

X

Of current with respect to rms value

THDI of the phase current

X

X

Additional Technical Characteristics

Measurement accuracy of the entire measurement system, including the sensors:

  • Current: +/- 1%

  • Voltage: +/- 0.5%

  • Power and energy: +/- 2%

  • Frequency: +/- 0.1%

Operating-Assistance Functions Characteristics

MicroLogic Trip Unit Alarms with Time-Stamping

Alarm Types

The user can assign an alarm to all MicroLogic A or E trip unit measurements or events:

  • up to 12 alarms can be used together:

  • two alarms are predefined and activated automatically:
    MicroLogic 5 trip unit: overload (Ir)


    MicroLogic 6 trip unit: overload (Ir) and ground fault (Ig)
  • thresholds, priorities and time delays can be set for ten other alarms.

  • the same measurement can be used for different alarms to precisely monitor certain values, e.g. the frequency or the voltage

  • alarms can also be assigned to various states: phase lead/lag, four quadrants, phase sequence selection of display priorities, with screen displaying a window showing high priority alarm

  • alarm time-stamping.

Alarm Settings

Alarms cannot be set using the keypad or the front display module. They are set through the communication network with the PC. Set-up includes the threshold, priority, activation delay before display and deactivation delay. It is also possible to reprogram the standard assignment for the two SDx relay outputs to user-selected alarms.

Alarm Reading

Remote alarm indicators:

  • reading on the front display module or on a PC through the communication network

  • system remote indicators using SDx relay with two output contacts for alarms

  • MicroLogic trip unit built-in LCD display

Histories and Event Tables

MicroLogic A and E trip unit have histories and event tables that are always active.

Three types of time-stamped histories

  • Tripping due to overruns of Ir, Isd, Ii, Ig: last 17 trips

  • Alarms: last 10 alarms

  • Operating events: last 10 events

Each history record is stored with:

  • indicators in clear text in a number of user-selectable languages

  • time-stamping: date and time of event

  • status: pick-up / drop-out

Two types of time-stamped event tables

  • Protection settings

  • Minimums / maximums

Display of alarms and tables

The time-stamped history and event tables may be displayed on a PC through the communication network.

Embedded memory

MicroLogic A and E trip units have a non-volatile memory that saves all data on alarms, histories, event tables, counters and maintenance indicators even if power is lost.

Maintenance Indicators

MicroLogic A and E trip units have indicators for, among others, the number of operating cycles, contact wear and operating times (operating hours counter) of the PowerPacT H-, J-, and L-frame circuit breakers.

It is possible to assign an alarm to the operating cycle counter to plan maintenance. The various indicators can be used together with the trip histories to analyze the level of stresses the device has been subjected to. The information provided by the indicators cannot be displayed on the MicroLogic trip unit LCD. It is displayed on the PC through the communication network.

Management of Installed Devices

Each circuit breaker equipped with a MicroLogic 5 or 6 trip unit can be identified using the communication network:

  • serial number

  • firmware version

  • hardware version

  • device name assigned by the user

This information together with that previously described provides a clear view of the state of the installed devices.

NOTE: Please refer to Display Functions for more details on display formats.

MicroLogic 5/6 Trip Units Operating Assistance Functions

 

Type

Display

A

E

Trip Unit LCD

Front Display Module

Personalized Alarms

Settings

Up to 10 alarms assigned to all A and E measurements

X

X

*

Phase lead/lag, four quadrants, phase sequence, display priority selection

X

*

Display

Alarms and tripping

X

X

*

Remote Indicators

Activation of two dedicated contacts on SDx module

X

X

*

Time-Stamped Histories

Trips (last 17)

Cause of tripping
(time-stamping with ms)

Ir, Isd, Ii (MicroLogic 5, 6 Trip Unit)
Ig (MicroLogic 6 Trip Unit)

X
X

X
X


*
*

Alarms (last 10)

X

X

*

Operating events (last 10)

Event types

Modification of protection setting by rotary switch
Opening of keypad lock
Test using keypad
Test using external tool
Time setting (date and time)
Reset for maximum, minimum and energy meter






X

X
X
X
X
X
X






X

*
*
*
*
*
X

Time Stamping

Presentation

Date and time, text, status

X

X

*

Time-Stamped Event Tables

Protection settings

Setting modified (value displayed)

Ir

tr

Isd

tsd

Ii

Ig

tg

X

X

*

Time-stamping
Previous value

Date and time of modification
Value before modification

X
X

X
X

*

Min/Max

Values monitored

IA

IB

IC

IN

Ii

   

X

X

*

Time-stamping
Previous value

Date and time of min/max record
Min/max value

X
X

X
X

*

Maintenance Indicators

Counter

Mechanical cycles*
Electrical cycles*
Trips
Alarms
Hours

Assignable to an alarm
Assignable to an alarm
One per type of trip
One for each type of alarm
Total operating time (hours)

X

X

*

Indicator

Contact wear

%

X

X

*

Load profile

Hours at different load levels

% of hours in four current ranges: 0–49% In, 50–79% In, 80–89% In and ≥ 90% In

X

X

*

Additional Technical Characteristics:

  • Contact wear
    Each time a PowerPacT H-, J-, or L-frame circuit breaker opens, the MicroLogic 5/6 trip unit measures the interrupted current and increments the contact-wear indicator as a function of the interrupted current, according to test results stored in memory. Breaking under normal load conditions results in a very slight increment. The indicator value may be read on the front display module. It provides an estimation of contact wear calculated on the basis of the cumulative forces affecting the circuit breaker. When the indicator reaches 80%, it is advised to replace the circuit breaker to ensure the availability of the protected equipment.

  • Circuit breaker load profile
    MicroLogic 5/6 trip units calculate the load profile of the circuit breaker protecting a load circuit. The profile indicates the percentage of the total operating time at four current levels (% of In):

    • 0 to 49% In

    • 50 to 79% In

    • 80 to 89% In

    • ≥ 90% In

  • This information can be used to optimize use of the protected devices or to plan ahead for expansion.

Motor Circuit Protectors (AC Only)

See Motor Circuit Protection for information about PowerPacT H-, J- and L-frame electronic motor circuit protectors (MCP) with trip units:

MicroLogic 1.3 M

MicroLogic 2 M

FDM121 Display

MicroLogic trip unit measurement capabilities come into full play with the FDM121 display. It connects with a circuit breaker ULP cord and displays the MicroLogic trip unit information. The result is a true integrated unit combining a circuit breaker and a power meter. Additional operating assistance functions can also be displayed.

An FDM121 display unit can be connected to ULP communication devices using a prefabricated cord to display all measurements, alarms, histories and event tables, maintenance indicators, and management of installed devices on a screen.

The FMD121 display unit requires a 24 Vdc power supply.

The FDM121 is a display that can be integrated with the PowerPacT H/J/L/P/R or MasterPacT NW/NT circuit breaker systems. It uses the sensors and processing capacity of the MicroLogic trip unit. It is easy to use and requires no special software or settings. It is immediately operational when connected to the circuit breaker by a ULP cord.

It also provides monitoring and control with the use of the I/O application module, the motor mechanism module, or the circuit breaker communication module.

The FDM121 has a large display, but requires very little depth. The anti-glare graphic screen is backlit for very easy reading even under poor ambient lighting and at sharp angles.

Display of MicroLogic Trip Unit Measurements and Alarms

The FDM121 is intended to display MicroLogic trip unit measurements, alarms and operating information. It cannot be used to modify the protection settings.

Measurements can be easily accessed using a menu. All user-defined alarms are automatically displayed. The display mode depends on the priority level selected during alarm set-up:

  • high priority: a pop-up window displays the time-stamped description of the alarm and the orange Alarm LED flashes;

  • medium priority: the orange Alarm LED goes continuously on;

  • low priority: no display on the screen.

All detected faults resulting in a trip automatically produce a high-priority alarm, without any special settings required. In all cases, the alarm history is updated. The MicroLogic trip unit saves the information in its non-volatile memory in the event of an FDM121 power loss.

Status Indications and Remote Control

FDM121 Display

Surface Mount Accessory

When the circuit breaker is equipped with the Breaker Communications Module (BSCM), the FDM121 display can also be used to view circuit breaker status conditions:

  • O/F: ON/OFF

  • SD: trip indication

  • SDE: fault-trip indication (overload, short-circuit, or ground fault).

When the circuit breaker system is equipped with the I/O application module, the FDM121 can monitor and control:

  • cradle management

  • circuit breaker operation

  • light and load control

  • custom applications.

When the circuit breaker is equipped with the communication motor operator etc., the FDM121 display can also be used to control (open/close) the circuit breaker.

Two operating mode are available:

  • local mode: open/close commands are enabled from the FDM121 while disabled from the communication network;

  • remote mode: open/close commands are disabled from the FDM121 while enabled from the communication network.

Main Characteristics

Connection with FDM121 Display Unit

  • A 3.78 x 3.78 x 1.18 in. (96 x 96 x 30 mm) screen requiring 0.39 in. (10 mm) behind the door (or 0.79 in. [20 mm] when the 24 V power supply connector is used)

  • White backlighting

  • Wide viewing angle: vertical ±60°, horizontal ±30°

  • High resolution: excellent reading of graphic symbols

  • Alarm LED: flashing orange for alarm pick-up, steady orange after operator reset if the alarm condition persists

  • Operating temperature range: +14°F (-10°C) to +131°F (+55°C)

  • CE / UL / CSA marking

  • 24 Vdc power supply, with tolerances: 24 V -20% (19.2 V) to 24 V +10%
    (26.4 V)

When the FDM121 is connected to the communication network, the 24 Vdc can be supplied by the communication system wiring system. Consumption is 40 mA.

Mounting

The FDM121 is easily installed in a switchboard.

  • Standard door cut-out is 3.6 x 3.6 in. (92 x 92 mm).

  • Attached using clips.

To avoid a cut-out in the door, an accessory is available for surface mounting by drilling only two 0.87 in. (22 mm) diameter holes.

Connection

The FDM121 is equipped with a 24 Vdc terminal block:

  • A plug-in type terminal block with two wire inputs per point for easy daisy-chaining.

  • A power supply range of 24 Vdc -20% (19.2 V) to 24 Vdc +10% (26.4 V).
    A 24 Vdc type auxiliary power supply must be connected to a single point on the ULP system. The FDM121 display has a two-point screw connector on the rear panel of the module for this purpose. The ULP module to which the auxiliary power supply is connected distributes the supply via the ULP cable to all the ULP modules connected to the system and therefore also to MicroLogic trip unit. See wiring diagram later in this section.

  • Two RJ45 jacks.

The MicroLogic trip unit connects to the internal communication terminal block on the PowerPacT or ComPacT circuit breaker with the circuit breaker ULP cord. Connection to one of the RJ45 connectors on the FDM121 automatically establishes communication between the MicroLogic trip unit and the FDM121 and supplies power to the MicroLogic trip unit measurement functions. When the second connector is not used, it must be fitted with a line terminator.

Navigation

Five buttons are used for intuitive and fast navigation. The “Context” button may be used to select the type of display (digital, bar graph, analog). The user can select the display language (Chinese, English, French, German, Italian, Portuguese, Spanish, etc.).

1 Escape

2 Down

3 OK

4 Up

5 Context

6 Alarm LED

 

Product Identification

Metering: Submenu

Metering: Meter

 

Services

Screens

Main Menu

When powered up, the FDM121 screen automatically displays the ON/OFF status of the device.

Quick View Metering Control Alarms Services

When not in use, the screen is not backlit. Backlighting can be activated by pressing one of the buttons. It goes off after three minutes.

Access to Essential Information

  • “Quick view” provides access to five screens that display a summary of essential operating information (I, U-V, f, P, E, THD, circuit breaker ON/OFF).

Access to Detailed Information

  • “Metering” can be used to display the measurement data (I, U-V, f, P, Q, S, E, THD, PF) with the corresponding min/max values.

  • “Alarms” displays active alarms and the alarm history.

  • “Services” provides access to the operation counters, energy and maximum ammeter reset function, maintenance indicators, identification of modules connected to the internal bus, and FDM121 internal settings (language, contrast, etc.).

Communication Components and FDM121 Connections

The FDM121 degree of protection is IP54 in front. IP54 is maintained after switchboard mounting by using the supplied gasket during installation.

FDM121 Connections

FDM128 Display

The MicroLogic trip unit measurement capabilities are fully utilized with the FDM128 display. The FDM128 display connects to Ethernet communication using the RJ45 port and displays MicroLogic trip unit information. The result is an integrated unit combining a circuit breaker with a power meter. Additional operating assistance functions can also be displayed.

The FDM128 display unit can be connected to a MicroLogic COM option (BSCM). It uses the sensors and processing capacity of the MicroLogic trip unit and requires no special software or settings. The FDM128 is a large display, but requires very little depth. The anti-glare graphic screen is backlit for easy reading even under poor ambient lighting and at sharp angles.

The FDM128 display is designed to manage up to eight devices (PowerPacT H/J/L/P/R or MasterPacT NW/NT circuit breakers).

Display of MicroLogic Trip Unit Measurements and Trips

The FDM128 is intended to display MicroLogic 5/6 trip unit measurements, trips, and operating information. It cannot be used to modify the protection settings.

  • Measurements may be easily accessed using a menu.

  • Trips are automatically displayed.

  • A pop-up window displays the time-stamped description of the trip.

Status Indications

When the circuit breaker is equipped with the COM option (BSCM) (including its set of sensors) the FDM128 display can also be used to view circuit breaker status conditions:

  • O/F: ON/OFF

  • SDE: Fault-trip indication (overload, short-circuit, ground fault)

  • CE, CD, CT cradle management with I/O application module.

Remote Control

When the circuit breaker is equipped with the COM option (BSCM) (including connection to a communicating motor operator), the FDM128 display can also be used to operate (open/close) the circuit breaker.

Two operating mode are available:

  • Local mode: open/close commands are enabled from the FDM128 while disabled from the communication network.

  • Remote mode: open/close commands are disabled from the FDM128 while enabled from the communication network.

Main Characteristics

FDM128 Display

  • 4.54 x 3.40 in. (115.2 x 86.4 mm) with 5.7 in. (145 mm) QVGA display 320 x 240 pixels.

  • Color TFT LCD, with LED backlight.

  • Wide viewing angle: vertical ±80°, horizontal ±70°.

  • High resolution: excellent reading of graphic symbols.

  • Operating temperature range: +14°F (-10°C) to +131°F (+55°C).

  • CE / UL / CSA marking.

  • 24 Vdc power supply, -10%/+20% (limit 20.4 - 28.8 Vdc).

  • Consumption 6.8 W.

Mounting

Surface Mount Accessory

The FDM128 is easily installed in a switchboard.

  • Standard door hole Ø 0.87 in. (22 mm).

  • The FDM128 degree of protection is IP65 at the touch screen cover. IP54 is maintained after installation by using the supplied gasket.

Connection

Connection with Display Unit

The FDM128 is equipped with:

  • a 24 Vdc terminal block:

    • with a power supply range of 24 Vdc (limit 20.4 - 28.8 Vdc).

    • secures to the FDM128 display unit using a 2-point screw connector on the rear panel of the module.

  • one RJ45 Ethernet jack.

The MicroLogic trip unit connects to the internal communication terminal block on the PowerPacT circuit breakers through the circuit breaker ULP cord and Ethernet connection through the IFE.

Navigation

  • A touch screen is used for intuitive and fast navigation.

  • The user can select the display language (Chinese, English, French, German, Italian, Portuguese, Spanish, etc.).

Product Identification

Metering: Meter

Services

Screens

Main Menu

Quick View Metering Control Alarms Services

When not in use, the screen is automatically shifted to low back-lighting.

Fast Access to Essential Information

  • “Quick view” provides access to five screens that display a summary of essential operating information (I, U-V, f, P, E, THD, circuit breaker On / Off).

Access to Detailed Information

  • "Metering" can be used to display the measurement data (I, U-V, f, P, Q, S, E, THD, PF) with the corresponding min/max values.

  • “Alarms” displays the trip history.

  • “Services” provides access to the operation counters, energy and maximum ammeter reset function, maintenance indicators, identification of modules connected to the internal bus and FDM128 internal settings (language, contrast, etc.).

Communication Components and FDM128 Connections

The FDM128 degree of protection is IP65 at the touch screen cover. IP54 is maintained after installation by using the supplied gasket.

FDM128 Connections

Panelboard and Switchboard Connections

Smart System Communication Devices and Displays

 

Name

Function

Port

Bin.
Input

Analog
Input

Bin.
Output

To Device

To Server

A

Panel Server

All-in-one gateway to retrieve data, connect edge software, or cloud applications.

Modbus Client

Ethernet Cable + WiFI

2

B

FDM128

Ethernet LCD Color Touch Screen

Ethernet

C

FDM121

LCD Display for Circuit Breaker

ULP

D

IFE Interface + Gateway

Ethernet Interface & Gateway

Modbus Client & ULP

Ethernet

IFE Interface

Ethernet Interface for Circuit Breakers

ULP

Ethernet

E

IFM

Modbus Interface for Circuit Breakers

ULP

Modbus Server

F

I/O

Input/Output Application Module for Circuit Breakers

ULP

ULP

6

1

1

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.