0611CT1001 R09/24

Circuit Breakers

Dual-Break Rotating Contacts

All PowerPacT H-, J-, and L-frame circuit breakers are equipped with dual-break rotating contacts that reduce the amount of peak current during a short-circuit fault. This reduces the let-through currents and enhances equipment protection.

Reduced Let-Through Currents

The moving contact has the shape of an elongated “S” and rotates around a floating axis. The shape of the fixed and moving contacts are such that the repelling forces appear as soon as the circuit reaches approximately 15 times In. Due to the rotating movement, repulsion is rapid and the device greatly limits short-circuit currents, whatever the interrupting level of the unit (D, G, J or L). The fault current is extinguished before it can fully develop. Lower let-through currents provide less peak energy, reducing the required busbar bracing, lowering enclosure pressure, and delivering improved series or combination ratings. See Current-Limiting.

High Ampere Interrupting Ratings (AIR)

Circuit breakers are available with interrupting ratings up to:

  • 200 kA at 240 Vac delta

  • 200 kA at 480 Vac delta

  • 100 kA at 600 Vac delta.

See Interrupting Rating for additional performance levels.

Internal Operating Mechanism

Push-to-Trip

PowerPacT H-, J-, and L-frame circuit breakers have an over-center toggle mechanism providing quick-make, quick-break operation. The operating mechanism is also trip-free, which allows tripping even when the circuit breaker handle is held in the “ON” position. Internal cross-bars provide common opening and closing of all poles with a single operating handle.

All PowerPacT circuit breakers have an integral push-to-trip button in the cover to manually trip the circuit breaker. This should be used as part of a regular preventive maintenance program.

Handle Position Indication

The circuit breaker handle can assume any of three positions, ON, tripped or OFF as shown. The center tripped position provides positive visual indication that the circuit breaker has tripped.

The circuit breaker can be reset by first pushing the handle to the extreme “OFF” position. Power can then be restored to the load by pushing the handle to the “ON” position.

Visi-Trip Breaker Locator

Provides a visual light alert when a breaker may require attention.

The Visi-Trip LED handle aids in quickly locating a circuit breaker that requires attention. Inspect the handle position for circuit breaker trip indication. The VisiTrip handle will flash an LED light as described in the table below.

Wait five seconds between handle operation and push-to-trip button operation to ensure that the Visi-Trip handle is in standby. Tripping the circuit breaker too soon after toggling may result in the Visi-Trip handle not operating as intended. If a nuisance LED flashing occurs, it can be reset by toggling the circuit breaker. If toggling the circuit breaker is not desired, LED flashing will reset after six hours. When performing annual maintenance in accordance with MCCB Field Testing and Maintenance Guide (0600IB1201), operate the push to trip button (if equipped) to verify the Visi-Trip functionality. Cycle the circuit breaker from tripped to OFF, and then from OFF to ON and take note of the battery health.

Light Pattern

Indicator

Fast flash for two seconds.

Battery low (20% remaining)*

Long duration slow flash (continuous flash up to for six hours).

The circuit breaker required inspection.

Circuit Breaker Ratings

The interrupting rating is the highest current at rated voltage the circuit breaker is designed to safely interrupt under standard test conditions. Circuit breakers must be selected with interrupting ratings equal to or greater than the available short-circuit current at the point where the circuit breaker is applied to the system (unless it is a branch device in a series rated combination). Interrupting ratings are shown on Interrupting Rating and on the faceplate label on the front of the circuit breaker.

Reverse Feeding of Circuit Breakers

The standard unit-mount H-, J-, and L-frame circuit breakers have sealed trip units and may be reverse fed. For catalog numbers, refer to the following tables:

Circuit breakers with field-interchangeable trip units (designated by the suffix T or R and labeled “LINE” and “LOAD”) cannot be reverse fed. Neither can circuit breaker frames without terminations or trip units.

Current-Limiting

The current-limiting attributes of PowerPacT H-, J-, and L-frame circuit breakers provide greater protection for downstream devices by limiting the let-through current in the event of a fault. The current-limiting capabilities of HJ/HL/HR, JJ/JL/JR, and LJ/LL/LR frame circuit breakers are documented with Underwriters Laboratories and Canadian Standards Association. These current-limiting circuit breakers ship with a label that identifies them as UL/CSA Current-Limiting Circuit Breakers. (The HD/HG, JD/JG, and LD/LG circuit breakers do not carry the UL Current-Limiting label).

The trip curves with let-through data are available in the trip curve section in this catalog, see Trip Curves.

Please note that as let-through curves for UL Listed / CSA Certified Current-Limiting Circuit Breakers, these curves are maximum let-through values.

100% Rated

Some models of the H-, J-, and L-frame circuit breakers are UL Listed / CSA Certified to be applied at up to 100% of their current rating. Because of the additional heat generated, the use of specially-designed enclosures on H- and J-frame circuit breakers and 194°F (90°C) rated wire is required when applying circuit breakers at 100% of continuous current rating. (H-, J-, and L-frame circuit breakers can use aluminum or copper lugs.) Markings on the circuit breaker indicate the minimum enclosure size and ventilation required. The 194°F (90°C) wire must be sized according to the ampacities of the 167°F (75°C) wire column in the NEC. Circuit breakers with 100% rating can also be used in applications requiring only standard (80%) continuous loading.

100% ratings are valid for:

  • Three-pole H/J-frame unit mount and busbar connection

  • Three- pole/four-pole L-frame 250 A and 400 A unit mount

  • Three-pole L-frame 250 A and 400 A I-Line

  • Rear connection and switches

Corner-Grounded Delta Ratings (1Ø-3Ø)

Circuit breakers suitable for corner-grounded circuits are marked 1Ø-3Ø. For additional information, refer to data bulletin 2700DB0202, Corner-Grounded Delta (Grounded B Phase) Systems.

Corner-Grounded Delta Ratings (1Ø-3Ø)

 

Two-Pole H-Frame

Two-Pole J-Frame

 

HD

HG

HJ*

HL*

HR*

JD*

JG*

JJ*

JL*

JR*

Ampere Rating (A)

15–150

150–250

Voltage Rating (Vac)

240

240

UL Interrupting Rating (kA)

42

42

65

100

42

42

65

100

Three-Phase 240 Vac Corner-Grounded Delta System

Special Applications

Protection of Industrial Control Panels

PowerPacT H-, J-, and L-frame circuit breakers are also used in industrial control panels. They serve as incoming devices or can be combined with contactors to protect motor feeders:

  • compliance with worldwide standards including IEC 60947-2 and UL 508 / CSA C22.2 N°14

  • overload and short-circuit protection

  • installation in universal and functional type

PowerPacT H-, J-, and L-frame circuit breakers equipped for motor protection functions as described in the following pages can be used in industrial control panels. The accessories for the PowerPacT H-, J-, and L-frame circuit breakers are suitable for the special needs of these applications

400 Hz Applications

Impact on Protective Devices

The current in 400 Hz systems has higher losses caused by eddy currents and an increase in the skin effect (reduction in the useful cross-sectional area of conductors). The higher losses cause additional temperature rise in circuit breakers subjected to the higher frequency current. To remain within the rated temperature-rise limits of devices, current derating is required. For circuit breakers equipped with MicroLogic electronic trip units, only the current rating (Ir) must be derated. See “Current Derating Maximum Ir Setting” below. On circuit breakers equipped with thermal-magnetic trip units, the current rating (In) must be derated and the magnetic trip setting Im must be increased. See “Current Rating (In) and Magnetic Trip Setting (Im) Rerating” below.

Breaking Capacity in 400 Hz, 480 V Systems

The power levels of 400 Hz applications rarely exceed a few hundred kW with relatively low short-circuit currents, generally not exceeding four times the rated current

Circuit Breaker

Max. Breaking Capacity AIR at 400 Hz

H-frame

10 kA

J-frame

10 kA

L-frame

10 kA

MicroLogic Electronic Trip Units

MicroLogic 3.2/3, 5.2/3 A or E and 6.2/3 with A or E measurement functions are suitable for 400 Hz. The use of electronics offers the advantage of greater operating stability when the frequency varies. However the units are still subject to temperature rise caused by the frequency.

The practical consequences are:

Current Derating Maximum Ir Setting

Circuit Breaker

Maximum Setting Coefficient

Max Ir Setting at 400 Hz

H-frame, 150 A

0.9

135

J-frame, 250 A

0.9

225

L-frame, 400 A

0.8

320

L-frame, 600 A

0.65

390

Thermal-Magnetic Trip Units

Thermal-magnetic trip units require the current rating (In) to be derated and the magnetic trip setting (Im) to be increased.

Current Rating (In) and Magnetic Trip Setting (Im) Rerating

Circuit Breaker

Maximum Setting Coefficient

Max Ir Setting at 400 Hz

Magnetic Im Coefficient at 400 Hz

H-frame, 150 A

0.9

135

1.6

J-frame, 250 A

0.9

225

1.6

L-frame, 400 A

0.8

320

1.6

L-frame, 600 A

0.65

390

1.6

Auxiliary Switch (OF) in 400 Hz Networks

Electrical Characteristics of Auxiliary Switches

Contact

Standard

Low Level

Utilization cat. (IEC 60947-5-1)

AC12

AC15

AC12

AC15

Operational current

24 V

6 A

6 A

5 A

3 A

40 V

6 A

6 A

5 A

3 A

110 V

6 A

5 A

5 A

2.5 A

200/240 V

6 A

4 A

5 A

2 A

380/415 V

6 A

2 A

5 A

1.5 A

Shunt Trip (MX) or Undervoltage Trip (MN) Voltage Release
at 400 Hz and 440 V

For circuit breakers on 400 Hz systems, only 125 Vdc undervoltage trip (MN) or shunt trip (MX) releases may be used. The release must be supplied by the 400 Hz system through a rectifier bridge (to be selected from the table below) and an additional resistor with characteristics depending on the system voltage.

Rectifier Bridges for MN or MX Releases

Voltage

Rectifier

Additional Resistor

220/240 V

Thomson 110 BHz or
General Instrument W06 or
Semikron SKB at 1.2/1.3

4.2 k -5 W

380/240 V

Semikron SKB at 1.2/1.3

10.7 k -10 W

H- and J-Frame Catalog Numbers

Unit-Mount Circuit Breaker Catalog Numbers

PowerPacT H-Frame Standard (80%) Rated 150 A Unit-Mount Thermal-Magnetic Circuit Breakers (600 Vac, 250 Vdc) with Factory-Sealed Trip Unit (Suitable for Reverse Connection)

Current Rating at
104°F (40°C)*

Fixed AC Magnetic Trip

Interrupting Rating

Hold

Trip

D

G

J*

L*

H-Frame, 150 A, Two-Pole, 600 Vac 50/60 Hz, 250 Vdc*

15 A 350 A 750 A

HDL26015

HGL26015

HJL26015

HLL26015

20 A 350 A 750 A

HDL26020

HGL26020

HJL26020

HLL26020

25 A 350 A 750 A

HDL26025

HGL26025

HJL26025

HLL26025

30 A 350 A 750 A

HDL26030

HGL26030

HJL26030

HLL26030

35 A 400 A 850 A

HDL26035

HGL26035

HJL26035

HLL26035

40 A 400 A 850 A

HDL26040

HGL26040

HJL26040

HLL26040

45 A 400 A 850 A

HDL26045

HGL26045

HJL26045

HLL26045

50 A 400 A 850 A

HDL26050

HGL26050

HJL26050

HLL26050

60 A 800 A 1450 A

HDL26060

HGL26060

HJL26060

HLL26060

70 A 800 A 1450 A

HDL26070

HGL26070

HJL26070

HLL26070

80 A 800 A 1450 A

HDL26080

HGL26080

HJL26080

HLL26080

90 A 800 A 1450 A

HDL26090

HGL26090

HJL26090

HLL26090

100 A 900 A 1700 A

HDL26100

HGL26100

HJL26100

HLL26100

110 A 900 A 1700 A

HDL26110

HGL26110

HJL26110

HLL26110

125 A 900 A 1700 A

HDL26125

HGL26125

HJL26125

HLL26125

150 A 900 A 1700 A

HDL26150

HGL26150

HJL26150

HLL26150

H-Frame, 150 A, Three-Pole, 600 Vac 50/60 Hz, 250 Vdc

15 A 350 A 750 A

HDL36015

HGL36015

HJL36015

HLL36015

20 A 350 A 750 A

HDL36020

HGL36020

HJL36020

HLL36020

25 A 350 A 750 A

HDL36025

HGL36025

HJL36025

HLL36025

30 A 350 A 750 A

HDL36030

HGL36030

HJL36030

HLL36030

35 A 400 A 850 A

HDL36035

HGL36035

HJL36035

HLL36035

40 A 400 A 850 A

HDL36040

HGL36040

HJL36040

HLL36040

45 A 400 A 850 A

HDL36045

HGL36045

HJL36045

HLL36045

50 A 400 A 850 A

HDL36050

HGL36050

HJL36050

HLL36050

60 A 800 A 1450 A

HDL36060

HGL36060

HJL36060

HLL36060

70 A 800 A 1450 A

HDL36070

HGL36070

HJL36070

HLL36070

80 A 800 A 1450 A

HDL36080

HGL36080

HJL36080

HLL36080

90 A 800 A 1450 A

HDL36090

HGL36090

HJL36090

HLL36090

100 A 900 A 1700 A

HDL36100

HGL36100

HJL36100

HLL36100

110 A 900 A 1700 A

HDL36110

HGL36110

HJL36110

HLL36110

125 A 900 A 1700 A

HDL36125

HGL36125

HJL36125

HLL36125

150 A 900 A 1700 A

HDL36150

HGL36150

HJL36150

HLL36150

PowerPacT H-Frame 100% Rated 150 A Unit-Mount Thermal-Magnetic Circuit Breakers (600 Vac, 250 Vdc) with Factory-Sealed Trip Unit (Suitable for Reverse Connection)

Current Rating at
104°F (40°C)*

Fixed AC Magnetic Trip

Interrupting Rating

Hold

Trip

D

G

J*

L*

H-Frame, 150 A, Two-Pole, 600 Vac 50/60 Hz, 250 Vdc*

15 A

350 A

750 A

HDL26015C

HGL26015C

HJL26015C

HLL26015C

20 A

350 A

750 A

HDL26020C

HGL26020C

HJL26020C

HLL26020C

25 A

350 A

750 A

HDL26025C

HGL26025C

HJL26025C

HLL26025C

30 A

350 A

750 A

HDL26030C

HGL26030C

HJL26030C

HLL26030C

35 A

400 A

850 A

HDL26035C

HGL26035C

HJL26035C

HLL26035C

40 A

400 A

850 A

HDL26040C

HGL26040C

HJL26040C

HLL26040C

45 A

400 A

850 A

HDL26045C

HGL26045C

HJL26045C

HLL26045C

50 A

400 A

850 A

HDL26050C

HGL26050C

HJL26050C

HLL26050C

60 A

800 A

1450 A

HDL26060C

HGL26060C

HJL26060C

HLL26060C

70 A

800 A

1450 A

HDL26070C

HGL26070C

HJL26070C

HLL26070C

80 A

800 A

1450 A

HDL26080C

HGL26080C

HJL26080C

HLL26080C

90 A

800 A

1450 A

HDL26090C

HGL26090C

HJL26090C

HLL26090C

100 A

900 A

1700 A

HDL26100C

HGL26100C

HJL26100C

HLL26100C

110 A

900 A

1700 A

HDL26110C

HGL26110C

HJL26110C

HLL26110C

125 A

900 A

1700 A

HDL26125C

HGL26125C

HJL26125C

HLL26125C

150 A

900 A

1700 A

HDL26150C

HGL26150C

HJL26150C

HLL26150C

H-Frame, 150 A, Three-Pole, 600 Vac 50/60 Hz, 250 Vdc

15 A

350 A

750 A

HDL36015C

HGL36015C

HJL36015C

HLL36015C

20 A

350 A

750 A

HDL36020C

HGL36020C

HJL36020C

HLL36020C

25 A

350 A

750 A

HDL36025C

HGL36025C

HJL36025C

HLL36025C

30 A

350 A

750 A

HDL36030C

HGL36030C

HJL36030C

HLL36030C

35 A

400 A

850 A

HDL36035C

HGL36035C

HJL36035C

HLL36035C

40 A

400 A

850 A

HDL36040C

HGL36040C

HJL36040C

HLL36040C

45 A

400 A

850 A

HDL36045C

HGL36045C

HJL36045C

HLL36045C

50 A

400 A

850 A

HDL36050C

HGL36050C

HJL36050C

HLL36050C

60 A

800 A

1450 A

HDL36060C

HGL36060C

HJL36060C

HLL36060C

70 A

800 A

1450 A

HDL36070C

HGL36070C

HJL36070C

HLL36070C

80 A

800 A

1450 A

HDL36080C

HGL36080C

HJL36080C

HLL36080C

90 A

800 A

1450 A

HDL36090C

HGL36090C

HJL36090C

HLL36090C

100 A

900 A

1700 A

HDL36100C

HGL36100C

HJL36100C

HLL36100C

110 A

900 A

1700 A

HDL36110C

HGL36110C

HJL36110C

HLL36110C

125 A

900 A

1700 A

HDL36125C

HGL36125C

HJL36125C

HLL36125C

150 A

900 A

1700 A

HDL36150C

HGL36150C

HJL36150C

HLL36150C

PowerPacT J-Frame Standard (80%) Rated 250 A Unit-Mount Thermal-Magnetic Circuit Breakers with Factory-Sealed Trip Unit (Suitable for Reverse Connection)

Current Rating at 104°F (40°C)

Adjustable AC Magnetic Trip

Interrupting Rating

Hold

Trip

D

G

J*

L*

R*

J-Frame, 250 A, Two-Pole, 600 Vac 50/60 Hz, 250 Vdc

150 A*

750 A

1500 A

JDL26150

JGL26150

JJL26150

JLL26150

175 A*

875 A

1750 A

JDL26175

JGL26175

JJL26175

JLL26175

200 A*

1000 A

2000 A

JDL26200

JGL26200

JJL26200

JLL26200

225 A*

1125 A

2250 A

JDL26225

JGL26225

JJL26225

JLL26225

250 A*

1250 A

2500 A

JDL26250

JGL26250

JJL26250

JLL26250

J-Frame, 250 A, Three-Pole, 600 Vac 50/60 Hz, 250 Vdc

150 A*

750 A

1500 A

JDL36150

JGL36150

JJL36150

JLL36150

JRL36150

175 A*

875 A

1750 A

JDL36175

JGL36175

JJL36175

JLL36175

JRL36175

200 A*

1000 A

2000 A

JDL36200

JGL36200

JJL36200

JLL36200

JRL36200

225 A*

1125 A

2250 A

JDL36225

JGL36225

JJL36225

JLL36225

JRL36225

250 A*

1250 A

2500 A

JDL36250

JGL36250

JJL36250

JLL36250

JRL36250

PowerPacT J-Frame 100% Rated 250 A Unit-Mount Thermal-Magnetic Circuit Breakers with Factory-Sealed Trip Unit (Suitable for Reverse Connection)

Current Rating at
104°F (40°C)

Adjustable AC Magnetic Trip

Interrupting Rating

Hold

Trip

D

G

J*

L*

R*

J-Frame, 250 A, Two-Pole, 600 Vac 50/60 Hz, 250 Vdc

150 A*

750 A

1500 A

JDL26150C

JGL26150C

JJL26150C

JLL26150C

175 A*

875 A

1750 A

JDL26175C

JGL26175C

JJL26175C

JLL26175C

200 A*

1000 A

2000 A

JDL26200C

JGL26200C

JJL26200C

JLL26200C

225 A*

1125 A

2250 A

JDL26225C

JGL26225C

JJL26225C

JLL26225C

250 A*

1250 A

2500 A

JDL26250C

JGL26250C

JJL26250C

JLL26250C

J-Frame, 250 A, Three-Pole, 600 Vac 50/60 Hz, 250 Vdc

150 A*

750 A

1500 A

JDL36150C

JGL36150C

JJL36150C

JLL36150C

JRL36150C

175 A*

875 A

1750 A

JDL36175C

JGL36175C

JJL36175C

JLL36175C

JRL36175C

200 A*

1000 A

2000 A

JDL36200C

JGL36200C

JJL36200C

JLL36200C

JRL36200C

225 A*

1125 A

2250 A

JDL36225C

JGL36225C

JJL36225C

JLL36225C

JRL36225C

250 A*

1250 A

2500 A

JDL36250C

JGL36250C

JJL36250C

JLL36250C

JRL36250C

H-Frame 150 A and J-Frame 250 A Electronic Trip UL Rated Circuit Breakers (600 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating

Type

Function

Trip Unit

D

G

J*

L*

R*

Standard (80%) Rated Circuit Breakers, Three-Pole

Standard

LI

3.2*

60 A*

HDL36060U31X

HGL36060U31X

HJL36060U31X

HLL36060U31X

HRL36060U31X

100 A*

HDL36100U31X

HGL36100U31X

HJL36100U31X

HLL36100U31X

HRL36100U31X

150 A*

HDL36150U31X

HGL36150U31X

HJL36150U31X

HLL36150U31X

HRL36150U31X

250 A*

JDL36250U31X

JGL36250U31X

JJL36250U31X

JLL36250U31X

JRL36250U31X

Standard

LSI

3.2S*

60 A*

HDL36060U33X

HGL36060U33X

HJL36060U33X

HLL36060U33X

HRL36060U33X

100 A*

HDL36100U33X

HGL36100U33X

HJL36100U33X

HLL36100U33X

HRL36100U33X

150 A*

HDL36150U33X

HGL36150U33X

HJL36150U33X

HLL36150U33X

HRL36150U33X

250 A*

JDL36250U33X

JGL36250U33X

JJL36250U33X

JLL36250U33X

JRL36250U33X

Ammeter

LSI

5.2A

60 A*

HDL36060U43X

HGL36060U43X

HJL36060U43X

HLL36060U43X

HRL36060U43X

100 A*

HDL36100U43X

HGL36100U43X

HJL36100U43X

HLL36100U43X

HRL36100U43X

150 A*

HDL36150U43X

HGL36150U43X

HJL36150U43X

HLL36150U43X

HRL36150U43X

250 A*

JDL36250U43X

JGL36250U43X

JJL36250U43X

JLL36250U43X

JRL36250U43X

Energy

LSI

5.2E

60 A*

HDL36060U53X

HGL36060U53X

HJL36060U53X

HLL36060U53X

HRL36060U53X

100 A*

HDL36100U53X

HGL36100U53X

HJL36100U53X

HLL36100U53X

HRL36100U53X

150 A*

HDL36150U53X

HGL36150U53X

HJL36150U53X

HLL36150U53X

HRL36150U53X

250 A*

JDL36250U53X

JGL36250U53X

JJL36250U53X

JLL36250U53X

JRL36250U53X

Ammeter

LSIG

6.2A

60 A*

HDL36060U44X

HGL36060U44X

HJL36060U44X

HLL36060U44X

HRL36060U44X

100 A*

HDL36100U44X

HGL36100U44X

HJL36100U44X

HLL36100U44X

HRL36100U44X

150 A*

HDL36150U44X

HGL36150U44X

HJL36150U44X

HLL36150U44X

HRL36150U44X

250 A*

JDL36250U44X

JGL36250U44X

JJL36250U44X

JLL36250U44X

JRL36250U44X

Energy

LSIG

6.2E

60 A*

HDL36060U54X

HGL36060U54X

HJL36060U54X

HLL36060U54X

HRL36060U54X

100 A*

HDL36100U54X

HGL36100U54X

HJL36100U54X

HLL36100U54X

HRL36100U54X

150 A*

HDL36150U54X

HGL36150U54X

HJL36150U54X

HLL36150U54X

HRL36150U54X

250 A*

JDL36250U54X

JGL36250U54X

JJL36250U54X

JLL36250U54X

JRL36250U54X

100% Rated Circuit Breakers, Three-Pole

Standard

LI

3.2*

60 A*

HDL36060CU31X

HGL36060CU31X

HJL36060CU31X

HLL36060CU31X

HRL36060CU31X

100 A*

HDL36100CU31X

HGL36100CU31X

HJL36100CU31X

HLL36100CU31X

HRL36100CU31X

150 A*

HDL36150CU31X

HGL36150CU31X

HJL36150CU31X

HLL36150CU31X

HRL36150CU31X

250 A*

JDL36250CU31X

JGL36250CU31X

JJL36250CU31X

JLL36250CU31X

JRL36250CU31X

Standard

LSI

3.2S*

60 A*

HDL36060CU33X

HGL36060CU33X

HJL36060CU33X

HLL36060CU33X

HRL36060CU33X

100 A*

HDL36100CU33X

HGL36100CU33X

HJL36100CU33X

HLL36100CU33X

HRL36100CU33X

150 A*

HDL36150CU33X

HGL36150CU33X

HJL36150CU33X

HLL36150CU33X

HRL36150CU33X

250 A*

JDL36250CU33X

JGL36250CU33X

JJL36250CU33X

JLL36250CU33X

JRL36250CU33X

Ammeter

LSI

5.2A

60 A*

HDL36060CU43X

HGL36060CU43X

HJL36060CU43X

HLL36060CU43X

HRL36060CU43X

100 A*

HDL36100CU43X

HGL36100CU43X

HJL36100CU43X

HLL36100CU43X

HRL36100CU43X

150 A*

HDL36150CU43X

HGL36150CU43X

HJL36150CU43X

HLL36150CU43X

HRL36150CU43X

250 A*

JDL36250CU43X

JGL36250CU43X

JJL36250CU43X

JLL36250CU43X

JRL36250CU43X

Energy

LSI

5.2E

60 A*

HDL36060CU53X

HGL36060CU53X

HJL36060CU53X

HLL36060CU53X

HRL36060CU53X

100 A*

HDL36100CU53X

HGL36100CU53X

HJL36100CU53X

HLL36100CU53X

HRL36100CU53X

150 A*

HDL36150CU53X

HGL36150CU53X

HJL36150CU53X

HLL36150CU53X

HRL36150CU53X

250 A*

JDL36250CU53X

JGL36250CU53X

JJL36250CU53X

JLL36250CU53X

JRL36250CU53X

J-Frame 250 A Mission Critical Electronic Trip UL Rated Circuit Breakers (Three-Pole, 480Y/277 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating*

Type

Function

Trip Unit

D

G

J

L

Standard (80%) Rated Circuit Breakers, Three-Pole

Standard

LI

3.2-W

250 A

JDL34250WU31X

JGL34250WU31X

JJL34250WU31X

JLL34250WU31X

Standard

LSI

3.2S-W

250 A

JDL34250WU33X

JGL34250WU33X

JJL34250WU33X

JLL34250WU33X

Ammeter

LSI

5.2A-W

250 A

JDL34250WU43X

JGL34250WU43X

JJL34250WU43X

JLL34250WU43X

Energy

LSI

5.2E-W

250 A

JDL34250WU53X

JGL34250WU53X

JJL34250WU53X

JLL34250WU53X

Ammeter

LSIG

6.2A-W

250 A

JDL34250WU44X

JGL34250WU44X

JJL34250WU44X

JLL34250WU44X

Energy

LSIG

6.2E-W

250 A

JDL34250WU54X

JGL34250WU54X

JJL34250WU54X

JLL34250WU54X

I-Line Circuit Breaker Catalog Numbers

PowerPacT H-Frame 150 A I-Line Thermal-Magnetic Circuit Breakers with Factory-Sealed Trip Unit (Suitable for Reverse Connection)

Current Rating at
104°F (40°C)*

Fixed AC Magnetic Trip

Interrupting Rating*
Standard (80%) Rated*

Hold

Trip

D

G

J*

L*

H-Frame, 150 A, Two-Pole, 600 Vac 50/60 Hz, 250 Vdc

15 A

350 A

750 A

HDA26015( )

HGA26015( )

HJA26015( )

HLA26015( )

20 A

350 A

750 A

HDA26020( )

HGA26020( )

HJA26020( )

HLA26020( )

25 A

350 A

750 A

HDA26025( )

HGA26025( )

HJA26025( )

HLA26025( )

30 A

350 A

750 A

HDA26030( )

HGA26030( )

HJA26030( )

HLA26030( )

35 A

400 A

850 A

HDA26035( )

HGA26035( )

HJA26035( )

HLA26035( )

40 A

400 A

850 A

HDA26040( )

HGA26040( )

HJA26040( )

HLA26040( )

45 A

400 A

850 A

HDA26045( )

HGA26045( )

HJA26045( )

HLA26045( )

50 A

400 A

850 A

HDA26050( )

HGA26050( )

HJA26050( )

HLA26050( )

60 A

800 A

1450 A

HDA26060( )

HGA26060( )

HJA26060( )

HLA26060( )

70 A

800 A

1450 A

HDA26070( )

HGA26070( )

HJA26070( )

HLA26070( )

80 A

800 A

1450 A

HDA26080( )

HGA26080( )

HJA26080( )

HLA26080( )

90 A

800 A

1450 A

HDA26090( )

HGA26090( )

HJA26090( )

HLA26090( )

100 A

900 A

1700 A

HDA26100( )

HGA26100( )

HJA26100( )

HLA26100( )

110 A

900 A

1700 A

HDA26110( )

HGA26110( )

HJA26110( )

HLA26110( )

125 A

900 A

1700 A

HDA26125( )

HGA26125( )

HJA26125( )

HLA26125( )

150 A

900 A

1700 A

HDA26150( )

HGA26150( )

HJA26150( )

HLA26150( )

H-Frame, 150 A, Three-Pole, 600 Vac 50/60 Hz, 250 Vdc

15 A

350 A

750 A

HDA36015

HGA36015

HJA36015

HLA36015

20 A

350 A

750 A

HDA36020

HGA36020

HJA36020

HLA36020

25 A

350 A

750 A

HDA36025

HGA36025

HJA36025

HLA36025

30 A

350 A

750 A

HDA36030

HGA36030

HJA36030

HLA36030

35 A

400 A

850 A

HDA36035

HGA36035

HJA36035

HLA36035

40 A

400 A

850 A

HDA36040

HGA36040

HJA36040

HLA36040

45 A

400 A

850 A

HDA36045

HGA36045

HJA36045

HLA36045

50 A

400 A

850 A

HDA36050

HGA36050

HJA36050

HLA36050

60 A

800 A

1450 A

HDA36060

HGA36060

HJA36060

HLA36060

70 A

800 A

1450 A

HDA36070

HGA36070

HJA36070

HLA36070

80 A

800 A

1450 A

HDA36080

HGA36080

HJA36080

HLA36080

90 A

800 A

1450 A

HDA36090

HGA36090

HJA36090

HLA36090

100 A

900 A

1700 A

HDA36100

HGA36100

HJA36100

HLA36100

110 A

900 A

1700 A

HDA36110

HGA36110

HJA36110

HLA36110

125 A

900 A

1700 A

HDA36125

HGA36125

HJA36125

HLA36125

150 A

900 A

1700 A

HDA36150

HGA36150

HJA36150

HLA36150

PowerPacT J-Frame 250 A I-Line Thermal-Magnetic Circuit Breakers with Factory-Sealed Trip Unit (Suitable for Reverse Connection)

Current Rating at
104°F (40°C)

Adjustable AC Magnetic Trip

Interrupting Rating*
Standard* (80%) Rated*

Hold

Trip

D

G

J*

L3*

R3*

J-Frame, 250 A, Two-Pole, 600 Vac 50/60 Hz, 250 Vdc

150 A*

750 A

1500 A

JDA26150( )

JGA26150( )

JJA26150( )

175 A*

875 A

1750 A

JDA26175( )

JGA26175( )

JJA26175( )

200 A*

1000 A

2000 A

JDA26200( )

JGA26200( )

JJA26200( )

225 A*

1125 A

2250 A

JDA26225( )

JGA26225( )

JJA26225( )

250 A*

1250 A

2500 A

JDA26250( )

JGA26250( )

JJA26250( )

J-Frame, 250 A, Three-Pole, 600 Vac 50/60 Hz, 250 Vdc

150 A*

750 A

1500 A

JDA36150

JGA36150

JJA36150

JLA36150

JRA36150

175 A*

875 A

1750 A

JDA36175

JGA36175

JJA36175

JLA36175

JRA36175

200 A*

1000 A

2000 A

JDA36200

JGA36200

JJA36200

JLA36200

JRA36200

225 A*

1125 A

2250 A

JDA36225

JGA36225

JJA36225

JLA36225

JRA36225

250 A*

1250 A

2500 A

JDA36250

JGA36250

JJA36250

JLA36250

JRA36250

H-Frame 150 A and J-Frame 250 A I-Line Standard (80%) Rated Electronic Trip UL Rated Circuit Breakers (Three-Pole, 600 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating

Type*

Function

Trip Unit

D

G

J*

L*

R*

Standard

LI

3.2*

60 A*

HDA36060U31X

HGA36060U31X

HJA36060U31X

HLA36060U31X

HRA36060U31X

100 A*

HDA36100U31X

HGA36100U31X

HJA36100U31X

HLA36100U31X

HRA36100U31X

150 A*

HDA36150U31X

HGA36150U31X

HJA36150U31X

HLA36150U31X

HRA36150U31X

250 A * *

JDA36250U31X

JGA36250U31X

JJA36250U31X

JLA36250U31X

JRA36250U31X

Standard

LSI

3.2S*

60 A*

HDA36060U33X

HGA36060U33X

HJA36060U33X

HLA36060U33X

HRA36060U33X

100 A*

HDA36100U33X

HGA36100U33X

HJA36100U33X

HLA36100U33X

HRA36100U33X

150 A*

HDA36150U33X

HGA36150U33X

HJA36150U33X

HLA36150U33X

HRA36150U33X

250 A * *

JDA36250U33X

JGA36250U33X

JJA36250U33X

JLA36250U33X

JRA36250U33X

Ammeter

LSI

5.2A

60 A*

HDA36060U43X

HGA36060U43X

HJA36060U43X

HLA36060U43X

HRA36060U43X

100 A*

HDA36100U43X

HGA36100U43X

HJA36100U43X

HLA36100U43X

HRA36100U43X

150 A*

HDA36150U43X

HGA36150U43X

HJA36150U43X

HLA36150U43X

HRA36150U43X

250 A* *

JDA36250U43X

JGA36250U43X

JJA36250U43X

JLA36250U43X

JRA36250U43X

Energy

LSI

5.2E

60 A*

HDA36060U53X

HGA36060U53X

HJA36060U53X

HLA36060U53X

HRA36060U53X

100 A*

HDA36100U53X

HGA36100U53X

HJA36100U53X

HLA36100U53X

HRA36100U53X

150 A*

HDA36150U53X

HGA36150U53X

HJA36150U53X

HLA36150U53X

HRA36150U53X

250 A* *

JDA36250U53X

JGA36250U53X

JJA36250U53X

JLA36250U53X

JRA36250U53X

Ammeter

LSIG

6.2A*

60 A*

HDA36060U44X

HGA36060U44X

HJA36060U44X

HLA36060U44X

HRA36060U44X

100 A*

HDA36100U44X

HGA36100U44X

HJA36100U44X

HLA36100U44X

HRA36100U44X

150 A*

HDA36150U44X

HGA36150U44X

HJA36150U44X

HLA36150U44X

HRA36150U44X

250 A* *

JDA36250U44X

JGA36250U44X

JJA36250U44X

JLA36250U44X

JRA36250U44X

Energy

LSIG

6.2E

60 A*

HDA36060U54X

HGA36060U54X

HJA36060U54X

HLA36060U54X

HRA36060U54X

100 A*

HDA36100U54X

HGA36100U54X

HJA36100U54X

HLA36100U54X

HRA36100U54X

150 A*

HDA36150U54X

HGA36150U54X

HJA36150U54X

HLA36150U54X

HRA36150U54X

250 A* *

JDA3625054X

JGA36250U54X

JJA36250U54X

JLA36250U54X

JRA36250U54X

J-Frame 250 A Mission Critical I-Line Standard (80%) Rated Electronic Trip UL Rated Circuit Breakers (Three-Pole, 480Y/277 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating*

Type

Function

Trip Unit

D

G

J

L

Standard

LI

3.2-W

250 A

JDA34250WU31X

JGA34250WU31X

JJA34250WU31X

JLA34250WU31X

Standard

LSI

3.2S-W

250 A

JDA34250WU33X

JGA34250WU33X

JJA34250WU33X

JLA34250WU33X

Ammeter

LSI

5.2A-W

250 A

JDA34250WU43X

JGA34250WU43X

JJA34250WU43X

JLA34250WU43X

Energy

LSI

5.2E-W

250 A

JDA34250WU53X

JGA34250WU53X

JJA34250WU53X

JLA34250WU53X

Ammeter

LSIG

6.2A-W

250 A

JDA34250WU44X

JGA34250WU44X

JJA34250WU44X

JLA34250WU44X

Energy

LSIG

6.2E-W

250 A

JDA34250WU54X

JGA34250WU54X

JJA34250WU54X

JLA34250WU54X

Circuit Breakers with Field-Interchangeable Trip Units

H-Frame 150 A Circuit Breaker Frame with Field-Interchangeable Thermal-Magnetic Trip Units (Three-Pole, 600 Vac, 250 Vdc)

Ampere Rating*

Fixed AC Magnetic Trip*

Interrupting Rating

D

G

J*

L*

Hold

Trip

Cat. No.

Cat. No.

Cat. No.

Cat. No.

15 A

350 A

750 A

HDL36015T*

HGL36015T

HJL36015T

HLL36015T

20 A

350 A

750 A

HDL36020T

HGL36020T

HJL36020T

HLL36020T

25 A

350 A

750 A

HDL36025T

HGL36025T

HJL36025T

HLL36025T

30 A

350 A

750 A

HDL36030T

HGL36030T

HJL36030T

HLL36030T

35 A

400 A

850 A

HDL36035T

HGL36035T

HJL36035T

HLL36035T

40 A

400 A

850 A

HDL36040T

HGL36040T

HJL36040T

HLL36040T

45 A

400 A

850 A

HDL36045T

HGL36045T

HJL36045T

HLL36045T

50 A

400 A

850 A

HDL36050T

HGL36050T

HJL36050T

HLL36050T

60 A

800 A

1450 A

HDL36060T

HGL36060T

HJL36060T

HLL36060T

70 A

800 A

1450 A

HDL36070T

HGL36070T

HJL36070T

HLL36070T

80 A

800 A

1450 A

HDL36080T

HGL36080T

HJL36080T

HLL36080T

90 A

800 A

1450 A

HDL36090T

HGL36090T

HJL36090T

HLL36090T

100 A

900 A

1700 A

HDL36100T

HGL36100T

HJL36100T

HLL36100T

110 A

900 A

1700 A

HDL36110T

HGL36110T

HJL36110T

HLL36110T

125 A

900 A

1700 A

HDL36125T

HGL36125T

HJL36125T

HLL36125T

150 A

900 A

1700 A

HDL36150T

HGL36150T

HJL36150T

HLL36150T

J-Frame 250 A Circuit Breaker Frame with Field-Interchangeable Thermal-Magnetic Trip Units (Three-Pole, 600 Vac, 250 Vdc)

Ampere Rating *

Adjustable AC Magnetic Trip

Interrupting Rating

D

G

J*

L*

Low

High

Cat. No.

Cat. No.

Cat. No.

Cat. No.

150 A*

750 A

1500 A

JDL36150T*

JGL36150T

JJL36150T

JLL36150T

175 A*

875 A

1750 A

JDL36175T

JGL36175T

JJL36175T

JLL36175T

200 A*

1000 A

2000 A

JDL36200T

JGL36200T

JJL36200T

JLL36200T

225 A*

1125 A

2250 A

JDL36225T

JGL36225T

JJL36225T

JLL36225T

250 A*

1250 A

2500 A

JDL36250T

JGL36250T

JJL36250T

JLL36250T

H-Frame 150 A and J-Frame 250 A Three-Pole Circuit Breakers with Lugs and Field-Interchangeable Electronic Trip Units (Standard (80%) Rated, 600 Vac, 50/60 Hz)

Electronic Trip Unit* *

Sensor Size

Interrupting Rating

Type

Function

Trip Unit

D

G

J*

L*

Standard

LI

3.2

60 A*

HDL36060TU31X*

HGL36060TU31X

HJL36060TU31X

HLL36060TU31X

100 A*

HDL36100TU31X

HGL36100TU31X

HJL36100TU31X

HLL36100TU31X

150 A*

HDL36150TU31X

HGL36150TU31X

HJL36150TU31X

HLL36150TU31X

250 A*

JDL36250TU31X

JGL36250TU31X

JJL36250TU31X

JLL36250TU31X

Standard

LSI

3.2S

60 A*

HDL36060TU33X

HGL36060TU33X

HJL36060TU33X

HLL36060TU33X

100 A*

HDL36100TU33X

HGL36100TU33X

HJL36100TU33X

HLL36100TU33X

150 A*

HDL36150TU33X

HGL36150TU33X

HJL36150TU33X

HLL36150TU33X

250 A*

JDL36250TU33X

JGL36250TU33X

JJL36250TU33X

JLL36250TU33X

Ammeter

LSI

5.2A

60 A*

HDL36060TU43X

HGL36060TU43X

HJL36060TU43X

HLL36060TU43X

100 A*

HDL36100TU43X

HGL36100TU43X

HJL36100TU43X

HLL36100TU43X

150 A*

HDL36150TU43X

HGL36150TU43X

HJL36150TU43X

HLL36150TU43X

250 A*

JDL36250TU43X

JGL36250TU43X

JJL36250TU43X

JLL36250TU43X

Energy

LSI

5.2E

60 A*

HDL36060TU53X

HGL36060TU53X

HJL36060TU53X

HLL36060TU53X

100 A*

HDL36100TU53X

HGL36100TU53X

HJL36100TU53X

HLL36100TU53X

150 A*

HDL36150TU53X

HGL36150TU53X

HJL36150TU53X

HLL36150TU53X

250 A*

JDL36250TU53X

JGL36250TU53X

JJL36250TU53X

JLL36250TU53X

Ammeter

LSIG

6.2A

60 A*

HDL36060TU44X

HGL36060TU44X

HJL36060TU44X

HLL36060TU44X

100 A*

HDL36100TU44X

HGL36100TU44X

HJL36100TU44X

HLL36100TU44X

150 A*

HDL36150TU44X

HGL36150TU44X

HJL36150TU44X

HLL36150TU44X

250 A*

JDL36250TU44X

JGL36250TU44X

JJL36250TU44X

JLL36250TU44X

Energy

LSIG

6.2E

60 A*

HDL36060TU54X

HGL36060TU54X

HJL36060TU54X

HLL36060TU54X

100 A*

HDL36100TU54X

HGL36100TU54X

HJL36100TU54X

HLL36100TU54X

150 A*

HDL36150TU54X

HGL36150TU54X

HJL36150TU54X

HLL36150TU54X

250 A*

JDL36250TU54X

JGL36250TU54X

JJL36250TU54X

JLL36250TU54X

H-Frame and J-Frame Three-Pole Field-Installable Thermal-Magnetic Trip Units

 

15–60 A H-Frame

70–150 A H-Frame

150–250 A J-Frame

Amperage

Cat. No.

Amperage

Cat. No.

Amperage

Cat. No.

15 A

HT3015

70 A

HT3070

150 A

JT3150

20 A

HT3020

80 A

HT3080

175 A

JT3175

25 A

HT3025

90 A

HT3090

200 A

JT3200

30 A

HT3030

100 A

HT3100

225 A

JT3225

35 A

HT3035

110 A

HT3110

250 A

JT3250

40 A

HT3040

125 A

HT3125

45 A

HT3045

150 A

HT3150

50 A

HT3050

60 A

HT3060

H-Frame and J-Frame Three-Pole Field-Installable MicroLogic Electronic Trip Units

Electronic Trip Unit *

Ampere Settings

Trip Unit Cat. No.

Type

Function

Trip Unit

Standard

LI

3.2

15-20-25-30-35-40-45-50-60

HE3060U31X

35-40-45-50-60-70-80-90-100

HE3100U31X

50-60-70-80-90-100-110-125-150

HE3150U31X

70-80-100-125-150-175-200-225-250

JE3250U31X

LSI

3.2S

15-20-25-30-35-40-45-50-60

HE3060U33X

35-40-45-50-60-70-80-90-100

HE3100U33X

50-60-70-80-90-100-110-125-150

HE3150U33X

70-80-100-125-150-175-200-225-250

JE3250U33X

Ammeter

LSI

5.2A

15–60

HE3060U43X

35–100

HE3100U43X

50–150

HE3150U43X

70–250

JE3250U43X

LSIG

6.2A

15–60

HE3060U44X

35–100

HE3100U44X

50–150

HE3150U44X

70–250

JE3250U44X

Energy

LSI

5.2E

15–60

HE3060U53X

35–100

HE3100U53X

50–150

HE3150U53X

70–250

JE3250U53X

LSIG

6.2E

15–60

HE3060U54X

35–100

HE3100U54X

50–150

HE3150U54X

70–250

JE3250U54X

L-Frame Circuit Breaker Catalog Numbers

Unit-Mount Circuit Breaker Catalog Numbers

L-Frame 600 A Electronic Trip UL Rated Three-Pole Circuit Breakers (600 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating (2nd Letter of Catalog Number)

Type

Function

Trip Unit

D

G

J*

L*

R*

Standard (80%) Rated, 600 Vac, 50/60 Hz

Standard

LI

3.3*

250 A*

LDL36250U31X

LGL36250U31X

LJL36250U31X

LLL36250U31X

LRL36250U31X

400 A*

LDL36400U31X

LGL36400U31X

LJL36400U31X

LLL36400U31X

LRL36400U31X

600 A*

LDL36600U31X

LGL36600U31X

LJL36600U31X

LLL36600U31X

LRL36600U31X

Standard

LSI

3.3S*

250 A*

LDL36250U33X

LGL36250U33X

LJL36250U33X

LLL36250U33X

LRL36250U33X

400 A*

LDL36400U33X

LGL36400U33X

LJL36400U33X

LLL36400U33X

LRL36400U33X

600 A*

LDL36600U33X

LGL36600U33X

LJL36600U33X

LLL36600U33X

LRL36600U33X

Ammeter

LSI

5.3A

400 A*

LDL36400U43X

LGL36400U43X

LJL36400U43X

LLL36400U43X

LRL36400U43X

600 A*

LDL36600U43X

LGL36600U43X

LJL36600U43X

LLL36600U43X

LRL36600U43X

Energy

LSI

5.3E

400 A*

LDL36400U53X

LGL36400U53X

LJL36400U53X

LLL36400U53X

LRL36400U53X

600 A*

LDL36600U53X

LGL36600U53X

LJL36600U53X

LLL36600U53X

LRL36600U53X

Ammeter

LSIG

6.3A*

400 A*

LDL36400U44X

LGL36400U44X

LJL36400U44X

LLL36400U44X

LRL36400U44X

600 A*

LDL36600U44X

LGL36600U44X

LJL36600U44X

LLL36600U44X

LRL36600U44X

Energy

LSIG

6.3E

400 A*

LDL36400U54X

LGL36400U54X

LJL36400U54X

LLL36400U54X

LRL36400U54X

600 A*

LDL36600U54X

LGL36600U54X

LJL36600U54X

LLL36600U54X

LRL36600U54X

100% Rated, 600 Vac, 50/60 Hz

Standard

LI

3.3*

250 A*

LDL36250CU31X

LGL36250CU31X

LJL36250CU31X

LLL36250CU31X

LRL36250CU31X

400 A*

LDL36400CU31X

LGL36400CU31X

LJL36400CU31X

LLL36400CU31X

LRL36400CU31X

Standard

LSI

3.3S*

250 A*

LDL36250CU33X

LGL36250CU33X

LJL36250CU33X

LLL36250CU33X

LRL36250CU33X

400 A*

LDL36400CU33X

LGL36400CU33X

LJL36400CU33X

LLL36400CU33X

LRL36400CU33X

Ammeter

LSI

5.3A

400 A*

LDL36400CU43X

LGL36400CU43X

LJL36400CU43X

LLL36400CU43X

LRL36400CU43X

Energy

LSI

5.3E

400 A*

LDL36400CU53X

LGL36400CU53X

LJL36400CU53X

LLL36400CU53X

LRL36400CU53X

Ammeter

LSIG

6.3A*

400 A*

LDL36400CU44X

LGL36400CU44X

LJL36400CU44X

LLL36400CU44X

LRL36400CU44X

Energy

LSIG

6.3E

400 A*

LDL36400CU54X

LGL36400CU54X

LJL36400CU54X

LLL36400CU54X

LRL36400CU54X

L-Frame 600 A Mission Critical Standard (100 %) Rated Electronic Trip UL Rated Three-Pole Circuit Breakers (480Y/277 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit *

Sensor Rating

Interrupting Rating (2nd Letter of Catalog Number)

Type

Function

Trip Unit

D

G

J

L

Standard

LI

3.3-W

250 A*

LDL34250WU31X

LGL34250WU31X

LJL34250WU31X

LLL34250WU31X

400 A*

LDL34400WU31X

LGL34400WU31X

LJL34400WU31X

LLL34400WU31X

600 A*

LDL34600WU31X

LGL34600WU31X

LJL34600WU31X

LLL34600WU31X

Standard

LSI

3.3S-W

250 A*

LDL34250WU33X

LGL34250WU33X

LJL34250WU33X

LLL34250WU33X

400 A*

LDL34400WU33X

LGL34400WU33X

LJL34400WU33X

LLL34400WU33X

600 A*

LDL34600WU33X

LGL34600WU33X

LJL34600WU33X

LLL34600WU33X

Ammeter

LSI

5.3A-W

400 A*

LDL34400WU43X

LGL34400WU43X

LJL34400WU43X

LLL34400WU43X

600 A*

LDL34600WU43X

LGL34600WU43X

LJL34600WU43X

LLL34600WU43X

Energy

LSI

5.3E-W

400 A*

LDL34400WU53X

LGL34400WU53X

LJL34400WU53X

LLL34400WU53X

600 A*

LDL34600WU53X

LGL34600WU53X

LJL34600WU53X

LLL34600WU53X

Ammeter

LSIG

6.3A-W

400 A*

LDL34400WU44X

LGL34400WU44X

LJL34400WU44X

LLL34400WU44X

600 A*

LDL34600WU44X

LGL34600WU44X

LJL34600WU44X

LLL34600WU44X

Energy

LSIG

6.3E-W

400 A*

LDL34400WU54X

LGL34400WU54X

LJL34400WU54X

LLL34400WU54X

600 A*

LDL34600WU54X

LGL34600WU54X

LJL34600WU54X

LLL34600WU54X

L-Frame 600 A Electronic Trip UL Rated Four-Pole Circuit Breakers (600 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating (2nd Letter of Catalog Number)

Type

Function

Trip Unit

D

G

J*

L*

R*

Standard (80%) Rated, 600 Vac, 50/60 Hz

Standard

LI

3.3

250 A *

LDL46250U31X

LGL46250U31X

LJL46250U31X

LLL46250U31X

LRL46250U31X

400 A*

LDL46400U31X

LGL46400U31X

LJL46400U31X

LLL46400U31X

LRL46400U31X

600 A*

LDL46600U31X

LGL46600U31X

LJL46600U31X

LLL46600U31X

LRL46600U31X

Standard

LSI

3.3S

250 A*

LDL46250U33X

LGL46250U33X

LJL46250U33X

LLL46250U33X

LRL46250U33X

400 A*

LDL46400U33X

LGL46400U33X

LJL46400U33X

LLL46400U33X

LRL46400U33X

600 A*

LDL46600U33X

LGL46600U33X

LJL46600U33X

LLL46600U33X

LRL46600U33X

Ammeter

LSI

5.3A

400 A*

LDL46400U43X

LGL46400U43X

LJL46400U43X

LLL46400U43X

LRL46400U43X

600 A*

LDL46600U43X

LGL46600U43X

LJL46600U43X

LLL46600U43X

LRL46600U43X

Energy

LSI

5.3E

400 A*

LDL46400U53X

LGL46400U53X

LJL46400U53X

LLL46400U53X

LRL46400U53X

600 A*

LDL46600U53X

LGL46600U53X

LJL46600U53X

LLL46600U53X

LRL46600U53X

Ammeter

LSIG

6.3A

400 A*

LDL46400U44X

LGL46400U44X

LJL46400U44X

LLL46400U44X

LRL46400U44X

600 A*

LDL46600U44X

LGL46600U44X

LJL46600U44X

LLL46600U44X

LRL46600U44X

Energy

LSIG

6.3E

400 A*

LDL46400U54X

LGL46400U54X

LJL46400U54X

LLL46400U54X

LRL46400U54X

600 A*

LDL46600U54X

LGL46600U54X

LJL46600U54X

LLL46600U54X

LRL46600U54X

100% Rated, 600 Vac, 50/60 Hz

Standard

LI

3.3

250 A*

LDL46250CU31X

LGL46250CU31X

LJL46250CU31X

LLL46250CU31X

LRL46250CU31X

400 A*

LDL46400CU31X

LGL46400CU31X

LJL46400CU31X

LLL46400CU31X

LRL46400CU31X

Standard

LSI

3.3S

250 A*

LDL46250CU33X

LGL46250CU33X

LJL46250CU33X

LLL46250CU33X

LRL46250CU33X

400 A*

LDL46400CU33X

LGL46400CU33X

LJL46400CU33X

LLL46400CU33X

LRL46400CU33X

Ammeter

LSI

5.3A

400 A*

LDL46400CU43X

LGL46400CU43X

LJL46400CU43X

LLL46400CU43X

LRL46400CU43X

Energy

LSI

5.3E

400 A*

LDL46400CU53X

LGL46400CU53X

LJL46400CU53X

LLL46400CU53X

LRL46400CU53X

Ammeter

LSIG

6.3A

400 A*

LDL46400CU44X

LGL46400CU44X

LJL46400CU44X

LLL46400CU44X

LRL46400CU44X

Energy

LSIG

6.3E

400 A*

LDL46400CU54X

LGL46400CU54X

LJL46400CU54X

LLL46400CU54X

LRL46400CU54X

L-Frame 600 A Mission Critical Standard (80%) Rated Electronic Trip UL Rated Four-Pole Circuit Breakers (480Y/277 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating (2nd Letter of Catalog Number)

Type

Function

Trip Unit

D

G

J

L

Standard

LI

3.3-W

250 A*

LDL44250WU31X

LGL44250WU31X

LJL44250WU31X

LLL44250WU31X

400 A*

LDL44400WU31X

LGL44400WU31X

LJL44400WU31X

LLL44400WU31X

600 A*

LDL44600WU31X

LGL44600WU31X

LJL44600WU31X

LLL44600WU31X

Standard

LSI

3.3S-W

250 A*

LDL44250WU33X

LGL44250WU33X

LJL44250WU33X

LLL44250WU33X

400 A*

LDL44400WU33X

LGL44400WU33X

LJL44400WU33X

LLL44400WU33X

600 A*

LDL44600WU33X

LGL44600WU33X

LJL44600WU33X

LLL44600WU33X

Ammeter

LSI

5.3A-W

400 A*

LDL44400WU43X

LGL44400WU43X

LJL44400WU43X

LLL44400WU43X

600 A*

LDL44600WU43X

LGL44600WU43X

LJL44600WU43X

LLL44600WU43X

Energy

LSI

5.3E-W

400 A*

LDL44400WU53X

LGL44400WU53X

LJL44400WU53X

LLL44400WU53X

600 A*

LDL44600WU53X

LGL44600WU53X

LJL44600WU53X

LLL44600WU53X

Ammeter

LSIG

6.3A-W

400 A*

LDL44400WU44X

LGL44400WU44X

LJL44400WU44X

LLL44400WU44X

600 A*

LDL44600WU44X

LGL44600WU44X

LJL44600WU44X

LLL44600WU44X

Energy

LSIG

6.3E-W

400 A*

LDL44400WU54X

LGL44400WU54X

LJL44400WU54X

LLL44400WU54X

600 A*

LDL44600WU54X

LGL44600WU54X

LJL44600WU54X

LLL44600WU54X

I-Line Circuit Breaker Catalog Numbers

L-Frame 600 A I-Line Standard (80%) Rated Electronic Trip UL Rated Circuit Breakers (600 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating

Type

Function

Trip Unit

D

G

J *

L3 *

R3 *

Standard

LI

3.3*

250 A*

LDA36250U31X

LGA36250U31X

LJA36250U31X

LLA36250U31X

LRA36250U31X

400 A*

LDA36400U31X

LGA36400U31X

LJA36400U31X

LLA36400U31X

LRA36400U31X

600 A*

LDA36600U31X

LGA36600U31X

LJA36600U31X

LLA36600U31X

LRA36600U31X

Standard

LSI

3.3S*

250 A*

LDA36250U33X

LGA36250U33X

LJA36250U33X

LLA36250U33X

LRA36250U33X

400 A*

LDA36400U33X

LGA36400U33X

LJA36400U33X

LLA36400U33X

LRA36400U33X

600 A*

LDA36600U33X

LGA36600U33X

LJA36600U33X

LLA36600U33X

LRA36600U33X

Ammeter

LSI

5.3A

400 A*

LDA36400U43X

LGA36400U43X

LJA36400U43X

LLA36400U43X

LRA36400U43X

600 A*

LDA36600U43X

LGA36600U43X

LJA36600U43X

LLA36600U43X

LRA36600U43X

Energy

LSI

5.3E

400 A*

LDA36400U53X

LGA36400U53X

LJA36400U53X

LLA36400U53X

LRA36400U53X

600 A*

LDA36600U53X

LGA36600U53X

LJA36600U53X

LLA36600U53X

LRA36600U53X

Ammeter

LSIG

6.3A*

400 A*

LDA36400U44X

LGA36400U44X

LJA36400U44X

LLA36400U44X

LRA36400U44X

600 A*

LDA36600U44X

LGA36600U44X

LJA36600U44X

LLA36600U44X

LRA36600U44X

Energy

LSIG

6.3E

400 A*

LDA36400U54X

LGA36400U54X

LJA36400U54X

LLA36400U54X

LRA36400U54X

600 A*

LDA36600U54X

LGA36600U54X

LJA36600U54X

LLA36600U54X

LRA36600U54X

L-Frame 600 A Mission Critical I-Line Standard (80%) Rated Electronic Trip UL Rated Circuit Breakers (480/277 Vac, 50/60 Hz) With Factory Sealed Trip Units Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating

Type

Function

Trip Unit

D

G

J

L

Standard

LI

3.3 W

250 A*

LDA34250WU31X

LGA34250WU31X

LJA34250WU31X

LLA34250WU31X

400 A*

LDA34400WU31X

LGA34400WU31X

LJA34400WU31X

LLA34400WU31X

600 A*

LDA34600WU31X

LGA34600WU31X

LJA34600WU31X

LLA34600WU31X

Standard

LSI

3.3S-W

250 A*

LDA34250WU33X

LGA34250WU33X

LJA34250WU33X

LLA34250WU33X

400 A*

LDA34400WU33X

LGA34400WU33X

LJA34400WU33X

LLA34400WU33X

600 A*

LDA34600WU33X

LGA34600WU33X

LJA34600WU33X

LLA34600WU33X

Ammeter

LSI

5.3A-W

400 A*

LDA34400WU43X

LGA34400WU43X

LJA34400WU43X

LLA34400WU43X

600 A*

LDA34600WU43X

LGA34600WU43X

LJA34600WU43X

LLA34600WU43X

Energy

LSI

5.3E-W

400 A*

LDA34400WU53X

LGA34400WU53X

LJA34400WU53X

LLA34400WU53X

600 A*

LDA34600WU53X

LGA34600WU53X

LJA34600WU53X

LLA34600WU53X

Ammeter

LSIG

6.3A-W

400 A*

LDA34400WU44X

LGA34400WU44X

LJA34400WU44X

LLA34400WU44X

600 A*

LDA34600WU44X

LGA34600WU44X

LJA34600WU44X

LLA34600WU44X

Energy

LSIG

6.3E-W

400 A*

LDA34400WU54X

LGA34400WU54X

LJA34400WU54X

LLA34400WU54X

600 A*

LDA34600WU54X

LGA34600WU54X

LJA34600WU54X

LLA34600WU54X

L-Frame 250 A and 400 A I–Line 100% Rated Electronic Trip UL Rated Circuit Breakers (600 Vac, 50/60 Hz) With Factory Sealed Trip Unit Suitable for Reverse Connection

Electronic Trip Unit

Sensor Rating

Interrupting Rating

D

G

J*

L*

R*

Type

Function

Trip Unit

Standard

LI

3.3*

250 A*

LDA36250CU31X

LGA36250CU31X

LJA36250CU31X

LLA36250CU31X

LRA36250CU31X

400 A

LDA36400CU31X

LGA36400CU31X

LJA36400CU31X

LLA36400CU31X

LRA36400CU31X

Standard

LSI

3.3S*

250 A*

LDA36250CU33X

LGA36250CU33X

LJA36250CU33X

LLA36250CU33X

LRA36250CU33X

400 A*

LDA36400CU33X

LGA36400CU33X

LJA36400CU33X

LLA36400CU33X

LRA36400CU33X

Ammeter

LSI

5.3A

400 A*

LDA36400CU43X

LGA36400CU43X

LJA36400CU43X

LLA36400CU43X

LRA36400CU43X

Energy

LSI

5.3E

400 A*

LDA36400CU53X

LGA36400CU53X

LJA36400CU53X

LLA36400CU53X

LRA36400CU53X

Ammeter

LSIG

6.3A*

400 A*

LDA36400CU44X

LGA36400CU44X

LJA36400CU44X

LLA36400CU44X

LRA36400CU44X

Energy

LSIG

6.3E

400 A*

LDA36400CU54X

LGA36400CU54X

LJA36400CU54X

LLA36400CU54X

LRA36400CU54X

Circuit Breakers with Field-Interchangeable Trip Units Catalog Numbers

L-Frame 3-Pole, 600 A Circuit Breakers with Lugs and Field-Interchangeable Electronic Trip Units (600 Vac, 50/60 Hz)

Electronic Trip Unit

Sensor Rating

Interrupting Rating

D

G

J*

L*

Type

Function

Trip Unit

Standard (80% Rated), 600 Vac, 50/60 Hz* *

Standard

LI

3.3

250 A*

LDL36250TU31X

LGL36250TU31X

LJL36250TU31X

LLL36250TU31X

400 A*

LDL36600TU31X

LGL36600TU31X

LJL36600TU31X

LLL36600TU31X

600 A*

LDL36400TU31X

LDL36400TU31X

LDL36400TU31X

LDL36400TU31X

Standard

LSI

3.3S

250 A*

LDL36250TU33X

LGL36250TU33X

LJL36250TU33X

LLL36250TU33X

400 A*

LDL36400TU33X

LGL36400TU33X

LJL36400TU33X

LLL36400TU33X

600 A*

LDL36600TU33X

LGL36600TU33X

LJL36600TU33X

LLL36600TU33X

Ammeter

LSI

5.3A

400 A*

LDL36400TU43X

LGL36400TU43X

LJL36400TU43X

LLL36400TU43X

600 A*

LDL36600TU43X

LGL36600TU43X

LJL36600TU43X

LLL36600TU43X

Energy

LSI

5.3E

400 A*

LDL36400TU53X

LGL36400TU53X

LJL36400TU53X

LLL36400TU53X

600 A*

LDL36600TU53X

LGL36600TU53X

LJL36600TU53X

LLL36600TU53X

Ammeter

LSIG

6.3A

400 A*

LDL36400TU44X

LGL36400TU44X

LJL36400TU44X

LLL36400TU44X

600 A*

LDL36600TU44X

LGL36600TU44X

LJL36600TU44X

LLL36600TU44X

Energy

LSIG

6.3E

400 A*

LDL36400TU54X

LGL36400TU54X

LJL36400TU54X

LLL36400TU54X

600 A*

LDL36600TU54X

LGL36600TU54X

LJL36600TU54X

LLL36600TU54X

100% Rated, 600 Vac, 50/60 Hz* * *

Standard

LI

3.3

250 A*

LDL36250RU31X

LGL36250RU31X

LJL36250RU31X

LLL36250RU31X

400 A*

LDL36400RU31X

LGL36400RU31X

LJL36400RU31X

LLL36400RU31X

Standard

LSI

3.3S

250 A*

LDL36250RU33X

LGL36250RU33X

LJL36250RU33X

LLL36250RU33X

400 A*

LDL36400RU33X

LGL36400RU33X

LJL36400RU33X

LLL36400RU33X

Ammeter

LSI

5.3A

400 A*

LDL36400RU43X

LGL36400RU43X

LJL36400RU43X

LLL36400RU43X

Energy

LSI

5.3E

400 A*

LDL36400RU53X

LGL36400RU53X

LJL36400RU53X

LLL36400RU53X

Ammeter

LSIG

6.3A

400 A*

LDL36400RU44X

LGL36400RU44X

LJL36400RU44X

LLL36400RU44X

Energy

LSIG

6.3E

400 A*

LDL36400RU54X

LGL36400RU54X

LJL36400RU54X

LLL36400RU54X

L-Frame Three-Pole Field-Installable Micrologic Electronic Trip Units

Electronic Trip Unit

Ampere Setting

Trip Unit Cat. No.

Type

Function

Trip Unit

Standard

LI

3.3

70-80-100-125-150-175-200-225-250

LE3250U31X

125-150-175-200-225-250-300-350-400

LE3400U31X

200-225-250-300-350-400-450-500-600

LE3600U31X

LSI

3.3S

70-80-100-125-150-175-200-225-250

LE3250U33X

125-150-175-200-225-250-300-350-400

LE3400U33X

200-225-250-300-350-400-450-500-600

LE3600U33X

Ammeter

LSI

5.3A

125–400

LE3400U43X

200–600

LE3600U43X

LSIG

6.3A

125–400

LE3400U44X

200–600

LE3600U44X

Energy

LSI

5.3E

125–400

LE3400U53X

200–600

LE3600U53X

LSIG

6.3E

125–400

LE3400U54X

200–600

LE3600U54X

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.