0611CT1001 R09/24

General Information

The PowerPacT H-, J-, and L-frame circuit breakers are designed to protect electrical systems from damage caused by overloads and short circuits. H- and J-frame circuit breakers are available with either thermal-magnetic or MicroLogic electronic trip units. L-frame circuit breakers are available with MicroLogic electronic trip units only.

H- and J-frame circuit breakers with thermal-magnetic trip units contain individual thermal (overload) and instantaneous (short circuit) sensing elements in each pole. The amperage ratings of the thermal trip elements are calibrated at 104°F (40°C) free air ambient temperature. Per the National Electric Code® (NEC®) and the Canadian Electrical Code, standard circuit breakers may only be applied continuously at up to 80% of their rating. Circuit breakers rated for 100% operation are available but require specially-designed enclosures and 194°F (90°C) rated wire.

Devices with the MicroLogic electronic trip unit provide adjustable protection settings for greater system flexibility. In addition to electronic protection, MicroLogic trip units allow users to monitor both energy and power. Through direct access to in-depth information and networking using open protocols, PowerPacT circuit breakers with MicroLogic trip units let operators optimize the management of their electrical installations. Far more than just a circuit breaker, these devices are a measurement and communication tool ready to meet energy-efficiency needs through optimized power requirements, increased energy availability, and improved installation management.

PowerPacT™ H-, J-, and L-frame will include the industries only LED locator in an MCCB called Visi-Trip. Visi-Trip is designed to provide a visual light alert when a breaker needs to be inspected, increasing safety and saving customers time finding the concern and allowing them to being the troubleshooting process faster.

Applications

PowerPacT H-, J- and L-frame circuit breakers offer high performance and a wide range of interchangeable trip units to protect most applications.

Electronic trip units provide highly accurate protection with wide setting ranges and can integrate measurement, metering and communication functions. They can be combined with the front display module (FDM121) to provide functions similar to a power meter.

Power Meter

PowerPacT H-, J-, and L-frame circuit breakers equipped with MicroLogic 5/6 trip units offer type A (ammeter) or E (energy) metering functions as well as communication capability. Using MicroLogic trip unit sensors and intelligence, PowerPacT H-, J-, and L-frame circuit breakers provide access to measurements of all the main electrical parameters on the built-in screen, on a dedicated front display module (FDM121) or through the communication network.

Operating assistance

Integration of measurement functions provides operators with operating assistance functions including alarms tripped by user-selected measurement values, time-stamped event tables and histories, and maintenance indicators.

Front display module

The main measurements can be read on the built-in screen of MicroLogic 5/6 trip units. They can also be displayed on the equipment FDM121 along with pop-up windows signalling the main alarms.

Communication network

PowerPacT H-, J-, and L-frame circuit breakers equipped with MicroLogic 5/6 trip units provide communication capabilities. Simple RJ45 cables connect to a Modbus communication interface module.

Applications

Protection of distribution systems

The PowerPacT H-, J-, and L-frame circuit breakers provide protection against short circuits and overloads for:

  • distribution systems supplied by transformers

  • distribution systems supplied by engine generator sets

They are easily installed at all levels in distribution systems, from the main LV switchboard to the subdistribution boards and enclosures. All PowerPacT circuit breakers can protect against insulation faults by adding an external Vigirex relay.

Mission critical applications

The PowerPacT H-, J-, and L-frame mission critical circuit breakers provide high levels of selective coordination with QO and ED/EG/EJ circuit breakers.

Protection of motors

The PowerPacT H-, J-, and L-frame circuit breakers include a number of versions to protect motor applications:

  • basic short-circuit protection with electronic instantaneous only MCP or the electronic MicroLogic 1.3 M trip units, combined with a special overload relay to provide thermal protection

  • protection against overloads, short circuit and phase unbalance or loss with MicroLogic 2 M trip units

The exceptional limiting capacity of the PowerPacT circuit breakers automatically provides coordination with the motor starter.

Protection of special applications

The PowerPacT H-, J-, and L-frame circuit breakers offer a number of versions for special protection applications:

  • industrial control panels with:
    — compliance with international standards IEC 60947-2 and UL 508/CSA 22.2 N°14
    — compliance with UL 489
    — installation in universal and functional enclosures

  • 400 Hz systems

Control using automatic switches

An automatic switch version of PowerPacT H-, J-, and L-frame circuit breakers is available for circuit control. All add-on functions for the circuit breakers may be combined with the basic automatic switch function, including motor operators.

For information on other automatic switches, contact Schneider Electric.

Manual transfer systems

To ensure a continuous supply of power, some electrical installations are connected to two power systems:

  • the normal source, usually the utility (U)

  • a replacement source to supply the installation when the normal source is not available, generally from a generator (G)

A mechanical and/or electrical interlocking system between two circuit breakers or automatic switches helps minimize risk of parallel connection of the sources during switching.

A system can be manual transfer mechanical device interlocking.

Mission Critical Circuit Breakers

The PowerPacT J- and L-Frame Mission Critical circuit breakers deliver high levels of selective coordination in a flexible design that can be easily configured for a variety of applications. Tested to be selectively coordinated with the QO family of miniature circuit breakers and the ED, EG, and EJ circuit breakers, this solution provides peace of mind when power availability is critical.

An electronic trip unit provides adjustable long-time settings in three sensor sizes, allowing coverage from 70 through 600 A on 120–240, 208Y/120, 240, and 480Y/277 V systems.

Ratings

 

Available Configurations

UL 489 Listed

CSA Certified

Voltage: 480Y/277 V

 
  • I-Line mounting

  • Main circuit breaker in NQ and NF panelboards

  • Unit mount for OEM users

  • Plug-in base for OEM users

  • Drawout base for OEM users

In addition to unique design attributes, the PowerPacT Mission Critical circuit breakers have also undergone rigorous testing procedures to certify the coordination with downstream circuit breakers— combining innovative engineering with validated test results.

Apply Schneider Electric Mission Critical circuit breakers in emergency power distribution systems, data centers, hospitals, or anywhere continuity of service is desired

Theory of Operation

There are several dynamic forces between the PowerPacT Mission Critical circuit breakers and downstream circuit breakers when a fault occurs downstream of the branch circuit breaker. Many of these events cannot be shown on the trip curve.

The PowerPacT Mission Critical circuit breakers analyze the fault current to make decisions which maximize selectivity with downstream circuit breakers. The trip units deploy a special selectivity delay to allow downstream circuit breakers to clear. However, on very high faults or if the downstream circuit breaker does not trip, the circuit breaker trips the mechanism instantaneously.

The combination of the PowerPacT Mission Critical circuit breaker and downstream circuit breakers shown in the selectivity charts in the instruction bulletin are selective due to the fact that the series impedance and the let-through from the downstream circuit breaker does not produce enough energy to trip the PowerPacT Mission Circuit circuit breaker.

This system maximizes the interaction of the circuit breakers in series to allow selectivity.

Trip Units and Trip Curves

The PowerPacT J- and L-Frame Mission Critical circuit breakers deliver high levels of selective coordination with the QO family of miniature circuit breakers and the ED, EG, and EJ circuit breakers in a flexible design that can be easily configured for a variety of applications. These circuit breaker can be equipped with 3.2-W, 3.2S-W, 5.2A-W, 5.2E-W, 6.2A-W, 3.3S-W, 5.3A-W, 6.3A-2, and 6.3E-2 MicroLogic trip units. See the catalog numbers and references beginning in J-Frame 250 A Mission Critical Electronic Trip UL Rated Circuit Breakers (Three-Pole, 480Y/277 Vac, 50/60 Hz) With Factory-Sealed Trip Unit Suitable for Reverse Connection.

The mission critical trip units have the same settings and trip curves as the standard trip units described in this document.

For more information see the trip unit user guides 48940-310-01 and 48940-312-01 on the Schneider Electric website.

J-frame mission critical circuit breakers are selective with QO or E-frame circuit breakers per the table below when the amperage of the main circuit breaker is at least two times the amperage of the branch circuit breaker.

J-Frame Selectivity with QO and E-Frame Circuit Breakers

Circuit Breaker*

Voltage

Current

One-Line Diagram

Main

Branch

J–W, 250 A

QO(B)
QO(B)-H
QO(B)-VH
QH

1P, 2P

10–30 A

240/120 V
120 V

18 kA

35–60 A

15 kA

70–125 A

12 kA

3P

10–30 A

240 V
208 V

15 kA

35–60 A

13 kA

70–125 A

10 kA

J–W, 250 A

E-Frame

1P, 2P, 3P

15–125 A

240 V

18 kA

15–60 A

480Y/277 V

10 kA

70–125 A

7 kA

L-frame mission critical circuit breakers are selective with QO-style and E-frame circuit breakers per the table below when the amperage of the main circuit breaker is at least two times greater than the amperage of the branch circuit breaker.

L-Frame Selectivity with QO and E-Frame Circuit Breakers

Circuit Breaker*

Voltage

Current

One-Line Diagram

Main

Branch

L–W, 250 A

QO(B)
QO(B)-H
QO(B)-VH
QH

10–60 A

240 V

18 kA

70–125 A

10 kA

L–W, 400 A
L–W, 600 A

QO(B)
QO(B)-H
QO(B)-VH
QH

15–150 A

240 V

30 kA

L–W, 250 A
L–W, 400 A
L–W, 600 A

E-Frame

15–125 A

240 V

30 kA

480Y/277

30 kA

Flexible Configurations

The PowerPacT H-, J- and L-frame circuit breakers may be configured with lugs, bus bar connections, rear connections, I-Line, drawout cradle, or plug-in base.

Field Installable Accessories and Trip Units

Field Installable Accessories and Trip Units

General Characteristics

Faceplate Label

Characteristics indicated on the faceplate label:

A. Circuit breaker type

B. Circuit breaker disconnector symbol

C. Performance levels

D. Standards

E. Ue: Operating voltage per IEC

F. Icu: Ultimate breaking capacity per IEC

G. Ics: Service breaking capacity per IEC

H. Uimp: Rated impulse withstand voltage per IEC

I. Ui: Insulation voltage per IEC

J. Certification marks

NOTE: When the circuit breaker is equipped with an extended rotary handle, the door must be opened to view the faceplate.

Codes and Standards

PowerPacT H-, J-, and L-frame circuit breakers, automatic switches and electronic motor circuit protectors are manufactured and tested in accordance with the following standards.

NOTE: Apply circuit breakers according to guidelines detailed in the National Electric Code (NEC) and other local wiring codes.

Codes and Standards

PowerPacT H-, J-, and L-Frame Circuit Breakers

H-, J-, and L-Frame Switches

Motor Circuit Protectors

UL 489*
IEC 60947-2
CSA C22.2 No. 5*
Federal Specification W-C-375B/GEN
NEMA AB1
NMX J-266
CCC
CE and UKCA Marking

UL 489*
IEC 60947-3
CSA C22.2 No. 5**
Federal Specification W-C-375B/GEN
NEMA AB1
NMX J-266
CE and UKCA Marking

UL 508
IEC 60947-2
CSA C22.2 No. 14
NEMA AB1
CCC
CE and UKCA Marking

Vibration

PowerPacT H-, J-, and L-frame devices resist mechanical vibration.

Tests are carried out in compliance with standard UL 489 SA and SB for the levels required by merchant-marine inspection organizations (Veritas®, Lloyd's®, etc.):

PowerPacT H-, J-, and L-frame circuit breaker meet IEC 60068-2-6 for vibration:

— 2.0 to 25.0 Hz and amplitude +/- 1.6 mm

— 25.0 to 100 Hz acceleration +/- 4.0 g

Excessive vibration may cause tripping, breaks in connections or damage to mechanical parts.

Electromagnetic Disturbances

PowerPacT H-, J-, and L-frame devices are protected against:

  • overvoltages caused by circuit switching

  • overvoltages caused by an atmospheric disturbances or by a distribution-system outage (such as from failure due to lightning)

  • devices emitting radio waves (radios, walkie-talkies, radar, etc.)

  • electrostatic discharges produced directly by users

PowerPacT H-, J-, and L-frame devices have successfully passed the electromagnetic-compatibility

tests (EMC) defined by the following international standards:

  • IEC/EN 60947-2: Low-voltage switchgear and controlgear, part 2: Circuit breakers:
    — Annex F: Immunity tests for circuit breakers with electronic protection
    — Annex B: Immunity tests for residual current protection

  • IEC/EN 61000-4-2: Electrostatic-discharge immunity tests

  • IEC/EN 61000-4-3: Radiated, radio-frequency, electromagnetic-field immunity tests

  • IEC/EN 61000-4-4: Electrical fast transient/burst immunity tests

  • IEC/EN 61000-4-5: Surge immunity tests

  • IEC/EN 61000-4-6: Immunity tests for conducted disturbances induced by radio frequency fields

  • CISPR 11: Limits and methods of measurement of electromagnetic disturbance characteristics of industrial, scientific and medical (ISM) radio-frequency equipment.

These tests ensure that:

  • no nuisance tripping occurs due to electromagnetic disturbances

  • tripping times are respected

Tropicalization

The materials used in PowerPacT circuit breakers will not support the growth of fungus and mold.

PowerPacT circuit breakers have passed the test defined below for extreme atmospheric conditions.

Dry cold and dry heat:

  • IEC 60068–2-1 — Test A: Cold at +55°C

  • IEC 60068-2-2 — Dry Heat at +85°C

Damp heat (tropicalization)

  • IEC 60068-2-30 — damp heat (temperature 55°C and 95% relative humidity)

  • IEC 60068-2-52 — salt mist

Special Ratings

The H-frame and J-frame circuit breakers also comply with the following special ratings:

  • HACR rating

  • SWD switch duty rating (applies only to 15 and 20 A / 277 Vac or less, two- and three-pole)

  • HID high intensity discharge lighting rating (15–50 A)

The L-frame circuit breakers complies with the following special rating:

  • HACR rating

Marine Ratings

UL Marine Listed/CSA Certified Circuit Breakers (UL 489 Supplement SA)

The PowerPacT H- and J-frame circuit breakers with thermal-magnetic trip units with D, G, J and L interruption levels meet the UL 489 Supplement SA requirements for use on vessels of any length under or over 65 ft. (19.8 m). The PowerPacT H-, J-, and L-frame circuit breakers with MicroLogic electronic trip units meet the UL 489 Supplement SA for use on vessels over 65 ft. (19.8 m) in length. Marine circuit breakers must not use aluminum or aluminum alloys for terminal connections and must be calibrated at an ambient temperature of 104°F (40°C). Standard circuit breakers should not be specified or used in the place of marine rated circuit breakers. Circuit breakers can be ordered with the Marine SA listing by adding the suffix “YA” (marine) to the catalog number.

UL Naval Listed/CSA Certified Circuit Breakers (UL 489 Supplement SB)

The PowerPacT H-, J-, and L-frame circuit breakers with MicroLogic trip units with D, G, J and L interruption levels meet the UL 489 Supplement SB requirements for use on naval vessels. These circuit breakers are subject to various vibration tests as described in UL 489 Supplement SB. Naval circuit breakers must not use aluminum or aluminum alloys for terminal connections and must be calibrated at an ambient temperature of 122°F (50°C). Standard circuit breakers should not be specified or used in the place of navel rated circuit breakers. Circuit breakers can be ordered with the Naval SB listing by adding the suffix “YA1” (naval) to the catalog number.

American Bureau of Shipping (ABS)

The PowerPacT H-, J-, and L-Frame circuit breakers are certified to ABS-NVR (American Bureau of Shipping - Naval Vessel Rules), for use on Naval vessels.

UL 489 SC Listed 500 Vdc Circuit Breakers

The UL Listed / CSA Certified thermal-magnetic H-, J-, and L-frame molded case circuit breakers are specifically designed for use on ungrounded dc systems having a maximum short-circuit voltage of 500 Vdc or a maximum floating (unloaded) voltage of 600 Vdc. The circuit breakers are suitable for use only with UPS (uninterruptable power supplies) and ungrounded systems. This two-level voltage rating allows these circuit breakers to be applied to battery sources having a short-circuit availability of 20,000 or 50,000 amperes at 500 Vdc.

These circuit breakers are UL Listed/CSA Certified for the interrupting ratings shown only if applied with three poles connected in series (series connection is external to circuit breaker). See diagram below.

NOTE: Due to external series connection, I-Line circuit breakers are not available for this application.

DC Circuit Breaker Caution Labels

H- and J-Frame Circuit Breakers

 

Source = 600 Vdc max. (floating)
500 Vdc max. (loaded)

 

L-Frame Three-Pole Circuit Breakers

L-Frame Four-Pole Circuit Breakers

L-Frame Three-Pole Circuit Breakers

L-Frame Four-Pole Circuit Breakers

DC Molded Case Circuit Breakers—Adjustable Magnetic Trip

Ampere Rating

Circuit Breaker
Cat. No.

Adjustable Magnetic Trip Range—DC Amperes

Performance Level
@ 500 Vdc

Low

High

100 A

JGL37100D81

400

600

20 k AIR

125 A

JGL37125D81

400

600

150 A

JGL37150D81

400

600

175 A

JGL37175D81

400

600

200 A

JGL37200D82

500

850

225 A

JGL37225D82

500

850

250 A

JGL37250D82

500

850

20 k AIR

300 A

LGL37030D27

750

1500

20 k AIR

350 A

LGL37035D29

875

1750

400 A

LGL37040D30

1000

2000

450 A

LGL37045D31

1125

2250

500 A

LGL37050D32

1250

2500

600 A

LGL37060D33

1500

3000

700 A

LGL47070D35

1750

3500

800 A

LGL47080D36

2000

4000

900 A

LGL47090D86

2250

4500

1000 A

LGL47100D40

2500

5000

1200 A

LGL47120D42

3000

6000

100 A

JLL37100D81

400

600

50 k AIR

125 A

JLL37125D81

400

600

150 A

JLL37150D81

400

600

175 A

JLL37175D81

400

600

200 A

JLL37200D82

500

850

225 A

JLL37225D82

500

850

250 A

JLL37250D82

500

850

300 A

LLL37030D27

750

1500

50 k AIR

350 A

LLL37035D29

875

1750

400 A

LLL37040D30

1000

200

450 A

LLL37045D31

1125

2250

500 A

LLL37050D32

1250

2500

600 A

LLL37060D33

1500

3000

700 A

LLL47070D35

1750

3500

800 A

LLL47080D36

2000

4000

900 A

LLL47090D86

2250

4500

1000 A

LLL47100D40

2500

5000

1200 A

LLL47120D42

3000

6000

DC Molded Case Circuit Breakers—Fixed Magnetic Trip

Ampere Rating

Circuit Breaker
Cat. No.

Fixed Magnetic Trip Range—DC Amperes

Performance Level
@ 500 Vdc

Low

High

30 A

HGL37030D87

300

600

20 k AIR

50 A

HGL37050D87

300

600

70 A

HGL37070D87

300

600

30 A

HLL37030D87

300

600

50 k AIR

50 A

HLL37050D87

300

600

70 A

HLL37070D87

300

600

PowerPacT H- and J-Frame Ratings

PowerPacT H- and J-Frame Circuit Breaker Ratings

Circuit Breaker

150 A H-Frame

250 A J-Frame

Circuit Breaker Type

HD

HG

HJ

HL

HR

JD

JG

JJ

JL

JR

Number of poles*

2, 3

3

2, 3

3

Amperage Range (A)

15–150

70–250

UL 489 Circuit Breaker Ratings

Breaking Capacity
(AIR)

UL/CSA/NOM
(kA rms)

240 Vac

25

65

100

125

200

25

65

100

125

200

480 Vac

18

35

65

100

200

18

35

65

100

200

600 Vac

14

18

25

50

100

14

18

25

50

100

250 Vdc*

20

20

20

20

20

20

20

20

500 Vdc*, *

20

50

20

50

IEC 947-2 Circuit Breaker Ratings

Ultimate Breaking Capacity (Icu)

(kA rms)

220/240 Vac

25

65

100

125

150

25

65

100

125

150

380/415 Vac

18

35

65

100

125

18

35

65

100

125

440/480 Vac

18

35

65

100

125

18

35

65

100

125

500/525 Vac

14

18

25

50

75

14

18

25

50

75

690 Vac

20

20

250 Vdc*

20

20

20

20

500 Vdc*, *

20

20

20

20

Service Breaking Capacity (Ics)

% Icu

100%

100%

Insulation Voltage

Ui

750 V

750 Vac

Impulse Withstand Voltage

Uimp

8 kVac

8 kVac

Operational Voltage

Ue

690 Vac

690 Vac

Sensor Rating

In

150 A

250 A

Utilization Category

A

A

Operations (Open-Close Cycles)

Without Current

4000

5000

With Current

4000

1000

PowerPacT H- and J-Frame Protection and Measurements

Circuit Breaker

150 A H-Frame

250 A J-Frame

Circuit Breaker Type

HD

HG

HJ

HL

HR

JD

JG

JJ

JL

JR

Number of poles*

2, 3

3

2, 3

3

Protection and Measurements

Short-circuit Protection

Magnetic only

X

X

X

X

X

X

X

X

X

X

Overload/Short-circuit Protection

Thermal-magnetic

X

X

X

X

X

X

X

X

X

X

Electronic

X

X

X

X

X

X

X

X

X

X

with neutral protection
(Off-0.5-1-OSN)*

X

X

X

X

X

X

X

X

X

X

with ground fault protection

X

X

X

X

X

X

X

X

X

X

with zone selective interlocking (ZSI)*

X

X

X

X

X

X

X

X

X

X

Display / I, V, f, P, E, THD measurements / interrupted-current measurement

X

X

X

X

X

X

X

X

X

X

Options

Front display module (FDM121)

X

X

X

X

X

X

X

X

X

X

Operating assistance

X

X

X

X

X

X

X

X

X

X

Counters

X

X

X

X

X

X

X

X

X

X

Histories and alarms

X

X

X

X

X

X

X

X

X

X

Metering Com

X

X

X

X

X

X

X

X

X

X

Device status/control com

X

X

X

X

X

X

X

X

X

X

Visi-Trip

X

X

X

X

X

X

X

X

X

X

PowerPacT H- and J-Frame Dimensions / Weight / Connections

Circuit Breaker

150 A H-Frame

250 A J-Frame

Circuit Breaker Type

HD

HG

HJ

HL

HR

JD

JG

JJ

JL

JR

Number of poles*

2, 3

3

2, 3

3

Dimensions
(Three-Pole Unit Mount)
in. (mm)

Height

6.4 (163)

7.5 (191)

Width

4.1 (104)

4.1 (104)

Depth

3.4 (86)

3.4 (86)

Weight - lb. (Kg)

4.8 (2.2)

5.3 (2.4)

Connections / Terminations

Unit Mount

X

X

I-Line

X

X

Rear Connection

X

X

Plug-In

X

X

Drawout

X

X

Optional Lugs

X

X

PowerPacT L-Frame Ratings

PowerPacT L-Frame Circuit Breaker Ratings

Circuit Breaker

400 A L-Frame

600 A L-Frame

600 A DC L-Frame*

1200 A
DC L-Frame
*

Circuit Breaker Type

LG

LJ

LL

LR

LG

LJ

LL

LR

LG

LL

LG

LL

Number of Poles

3, 4

3, 4

3

3

4

Amperage Range (A)

70–400

200–600

300–600

700–1200

UL 489 Circuit Breaker Ratings

Breaking Capacity
(AIR)

UL/CSA/NOM
(kA rms)

240 Vac

65

100

125

200

65

100

125

200

480 Vac

35

65

100

200

35

65

100

200

600 Vac

18

25

50

100

18

25

50

100

250 Vdc*

500 Vdc*, *

20

50

20

20

IEC 947-2 Circuit Breaker Ratings

Ultimate Breaking Capacity (Icu)

(kA rms)

220/240 Vac

65

100

125

150

65

100

125

150

380/415 Vac

35

65

100

125

35

65

100

125

440/480 Vac

35

65

100

125

35

65

100

125

500/525 Vac

18

25

50

75

18

25

50

75*

690 Vac

20

20

250 Vdc*

500 Vdc*, *

Service Breaking Capacity (Ics)

% Icu

100%

100%

Insulation Voltage

Ui

800 Vac

800 Vac

Impulse Withstand Voltage

Uimp

8 kVac

8 kVac

Operational Voltage

Ue

690 Vac

690 Vac

Sensor Rating

In

400 A

600 A

Utilization Category

A

A

Operations (Open-Close Cycles)

Without Current

5000

5000

With Current

1000

1000

PowerPacT L-Frame Protection and Measurements

Circuit Breaker

400 A L-Frame

600 A L-Frame

1200 A
L-Frame

Circuit Breaker Type

LG

LJ

LL

LR

LG

LJ

LL

LR

LG

LL

Number of Poles

3, 4

3, 4

4

Protection and Measurements

Short-circuit Protection

Magnetic only

X

X

X

X

X

X

X

X

Overload/Short-circuit Protection

Thermal-magnetic

X

X

Electronic

X

X

X

X

X

X

X

X

with neutral protection
(Off-0.5-1-OSN)*

X

X

X

X

X

X

X

X

with ground fault protection

X

X

X

X

X

X

X

X

with zone selective interlocking (ZSI)*

X

X

X

X

X

X

X

X

Display / I, V, f, P, E, THD Measurements / Interrupted-Current Measurement

X

X

X

X

X

X

X

X

Options

Front display module (FDM121)

X

X

X

X

X

X

X

X

Operating assistance

X

X

X

X

X

X

X

X

Counters

X

X

X

X

X

X

X

X

Histories and alarms

X

X

X

X

X

X

X

X

Metering Com

X

X

X

X

X

X

X

X

Device status/control com

X

X

X

X

X

X

X

X

Visi-Trip

Visi-Trip

X

X

X

X

X

X

X

X

PowerPacT L-Frame Circuit Breaker Dimensions / Weight / Connections

Circuit Breaker

400 A L-Frame

600 A L-Frame

1200 A
L-Frame

Circuit Breaker Type

LG

LJ

LL

LR

LG

LJ

LL

LR

LG

LL

Number of Poles

3, 4

3, 4

4

Dimensions
(Three-Pole Unit Mount)
in. (mm)

Height

13.38 (340)

13.38 (340)

13.38 (340)

Width

5.51 (140)

5.51 (140)

5.51 (140)

Depth

4.33 (110)

4.33 (110)

4.33 (110)

Weight - lb. (Kg)

13.2 (6.0)

13.7 (6.2)

13.7 (6.2)

Connections / Terminations

Unit Mount

X

X

X

I-Line

X

X

Rear Connection

X

X

X*

Plug-In

X

X

Drawout

X

X

Optional Lugs

X

X

PowerPacT H-, J-, and L-frame Circuit Breaker Trip Units

MicroLogic Trip Unit Features

Features

MicroLogic Trip Unit
(X = Standard Feature, O = Available Option)

Standard

Ammeter

Energy

3.2/3.3

3.2S/3.3S

5.2A/5.3A

6.2A/6.3A

5.2E/5.3E

6.2E/6.3E

LI

X

 

LSI*

X

X

X

LSIG/Ground Fault Trip*

X

X

Ground-Fault Alarm Trip

X

X

Current Settings Directly in Amperes

X

X

X

X

X

X

True RMS Sensing

X

X

X

X

X

X

UL Listed

X

X

X

X

X

X

Thermal Imaging

X

X

X

X

X

X

LED for Long-Time Pickup

X

X

X

X

X

X

LED for Long-Time Alarm

X

X

X

X

X

X

LED Green “Ready” Indicator

X

X

X

X

X

X

Up to 12 Alarms Used Together

X

X

X

X

Digital Ammeter

X

X

X

X

Zone-Selective Interlocking*

X

X

X

X

Communications

O

O

O

O

O

O

LCD Display

X

X

X

X

Front Display Module FDM121

O

O

O

O

Advanced User Interface

X

X

X

X

Neutral Protection

X

X

X

X

Contact Wear Indication*

X

X

X

X

Incremental Fine Tuning of Settings

X

X

X

X

Load Profile*, *

X

X

X

X

Power Measurement

X

X

Power Quality Measurements

X

X

Thermal-Magnetic or Electronic Trip Unit

Thermal-magnetic trip units (available on H- and J-frame circuit breakers only) protect against overcurrents and short-circuits using tried and true techniques. For applications requiring installation optimization and energy efficiency, electronic trip units offer more advanced protection functions combined with measurements.

Trip units using digital electronics are faster as well as more accurate. Wide setting ranges make installation upgrades easier. Designed with processing capabilities, MicroLogic trip units can provide measurement information and device operating assistance. With this information, users can avoid or deal more effectively with disturbances and can play a more active role in system operation. They can manage the installation, anticipate events and plan any necessary servicing.

Accurate Measurements for Complete Protection

PowerPacT H-, J-, and L-frame circuit breakers offer excellent measurement accuracy from 15 amperes on up to the short-circuit currents. This is made possible by a new generation of current transformers combining “iron-core” sensors for self-powered electronics and “air core” sensors (Rogowski coils) for measurements. The protection functions are managed by an ASIC (Application Specific Integrated Circuit) component that is independent of the measurement functions. This independence ensures immunity to conducted and radiated disturbances and increases reliability.

Numerous Security Functions

Torque-limiting screws

The screws secure the trip unit to the circuit breaker. When the correct tightening torque is reached, the screw heads break off. Optimum tightening avoids any risk of temperature rise. A torque wrench is no longer required.

Easy and sure changing of trip units

All trip units are interchangeable, without wiring. A mechanical mismatch-protection system minimizes the possibility of mounting a trip unit on a circuit breaker with a lower rating.*

“Ready” LED for a continuous self-test

The LED on the front of the electronic trip units indicates the result of the self-test running continuously on the measurement system and the tripping release. As long as the green LED is flashing, the links between the CTs, the processing electronics and the tripping mechanism are operational. The circuit breaker is ready to protect. A minimum current of 15 to 50 A, depending on the device, is required for this indication function.

A patented dual adjustment system for protection functions

Available on MicroLogic 5/6 trip units, the system consists of:

  • an adjustment using rotary switches sets the maximum value

  • an adjustment using the keypad or made remotely fine-tunes the setting. This setting may not exceed the first one. It can be read directly on the MicroLogic trip unit screen, to within one ampere and a fraction of a second.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.