0611CT1001 R09/24

Installation Recommendations

NOTE: A special 122°F (50°C) rating is available for special high ambient conditions (not UL listed). Order by adding CA suffix to catalog number.

Operation Conditions

Temperature Derating

  • PowerPacT H-, J-, and L-frame circuit breakers may be used between -13°F and 158°F (-2°C and +70°C). For temperatures higher than 104°F (40°C) inside the enclosure, devices must be derated.

  • Circuit breakers should be put into service under normal ambient, operating-temperature conditions.

  • The permissible storage-temperature range for PowerPacT H-, J-, and L-frame circuit breakers in the original packing is -58°F* and 185°F (-50°C* and +85°C).

H-Frame Trip Curve

(ln) Fixed threshold thermal protection against overload
(li) Fixed threshold instantaneous protection against short circuits

Temperature Derating for H-Frame Trip Unit Thermal Protection—Long-Time

Temp.*

Rating (A) In

°F

°C

14

-10

23

30

38

46

53

60

68

76

88

103

112

123

137

160

180

221

32

0

21

28

36

43

49

56

63

71

83

97

107

117

131

151

171

207

50

10

20

26

33

40

46

52

59

66

77

90

101

111

126

141

161

194

68

20

18

24

31

37

42

48

54

62

72

84

96

105

120

132

152

180

86

30

17

22

28

34

39

44

50

56

66

77

88

98

110

121

139

165

104

40

15

20

25

30

35

40

45

50

60

70

80

90

100

110

125

150

122

50

12

17

21

25

30

34

38

43

53

62

72

80

86

95

109

131

140

60

9

14

17

20

24

28

31

35

46

53

63

70

72

80

93

111

J-Frame Trip Unit

(ln) Fixed threshold thermal protection against overload

(lm) Adjustable instantaneous protection against short circuits

Temperature Derating for J-Frame Trip Unit Thermal Protection—Long-Time

Temperature *

Rating (A) In

°F

°C

14

-10

221

264

289

330

377

32

0

207

247

273

310

354

50

10

194

230

256

290

330

68

20

180

213

240

270

307

86

30

165

194

220

248

279

104

40

150

175

200

225

250

122

50

131

150

176

193

214

140

60

111

124

151

160

177

PowerPacT H-, J- and L-Frame Circuit Breakers Equipped with Electronic Trip Units

Electronic trip units are not affected by variations in temperature. If the trip units are used in high temperature environments, the MicroLogic trip unit setting must nevertheless take into account the temperature limits of the circuit breaker.

Changes in temperature do not affect measurements by electronic trip units.

  • The built-in CT sensors with Rogowski coils measure the current.

  • The control electronics compare the value of the current to the settings defined for 104°F (40°C).

Because temperature has no effect on the CT measurements, the tripping thresholds do not need to be modified.

However, the temperature rise caused by the flow of current combined with the ambient temperature increases the temperature of the device. To avoid reaching the thermal withstand value, it is necessary to limit the current flowing through the device, that is the maximum Ir setting as a function of the temperature.

The table below indicates the maximum long-time (LT) protection setting Ir (A) depending on the ambient temperature.

Derating Circuit Breakers with MicroLogic Trip Units

Type of Device

Rating

Temperature

104°F (40°C)

113°F (45°C)

122°F (50°C)

131°F (55°C)

140°F (60°C)

149°F (65°C)

158°F (70°C)

H-Frame

Unit-mount, plug-in or drawout

60 A

No derating

100 A

No derating

150 A

No derating

J-Frame

Unit-mount

250 A

250

250

250

245

237

230

225

Plug-in or drawout

250 A

250

245

237

230

225

220

215

L-Frame

Unit-mount

400 A

400

400

400

390

380

370

360

Plug-in or drawout

400 A

400

390

380

370

360

350

340

Unit-mount

600 A

600

600

600

585

570

550

535

Plug-in or drawout

600 A

570

550

535

520

505

490

475

Example. A unit-mount PowerPacT L-frame circuit breaker equipped with a MicroLogic can have a maximum Ir setting of:

  • 400 A up to 122°F (50°C)

  • 380 A up to 140°F (60°C)

Altitude Derating

Altitude does not significantly affect the characteristics of PowerPacT H-, J-, and L-frame circuit breakers circuit breakers up to 6560 ft. (2000 m). Above this altitude, it is necessary to take into account the decrease in the dielectric strength and cooling capacity of air.

The following table gives the corrections to be applied for altitudes above 6560 ft. (2000 m). The breaking capacities remain unchanged.

Altitude Derating

Altitude

6560 ft
(2000 m)

9840 ft
(3000 m)

13120 ft
(4000 m)

16400 ft
(5000 m)

Dielectric withstand voltage

3000 V

2500 V

2100 V

1800 V

Insulation voltage

Vi

800 V

700 V

600 V

500 V

Maximum operational voltage

Ve

690 V

590 V

520 V

460 V

Average current capacity (A) at 104°F (40°C)

In x

1 0.

0.96

0.93

0.9

Frequency Derating

Application of H- and J-frame circuit breakers at frequencies above 60 Hz requires that special consideration be given to the effects of high frequency on the circuit breaker characteristics. Thermal and instantaneous operations must be treated separately.

At frequencies below 60 Hz, the thermal derating of PowerPacT H and J-frame circuit breakers is negligible. However, at frequencies above 60 Hz, thermal derating is required.

One of the most common high frequency applications is at 400 Hz. For 400 Hz derating information, see 400 Hz Applications.

For more information, refer to Data Bulletin 0100DB0101, Determining Current Carrying Capacity in Special Applications.

Installation in Equipment

Power from the Top or Bottom

PowerPacT H-, J-, and L-frame circuit breakers with factory-sealed trip units can be supplied from either the top or the bottom without any reduction in performance. This capability facilitates connection when installed in end-use equipment.

All connection and insulation accessories can be used on circuit breakers supplied either from the top or bottom.

Weight

The table below presents the weights of the circuit breakers and the main accessories, which must be summed to obtain the total weight. The values are valid for all performance categories.

Weights

Type of Device

Poles

Circuit Breakers

Base

Cradle

Motor Operator

H-frame, 100 A

2

3.95 lbs.
(1.79 kg)

1.75 lbs.
(0.8 kg)

4.85 lbs.
(2.2 kg)

2.65 lbs.
(1.2 kg)

3

4.52 lbs.
(2.05 kg)

1.75 lbs.
(0.8 kg)

4.85 lbs.
(2.2 kg)

2.65 lbs.
(1.2 kg)

H-frame, 150 A

2

4.08 lbs.
(1.85 kg)

1.75 lbs.
(0.8 kg)

4.85 lbs.
(2.2 kg)

2.65 lbs.
(1.2 kg)

3

4.85 lbs.
(2.2 kg)

1.75 lbs.
(0.8 kg)

4.85 lbs.
(2.2 kg)

2.65 lbs.
(1.2 kg)

J-frame, 250 A

3

5.29 lbs.
(2.4 kg)

1.75 lbs.
(0.8 kg)

4.85 lbs.
(2.2 kg)

2.65 lbs.
(1.2 kg)

L-frame, 600 A

3

13.65 lbs.
(6.19 kg)

5.29 lbs.
(2.4 kg)

4.85 lbs.
(2.2 kg)

6.17 lbs.
(2.8 kg)

4

17.92 lbs.
(8.13 kg)

6.17 lbs.
(2.8 kg)

4.85 lbs.
(2.2 kg)

6.17 lbs.
(2.8 kg)

Safety Clearances and Minimum Distances

General Rules

When installing a circuit breaker, minimum distances (safety clearances) must be maintained between the device and panels, bars and other protection devices installed nearby. These distances, which depend on the voltage, are defined by tests carried out in accordance with UL standards.

If installation is not checked by type tests, it is also necessary to:

  • use insulated bars for circuit-breaker connections

  • segregate the busbars using phase barriers

For PowerPacT H-, J-, and L-frame devices, terminal shields and interphase barriers are recommended and may be mandatory depending on the operating voltage of the device and type of installation (unit-mount, drawout, etc.).

Power Connections

The table below indicates the connection requirements for PowerPacT H-, J-, and L-frame devices to ensure insulation of live parts for the various types of connection.

  • unit-mount devices with front connection or rear connection

  • plug-in or drawout devices.

Connection accessories such as crimp lugs, terminal extensions (straight, right-angle, double-L and 45°) and spreaders are supplied with interphase barriers. Long terminal shields provide a degree of protection of IP40 (ingress).

Safety Clearance

H- and J-Frame Fiber Insulating Plate

If dimension A < 0.56 in. for H- and J-frame circuit breaker, attach fiber insulating plate, not provided, to enclosure cover.

Dimensions:

in.
(mm)

Control Wiring

Remote Tripping by Undervoltage Trip (MN) or Shunt Trip (MX)

Power requirements are approximately:

  • 30 VA for pick-up of the undervoltage trip (MN) and shunt trip (MX)

  • 300–500 VA for the motor operator.

Recommended Maximum Cable Lengths

Power Supply Voltage (Vdc)

Length*

12 Vdc

24 Vdc

48 Vdc

Cable cross-section

16 AWG
(1.5 mm²)

14 AWG
(2.5 mm²)

16 AWG
(1.5 mm²)

14 AWG
(2.5 mm²)

16 AWG
(1.5 mm²)

14 AWG
(2.5 mm²)

Undervoltage Trip (MN)

V source 100%

49 ft.
(15 m)

525 ft.
(160 m)

2100 ft.
(640 m)

V source 85%

23 ft.
(7 m)

131 ft.
(40 m)

525 ft.
(160 m)

Shunt Trip (MX)

V source 100%

197 ft.
(60 m)

787 ft.
(240 m)

3150 ft.
(960 m)

V source 85%

98 ft.
(30 m)

394 ft.
(120 m)

1575 ft.
(480 m)

Motor Operator

V source 100%

33 ft.
(10 m)

52 ft.
(16 m)

213 ft.
(65 m)

361 ft.
(110 m)

V source 85%

6.6 ft.
(2 m)

13 ft
(4 m)

56 ft.
(17 m)

82 ft.
(25 m)

External Neutral Voltage Tap (ENVT)

This connection is required for accurate power measurements on three-pole circuit breakers equipped with MicroLogic 5/6 E trip units in installations with a distributed neutral. It can be used to measure phase-neutral voltages and calculate power using the 3 wattmeter method.

PowerPacT H-, J-, and L-frame three-pole circuit breakers come with a wire installed on the device for the connection to the ENVT. This wire is equipped with a connector for connection to an external wire with:

  • cross-sectional area of 18–14 AWG (1 mm² to 2.5 mm²)

  • maximum length of 32.8 ft. (10 m).

External Neutral Current Transformer (ENCT)

This connection is required to protect the neutral on three-pole circuit breakers equipped with MicroLogic 5/6 A or E trip units in installations with a distributed neutral. For MicroLogic 6 A or E, it is required for ground-fault protection.

The ENCT is connected in the same way for unit-mount, plug-in or drawout devices:

  • unit-mount devices are connected using terminals T1 and T2 of the internal terminal block.

  • plug-in and drawout devices are not connected using the auxiliary terminals.

The wires must be connected/disconnected inside the devices using terminals T1 and T2.

The ENCT must be connected to the MicroLogic trip unit by a shielded twisted pair. The shielding should be connected to the enclosure earth only at the CT end, no more than 12 in. (30 cm) from the CT.

  • the power connections of the CT to the neutral (H2 and H1) must be made in the same way for power supply from the top or the bottom (see the figure). Make sure they are not reversed for devices with power supply from the bottom.

  • cross-sectional area of 22–16 AWG (0.4 mm² to 1.5 mm²)

  • maximum length of 32.8 ft. (10 m).

24 Vdc Power Supply Module

An external 24 Vdc power supply is required for installations with communication networks, regardless of the type of trip unit.

On installations without communication networks, the power supply is available as an option for MicroLogic 5/6 to:

  • modify settings when the circuit breaker is open (OFF position)

  • display measurements when the current flowing through the circuit breaker is low

  • maintain the display of the cause of tripping

To determine the power requirements of the devices, see Power Requirements.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.