Basic ArcFM Configuration
The sample data provided with the ArcFM Solution makes extensive use of model names and autoupdaters to support the functionality of tools and components that make editing more productive in ArcMap. This page lists the feature classes and fields to which model names and autoupdaters are assigned in a database such as Minerville. This page gives the basic configuration for ArcFM. ArcFM tools such as Feeder Manager and Tracing require additional configuration. See the Configuring ArcFM section for information about configuring specific ArcFM tools. Use the Snapping Manager to set snapping on feature classes.
Autoupdaters: All autoupdaters are described in the Appendix. It is a good idea to review the descriptions for the autoupdaters assigned below and ensure you understand what they do. Do not assign an autoupdater to a feature if you do not want it to fire.
Geodatabase Level Model Names
For all implementations, in ArcCatalog, using the ArcFM Properties Manager, assign the MM ENTERPRISE at the geodatabase level. Depending on mobile implementations, you might also assign additional model names at this level.
Create Domains
There are several domains you must create in order to use tracing. These domains provide the coded values for various functionality. The Object Class Model Name Domain and Field Model Name Domain must be created in order to assign model names in the ArcFM Properties Manager.
Create Conduit Tracing Domains
Create Feeder Manager 1.0 Domains
Create Feeder Manager 2.0 Domains
All Datasets
All feature classes
Set Editable to No on these fields: Creation User, Date Created, Last User, and Date Modified
Assign the ArcFM User Name autoupdater to the On Feature Create event of the Creation User field
Assign the ArcFM User Name autoupdater to the On Feature Update event of the Last User field
Assign the ArcFM Current Date autoupdater to the On Feature Create event of the Date Created field
Assign the ArcFM Current Date autoupdater to the On Feature Update event of the Date Modified field
Set ArcFM Primary Display field to FacilityID, if applicable
All point feature classes
Assign this field model name only if you wish to use the ArcFM Manual Angle Setter edit task or ArcFM Auto Angle Setter attribute autoupdater. Assign the SYMBOLROTATION field model name to the Symbol Rotation field.
All object classes
Set Editable to No on these fields: Creation User, Date Created, Last User, and Date Modified
Assign the ArcFM User Name autoupdater to the On Feature Create event of the Creation User field
Assign the ArcFM User Name autoupdater to the On Feature Update event of the Last User field
Assign the ArcFM Current Date autoupdater to the On Feature Create event of the Date Created field
Assign the ArcFM Current Date autoupdater to the On Feature Update event of the Date Modified field
Electric Dataset
All linear feature classes
Set ArcFM Length Measured Domain autoupdater for the MeasuredLength field On Feature Create
Ensure the MeasuredLength field is editable
Anchor Guy feature class
Assign model name ANCHORGUY
Assign field model name GUYCOUNT to Guy Count field
Assign field model name LEADLENGTH to Lead Length field
Assign field model name WIRESIZE to Wire Size field
Assign field model name WIRESTRENGTH to Wire Strength field
On Object Info tab, assign ArcFM Manual Angle Setter to Create Edit Task
BusBar feature class
Assign model name CONDUCTOR
Assign model name SPLITTARGET
Assign field model name PHASEDESIGNATION to Phase Designation field
Assign ArcFM Structure Relate autoupdater to On Feature Create and On Feature Update
ConductorInfo object class
Assign model name CONDUCTORINFO
Assign field model name PHASEDESIGNATION to phase designation field
Assign field model name CONDUCTORSIZE to Conductor Size field
Assign field model name CONDUCTORMATERIAL to Conductor Material field
Assign field model name NUMBERCONDUCTORSPERPHASE to Number Conductors Per Phase field
DeliveryPoint object class
On Object Info tab, assign the following autoupdater to the On Feature Update event:
-
ArcFM Connect Network Feature
DynamicProtectiveDevice (CircuitBreaker, Recloser, Sectionalizer)
Assign model name DYNAMICPROTECTIVEDEVICE
Assign model name PROTECTIVE
On Object Info tab, set the Split On Edit field to Yes.
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Create event:
-
ArcFM Structure Relate
-
ArcFM Segment Split
-
ArcFM Inherit Operating Voltage
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Update event:
-
ArcFM Structure Relate
-
ArcFM Connect Network Feature
-
ArcFM Segment Split
ElectricStation feature class
Assign model name STRUCTURE
Fuse feature class
Assign model name PROTECTIVE
On Field Info tab, assign the ArcFMArcFM Auto Phase Assign AU to the PhaseDesignation field's On Feature Create and On Feature Update
On Field Info tab, assign the ArcFM Auto Angle Setter AU to the SymbolRotation field's On Feature Create and On Feature Update
On Object Info tab, set the Split On Edit field to Yes.
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Create event:
-
ArcFM Segment Split
-
ArcFM Structure Relate
-
ArcFM Inherit Operating Voltage
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Update event:
-
ArcFMArcFM Structure Relate
-
ArcFM Connect Network Feature
-
ArcFM Segment Split
Generator feature class
On the ObjectInfo tab, assign the following autoupdater to the On Feature Update event:
-
ArcFMArcFM Connect Network Feature
MiscNetworkFeature feature class
On the ObjectInfo tab, assign the following autoupdater to the On Feature Update event:
-
ArcFMArcFM Connect Network Feature
Open Point feature class
On the ObjectInfo tab, assign the following autoupdaters (in the order listed) to the On Feature Create event:
-
ArcFM Segment Split
-
ArcFM Structure Relate
On the ObjectInfo tab, assign the following autoupdaters (in the order listed) to the On Feature Update event:
-
ArcFM Structure Relate
-
ArcFM Connect Network Feature
-
ArcFM Segment Split
PFCorrectingEquipment feature class
On the ObjectInfo tab, assign the following autoupdater to the On Feature Update event:
-
ArcFMArcFM Connect Network Feature
PrimaryMeter feature class
On the ObjectInfo tab, assign the following autoupdater to the On Feature Update event:
-
ArcFM Connect Network Feature
PriOHElectricLineSegment
Assign model name CONDUCTOR
Assign model name OVERHEADCONDUCTOR
Assign model name PRIMARYCONDUCTOR
Assign model name SPLITTARGET
Assign field model name PHASEDESIGNATION to Phase Designation field
Assign field model name NEUTRALSIZE to Neutral Size field
Assign field model name NEUTRALMATERIAL to Neutral Material field
Assign field model name MEASUREDLENGTH to Measured Length field
Set MeasuredLength field to be editable
Set PhaseDesignation field to be editable
PriUGElectricLineSegment
Assign model name CONDUCTOR
Assign model name PRIMARYCONDUCTOR
Assign model name SPLITTARGET
Assign field model name PHASEDESIGNATION to Phase Designation field
Assign field model name NEUTRALSIZE to Neutral Size field
Assign field model name NEUTRALMATERIAL to Neutral Material field
Assign field model name MEASUREDLENGTH to Measured Length field
Set MeasuredLength field to be editable
Set PhaseDesignation field to be editable
SecOHElectricLineSegment
Assign model name CONDUCTOR
Assign model name OVERHEADCONDUCTOR
Assign model name SPLITTARGET
Assign field model name PHASEDESIGNATION to Phase Designation field
Assign field model name NEUTRALSIZE to Neutral Size field
Assign field model name NEUTRALMATERIAL to Neutral Material field
Assign field model name MEASUREDLENGTH to Measured Length field
Set MeasuredLength field to be editable
Set PhaseDesignation field to be editable
SecUGElectricLineSegment
Assign model name CONDUCTOR
Assign model name SPLITTARGET
Assign field model name PHASEDESIGNATION to Phase Designation field
Assign field model name NEUTRALSIZE to Neutral Size field
Assign field model name NEUTRALMATERIAL to Neutral Material field
Assign field model name MEASUREDLENGTH to Measured Length field
Set MeasuredLength field to be editable
Set PhaseDesignation field to be editable
ServicePoint feature class
Assign model name SERVICEPOINT
Assign field model name SERVICECURRENTRATING to Service Current Rating field
Assign field model name PHASEDESIGNATION to Phase Designation field
On the ObjectInfo tab, assign the following autoupdater to the On Feature Update event:
-
ArcFM Connect Network Feature
Streetlight feature class
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Update event
-
ArcFMArcFM Structure Relate
-
ArcFM Connect Network Feature
SupportStructure feature class
Assign model name STRUCTURE
Assign model name OVERHEADSTRUCTURE
Assign field model name CLASS to Class field
Assign field model name HEIGHT to Height field
Assign field model name MATERIAL to Material field
Assign field model name USAGETYPE to Usage Type field
Assign field model name DIAMETER to Diameter field
Set visibility of Class field to No for Non-Wood subtypes
Set visibility of Diameter field to No for Wood subtypes
Set visibility of PoleCount field to No for all subtypes except H-Frame
SurfaceStructure feature class
Assign model name STRUCTURE
Switch feature class
Assign model name SWITCH
Assign model name PROTECTIVE
On Field Info tab, assign the ArcFM Auto Phase Assign autoupdater to the PhaseDesignation field’s On Feature Create and On Feature Update events
On Field Info tab, assign ArcFMArcFM Auto Angle Setter autoupdater to Symbol Rotation fields at On Feature Create and On Feature Update events
On Object Info tab, set the Split On Edit field to Yes.
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Create event
-
ArcFMArcFM Segment Split
-
ArcFM Structure Relate
-
ArcFM Inherit Operating Voltage
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Update event
-
ArcFMArcFM Structure Relate
-
ArcFM Connect Network Feature
-
ArcFM Segment Split
SwitchingFacility feature class
Assign model name STRUCTURE
Transformer feature class
Assign model name TRANSFORMER
Assign model name DISTRIBUTIONTRANSFORMER
Assign field model name RATEDKVA to RatedKVA field
Assign field model name PHASEDESIGNATION to Phase Designation field
Assign field model name LOWSIDEVOLTAGE to Low Side Voltage field
Assign field model name GROUNDRESISTANCE to Ground Resistance field
Assign field model name GROUNDREACTANCE to Ground Reactance field
Assign field model name HIGHSIDECONFIGURATION to High Side Configuration field
Assign field model name LOWSIDECONFIGURATION to Low Side Configuration field
Assign field model name HIGHSIDEGROUNDREACTANCE to High Side Ground Reactance field
Assign field model name HIGHSIDEGROUNDRESISTANCE to High Side Ground Resistance field
Assign field model name LOWSIDEGROUNDREACTANCE to Low Side Ground Reactance field
Assign field model name LOWSIDEGROUNDRESISTANCE to Low Side Ground Resistance field
Assign field model name SUBTYPECD to SubtypeCD field
On Object Info tab, assign ArcFM Manual Angle Setter to Create Edit Task
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Create event:
-
ArcFM Structure Relate
-
ArcFM Inherit Nominal Voltage
-
ArcFM Inherit Operating Voltage
On Object Info tab, assign the following autoupdaters (in the order listed) to the On Feature Update event:
-
ArcFM Structure Relate
-
ArcFM Connect Network Feature
Set Editable property of RatedKVA field to No
Transformer Unit object class
Assign model name TRANSFORMERUNIT
Assign field model name RATEDKVA to RatedKVA field
Assign field model name PHASEDESIGNATION to Phase Designation field
Assign ArcFM Update Transformer Bank Rated kVA autoupdater to the On Feature Update event
UndergroundStructure feature class
Assign model name STRUCTURE
VoltageRegulator feature class
On the ObjectInfo tab, assign the following autoupdaters (in the order listed) to the On Feature Update event:
-
ArcFM Structure Relate
-
ArcFM Connect Network Feature
Gas Dataset
ControllableFitting
Assign model name CONTROLFITTING
CPAnode
Assign model name ANODE
CPRectifier
Assign model name RECTIFIER
CPTestPoint
Assign model name TESTPOINT
DistributionMain
Assign model name DISTRIBUTIONMAIN
Assign model name PIPE
Assign model name SPLITTARGET
GasPipeCasing
Assign model name GASPIPECASING
GasValve
Assign model name VALVE
On the ObjectInfo tab, assign the ArcFM Segment Split autoupdater to the On Feature Create event
On the ObjectInfo tab, assign the following autoupdaters (in the order listed) to the On Feature Update event:
-
ArcFM Connect Network Feature
-
ArcFM Segment Split
LeakReport
Assign model name LEAKREPORT
LeakSurveyArea
Assign model name LEAKSURVEYAREA
MeterSetting
Assign model name SERVICEPOINT
NonControllableFitting
Assign model name NONCONTROLFITTING
PipeExposure
Assign model name PIPEEXPOSURE
RegulatorStation
Assign model name REGULATOR
Service
Assign model name PIPE
Assign model name SERVICE
TownBorderStation
Assign model name TBS
Vault
Assign model name VAULT
Water Dataset
wControlValve
Assign model name VALVE
On the ObjectInfo tab, assign the ArcFM Segment Split autoupdater to the On Feature Create event
On the ObjectInfo tab, assign the following autoupdaters (in the order listed) to the On Feature Update event:
-
ArcFMArcFM Connect Network Feature
-
ArcFM Segment Split
wCPAnode
Assign model name ANODE
wCPRectifier
Assign model name RECTIFIER
wCPTestPoint
Assign model name TESTPOINT
wGravityPressureMain
Assign model name DISTRIBUTIONMAIN
Assign model name SPLITTARGET
wLateralService
Assign model name DISTRIBUTIONMAIN
Assign model name PIPE
Assign model name SERVICE
wLeak
Assign model name LEAKREPORT
wMeter
Assign model name SERVICEPOINT
wNetworkStructure
Assign model name NETWORKSOURCE
wPumpPressureMain
Assign model name DISTRIBUTIONMAIN
Assign model name SPLITTARGET
wSystemValve
Assign model name VALVE
On the ObjectInfo tab, assign the ArcFM Segment Split autoupdater to the On Feature Create event
On the ObjectInfo tab, assign the following autoupdaters (in the order listed) to the On Feature Update event:
-
ArcFM Connect Network Feature
-
ArcFM Segment Split