Troubleshooting: CU Tag Filters Created in an SDE Do Not Function as Expected

When a user creates CU Tag filters, ArcFM builds two tables to support the feature: Cu_MM_CUTF_FilterName and MM_CUTF_FilterName (where FilterName is the unique name the user gives the created CU Tag filter). The Cu_MM_CUTF_FilterName table is a many-to-many relationship table. ArcCatalog in ArcGIS 10 will not assign privileges to many-to-many tables. Consequently, you must use your database console (Microsoft SQL Server Management Studio, Oracle SQL Plus, or similar) to assign correct privileges to the Cu_MM_CUTF_FilterName table for created CU Tag filters to function properly.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?