Assign Autoupdaters
Assign autoupdaters to the following classes via their Object info tab in the ArcFM Properties Manager.
Busbar, PriOHElectricLineSegment, PriUGElectricLineSegment,
SecOHElectricLineSegment, SecUGElectricLineSegment
The following autoupdaters should be assigned to all linear feature classes that conduct electricity, i.e., all edge feature classes in the geometric network.
The ArcFM Feeder Cache Maintenance Autoupdater section contains more information about this unique AU.
|
Event |
Autoupdater |
|
On Feature Create |
ArcFM Generic Electric Trace Weight |
|
On Feature Create |
ArcFM Feeder Cache Maintenance (assigned automatically when you enable FM 2.0) |
|
On Feature Update |
ArcFM Generic Electric Trace Weight |
|
On Feature Update |
ArcFM Feeder Subsource Level |
|
On Feature Update |
ArcFM Feeder Cache Maintenance (assigned automatically when you enable FM 2.0) |
|
On Feature Delete |
ArcFM Feeder Subsource Level |
|
On Feature Delete |
ArcFM Feeder Cache Maintenance (assigned automatically when you enable FM 2.0) |
CircuitSource, CircuitSourceID
|
Event |
Autoupdater |
|
On Feature Update |
ArcFM Internal FeederID Update |
DynamicProtectiveDevice, Fuse, Switch, OpenPoint, PrimaryMeter
The following autoupdaters should be assigned to any junction class that can have subsource features. Be sure that for each event, the following autoupdaters are assigned in the order listed.
The ArcFM Feeder Cache Maintenance Autoupdater section contains more information about this unique AU.
|
Event |
Autoupdater |
|
On Feature Create |
ArcFM Generic Electric Trace Weight |
|
On Feature Create |
ArcFM Feeder Subsource Relator |
|
On Feature Create |
ArcFM Feeder Subsource Name |
|
On Feature Create |
ArcFM Feeder Subsource Level |
|
On Feature Create |
ArcFM Feeder Internal FeederID Create |
|
On Feature Create |
ArcFM Feeder Cache Maintenance (assigned automatically when you enable FM 2.0) |
|
On Feature Update |
ArcFM Generic Electric Trace Weight |
|
On Feature Update |
ArcFM Feeder Subsource Relator |
|
On Feature Update |
ArcFM Feeder Subsource Name |
|
On Feature Update |
ArcFM Feeder Subsource Level |
|
On Feature Update |
ArcFM Feeder Internal FeederID Update |
|
On Feature Update |
ArcFM Feeder Cache Maintenance (assigned automatically when you enable FM 2.0) |
|
On Feature Delete |
ArcFM Delete Feeder Object |
|
On Feature Delete |
ArcFM Feeder Cache Maintenance (assigned automatically when you enable FM 2.0) |
DynamicProtDev_CircuitSource relationship class
|
Event |
Autoupdater |
|
On Relationship Created |
ArcFM Feeder Cache Maintenance (assigned automatically) |
|
On Relationship Deleted |
ArcFM Feeder Cache Maintenance (assigned automatically) |
The ArcFM Feeder Cache Maintenance Autoupdater section contains more information about this unique AU.
Transformer, ServicePoint
The following autoupdaters should be assigned to any junction class that has a phase designation and/or is switchable, but is not configured to have subsource features.
|
Event |
Autoupdater |
|
On Feature Create |
ArcFM Generic Electric Trace Weight |
|
On Feature Update |
ArcFM Generic Electric Trace Weight |
ArcFM Feeder Cache Maintenance Autoupdater
The Feeder Cache Maintenance Autoupdater is assigned to events on each feature class in the geometric network. It is also assigned to events on the CircuitSource and Subsource tables, as well as the relationship class that joins the circuit source feature class (e.g. DynProtDevice) to the CircuitSource table.
The assignments associated with the Feeder Cache Maintenance AU are described below so you know that to expect when examining Autoupdater assignments to the listed feature class and event types
All feature classes in the geometric network, including the default junction feature class:
-
On Feature Create
-
On Feature Update
-
On Feature Delete
All edge feature classes in the electric geometric network:
-
Before Feature Split
-
On Feature Split ( required for simple edge feature classes)
-
After Feature Split
The CircuitSource table:
-
On Feature Update
The Subsource table (commonly named CircuitSourceID):
-
On Feature Update
The relationship class that joins the circuit source feature class (e.g. DynProtDev) to the CircuitSource table:
-
On Relationship Created
-
On Relationship Deleted