Conductors (primary and secondary)
Object Model names: SPLITTARGET
ELECTRICNETWORKEDGE: You must assign this model name to any edge features in your electric network that will participate in the ArcFM Electric Next Upstream Protective Device and Isolation Protective Device traces.
FEEDERSECONDARY: Assign this model name if you want secondary conductors downstream of a transformer to inherit the transformer's LowSideVoltage or OperatingVoltage value.
Field Model names:
|
Field |
Field Model Name |
Properties |
|---|---|---|
|
FeederID |
FEEDERID |
Field Info Tab: Reset After Create = Yes |
|
FeederID2 |
FEEDERID2 |
Field Info Tab: Reset After Create = Yes |
|
FeederInfo |
FEEDERINFO |
Field Info Tab: Editable = No Reset After Create = Yes |
|
ElectricTraceWeight |
MMELECTRICTRACEWEIGHT |
Field Info Tab: Reset After Create = Yes |
|
OperatingVoltage |
OPERATINGVOLTAGE |
|
|
PhaseDesignation |
PHASEDESIGNATION |
|
|
Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID or ParentCircuitSourceGUID field should exist on every feature class that participates in the multi-tiered network. |
||
|
ParentCircuitSourceGUID |
PARENTCIRCUITSOURCGUID |
Field Info Tab: Visible = Yes Editable = No Reset After Create = Yes |
|
Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager. |
||
|
ParentCircuitSourceID |
PARENTCIRCUITSOURCEID |
Field Info Tab: Visible = Yes Editable = No< Reset After Create = Yes |
|
FacilityID |
FACILITYID |
Field Info Tab: Visible = Yes Editable = Yes Reset After Create = No |
Things to ensure for correct behavior:
-
FdrMgrNonTraceable is not set on features that you want to be traced
-
If you wish feeder manager to respect conductor phasing then a phase designation field is required for the edge, and the field must be driven by the phase designation domain (see previous step for instructions on setting up this domain)
-
Feeder Manager uses the voltage levels to determine continuity of phases when tracing though a transformer feature.