Upgrade Workflow Manager to 9.0.1 SP1

Use these upgrade instructions if you are:

  • Using a version of Workflow Manager older than 9.0.1 SP1

  • Upgrading to a version of Workflow Manager that is 9.0.1 SP1 or higher

These instructions are intended for GIS administrators who currently are in production with Workflow Manager and who want to upgrade to the most recent release of the ArcFM Solution. This document does not apply if you are not currently using Workflow Manager and will be implementing it with the most recent version of the ArcFM Solution (i.e., you are new to ArcFM and are starting with the most recent release). If this is the case, refer to Set Up Workflow Manager.

If you are upgrading your Process Framework, you may also need to use the Process Framework Database Upgrade tool.

Upgrade to 9.0.1 SP1

The following change should be made to the Workflow Manager database (e.g., WorkflowManager.mdb) on the Enterprise server. If you are using Mobile Designer, this change should also be made on the field Workflow Manager database (e.g., Field WorkflowManager.mdb).

Tasks

You will need to create the following task using the Process Framework Administration Tool. The Task Name must appear exactly as shown in bold below.

  • Save Design

    Node Type: design

    Transition: (None)

    Assign Subtasks: (in order as shown)

    • Save Design

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?