Service Point
Object Model names: FdrMgrLoadPoint
Note for Responder Users: The FdrMgrLoadPoint model name may be assigned differently depending on your data model. Refer to the Responder documentation for information about assigning this model name. It is strongly recommended that you assign this model name during the initial Feeder Manager configuration to avoid the need to re-initialize trace weights during Responder configuration.
Note for All Other Users: The FdrMgrLoadPoint model name is required for load point counting (counting affected customers) in ArcFM Mobile. It is strongly recommended that you assign it during the initial Feeder Manager configuration to avoid the need to re-initialize trace weights at a later time.
Field Model names:
|
Field |
Field Model Name |
Properties |
|---|---|---|
|
FeederID |
FeederID |
Field Info Tab: Reset After Create = Yes |
|
FeederID2 |
FeederID2 |
Field Info Tab: Reset After Create = Yes |
|
FeederInfo |
FeederInfo |
Field Info Tab: Editable = No Reset After Create = Yes |
|
ElectricTraceWeight |
MMElectricTraceWeight |
Field Info Tab: Reset After Create = Yes |
|
PhaseDesignation |
PhaseDesignation |
|
|
ServiceCurrentRating |
ServiceCurrentRating |
|
|
Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network. |
||
|
ParentCircuitSourceGUID |
ParentCircuitSourceGUID |
Field Info Tab: Visible = Yes Editable = No Reset After Create = Yes |
|
Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager. |
||
|
ParentCircuitSourceID |
ParentCircuitSourceID |
Field Info Tab: Visible = Yes Editable = No Reset After Create = Yes |
|
FacilityID |
FacilityID |
Field Info Tab: Visible = Yes Editable = Yes Reset After Create = No |