Identify Feature Classes

Decide which feature classes to include in your network. Below are the feature classes we recommend you include in your geodatabase. These feature classes are from the Minerville sample geodatabase. You may use different feature class names and include additional feature classes. Throughout this documentation, we will refer to the feature classes as named below.

NOTE: You may change the names of the feature classes, but the model names assigned later must have the EXACT spelling. This is crucial to your geodatabase working properly.
TIP: Indexing the FeederID field will greatly increase performance.

FdrMgrNonTraceable

The FDRMGRNONTRACEABLE model name may be assigned to a feature class or to an attribute field. If it is assigned at the feature class level, the entire class will be omitted from Feeder Manager traces.

You may also create a Feeder Manager NonTraceable Indicator field to which the model name is assigned. Below is required data type and domain for this field. You may change the name of the field, but the FDRMGRNONTRACEABLE field model name assigned later must have the EXACT spelling.

Field

Data Type

Domain

Feeder Manager NonTraceable Indicator

long integer

FdrMgrNonTraceable

The user will be able to select Traceable or NonTraceable for individual features.

The Appendix contains a detailed explanation of the relationship between Bitgate fields and FDRMGRNONTRACEABLE.

Conductors

Conductors consist of primary and secondary wire as well as other current-carrying lines such as bus and transmission lines. These feature classes must participate in your geometric network as simple edges or complex edges. If you have edges in your network that you don't want Feeder Manager to trace (but want to trace them for other purposes--such as bus in a substation that is upstream of the circuit breaker), include these feature classes in your network and use the model name FDRMGRNONTRACEABLE as an object class model name or field model name to disable edge feature classes from the trace. If you want Feeder Manager to trace with respect to conductor phasing, you must create a PhaseDesignation field for the edge features in your network. The PhaseDesignation field should be assigned a domain.

Below is a list of required fields for this feature class. You may change the names of the fields, but the field model names assigned later must have the EXACT spelling. Ensure the domains are assigned as shown.

Field

Data Type

Domain

FeederID

long integer or string/text (same as Circuit Source)

 

FeederID2

long integer or string/text

 

FeederInfo

long integer (precision = 10)

 

ElectricTraceWeight

long integer (precision = 10)

 

PhaseDesignation

long integer

On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase.

OperatingVoltage

any data type, domain required

OperatingVoltage

FdrMgrNonTraceable (optional)

long integer or string/text

FdrMgrNonTraceable

Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID or ParentCircuitSourceGUID field should exist on every feature class that participates in the multi-tiered network.

ParentCircuitSourceID

long integer

Data type = 32-bit integer
Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceGUID

GUID

Default value = null

FacilityID

text (length=20)

Default value = null

Switchable Devices

Switches can interrupt the flow of electricity in a circuit. You can include non-mechanical open points in this category as well because a switch that is normally open appears the same to the tracing algorithms as an open point. Modeling an open point as a switch allows you to close it out in the field and reflect that change by changing the normal open status fields. You can have one or more feature classes that store switchable devices but each must be assigned the model name of SWITCH. In your model, the switch classes must be a simple junction, and must have fields assigned the following model names. If you want to use the out-of-the-box autoupdaters to maintain the trace weights, the fields carrying the NORMALPOSITION_A, NORMALPOSITION _B, or NORMALPOSITION _C model name should have a domain assigned.

Below is a list of required fields for this feature class. You may change the names of the fields, but the field model names assigned later must have the EXACT spelling. Ensure the domains are assigned as shown.

Field

Data Type

Domain

FeederID

long integer or string/text (same as Circuit Source)

 

FeederID2

long integer or string/text

 

FeederInfo

long integer (precision = 10)

 

ElectricTraceWeight

long integer (precision = 10)

 

PhaseDesignation

long integer

On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase.

NormalPosition_A

long integer

NormalStatus

NormalPosition_B

long integer

NormalStatus

NormalPosition_C

long integer

NormalStatus

Optional: The following fields are required only if you have a multi-tiered network. The ParentCircuitSourceID or Parent CircuitSourceGUID field should exist on every feature class that participates in the multi-tiered network. The CircuitSourceID and Subsource fields should be added to all junction classes eligible to represent subsidiary or ultimate sources.

ParentCircuitSourceID

long integer

Data type = 32-bit integer

Default value = null

Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceGUID

GUID

Default value = null

CircuitSourceID

long integer

Data type = 32-bit integer

Default value = null

Subsource

short integer

Yes/No domain

Data type = 16-bit integer

Default value = null

FacilityID

text (length=20)

Default value = null

Protective Devices

Protective Devices provide overcurrent protection and can interrupt the flow of electricity in a circuit. You can have one or more feature classes that represent protective devices but each must be assigned the model name of FDRMGRPROTECTIVE to designate it as a member of this category. Please note that Feeder Manager makes no distinction between the categories of Switchable and Protective Devices. The autoupdaters provided with Feeder Manager use the FDRMGRPROTECTIVE model name to maintain the value in the trace weight field. The design of Feeder Manager anticipates that future applications (especially outage management) will need to determine from the trace weight alone whether a device is protective or not, i.e., whether it is designed to open automatically in response to a fault. Assign a domain to the fields with model names NORMALPOSITION_A, NORMALPOSITION _B, and NORMALPOSITION_C.

Below is a list of required fields for this feature class. You may change the names of the fields, but the field model names assigned later must have the EXACT spelling. Ensure the domains are assigned as shown.

Field

Data Type

Domain

FeederID

long integer or string/text (same as Circuit Source)

 

FeederID2

long integer or string/text

 

FeederInfo

long integer (precision = 10)

 

ElectricTraceWeight

long integer (precision = 10)

 

PhaseDesignation

long integer

On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase.

NormalPosition_A

long integer

NormalStatus

NormalPosition_B

long integer

NormalStatus

NormalPosition_C

long integer

NormalStatus

Optional: The following fields are required only if you have a multi-tiered network. The ParentCircuitSourceID or ParentCircuitSourceGUID field should exist on every feature class that participates in the multi-tiered network. The CircuitSourceID and Subsource fields should be added to all junction classes eligible to represent subsidiary or ultimate sources.

ParentCircuitSourceID

long integer

Data type = 32-bit integer

Default value = null

  Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceGUID 

GUID

Default value = null

CircuitSourceID

long integer

Data type = 32-bit integer

Default value = null

Subsource

short integer

Yes/No domain

Data type = 16-bit integer

Default value = null

FacilityID

text (length=20)

Default value = null

Transformers

Transformers are devices that transform the voltage level in a circuit. Transformers must be a junction feature class in your geometric network. You can include Step Transformers in this category as well. This feature class must be assigned the class model name of TRANSFORMER. The Phase Designation field should store the phase or phases that the transformer is tapping and have a domain assigned to it. This enables Feeder Manager to determine which phase of a three-phase conductor a single-phase transformer is tapping.

Below is a list of required fields for this feature class. You may change the names of the fields, but the field model names assigned later must have the EXACT spelling. Ensure the domains are assigned as shown.

Field

Data Type

Domain

FeederID

long integer or string/text (same as Circuit Source)

 

FeederID2

long integer or string/text

 

FeederInfo

long integer (precision = 10)

 

ElectricTraceWeight

long integer (precision = 10)

 

PhaseDesignation

long integer

On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase.

Optional: Create the following field if you want to display the Total RatedkVA for an electric trace. This functionality also requires the TransformerUnit object class.

RatedkVA

Long integer

Transformer Unit kVA

Optional: Create the following field if you want secondary conductors downstream of a transformer to inherit the transformer's LowSideVoltage value. If this value doesn't exist (and the functionality is configured), the downstream secondary conductors inherit the OperatingVoltage value from the transformer.

LowSideVoltage

long integer

 

Optional: The following fields are required only if you have a multi-tiered network. The ParentCircuitSourceID or ParentCircuitSourceGUID field should exist on every feature class that participates in the multi-tiered network. The CircuitSourceID and Subsource fields should be added to all junction classes eligible to represent subsidiary or ultimate sources.

ParentCircuitSourceID

long integer

Data type = 32-bit integer

Default value = null

      Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceGUID 

GUID

Default value = null

CircuitSourceID

long integer

Data type = 32-bit integer

Default value = null

Subsource

short integer

Yes/No domain

Data type = 16-bit integer

Default value = null

FacilityID

text (length=20)

Default value = null

Optional:

The following object class is required ONLY if you are using a multi-tiered network and Extended Feeder Manager.

CircuitSourceID Object Class

This table stores data about the multi-tiered network.

Field

Data Type

Domain

FeederLevel

Long integer

 

FeederName

text (length=48)

 

ObjectID

Object ID

 

ParentCircuitSourceID

Long integer

No domain

Data type = 32-bit integer

Default value = null

    Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager.

ParentCircuitSourceGUID

GUID

Default value = null

RelatedFeatureClassName

text (length=48)

 

RelatedObjectID

long integer

 

Optional:

The following object class is required if you wish to view the Total RatedkVA for an electric trace. This object may have additional fields in your geodatabase. The RatedKVA field is the only one necessary to display RatedKVA for an electric trace. This functionality also requires a field on the Transformer feature class.

TransformerUnit Object Class

Field

Data Type

Domain

RatedkVA

Long integer

Transformer Unit KVA

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?