Troubleshooting: Should SDE own the Extended Data tables?

The owner of the geodatabase feature/object classes is typically the owner of the Extended Data Definition (EDD) tables. It is critical that the permissions for the EDD tables are consistent with those of the feature/object classes. It isn’t required that SDE be the owner, as long as they are consistent.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?