Upgrade Session Manager to 9.1.2
Use these upgrade instructions if you are:
-
Using a version of Session Manager older than 9.1.2
-
Upgrading to a version of Session Manager that is 9.1.2 or higher
These instructions are intended for GIS administrators who currently are in production with a previous version of Session Manager and who want to upgrade to the most recent version of the ArcFM Solution. This document does not apply if you are not currently using Session Manager and will be implementing it with the latest release of ArcFM (i.e., you are new to ArcFM and are starting with the current release). If this is the case, refer to Set Up Session Manager.
If you are upgrading your Process Framework, you may also need to use the Process Framework Database Upgrade tool.
Upgrade to 9.1.2
With release 9.1.2, changes were made to support enhanced Mobile functionality. The following task is necessary only if you wish to use ArcFM Solution's Mobile functionality.
New Tasks
You will need to create the following task using the Process Framework Administration Tool. The Task Name must appear exactly as shown in bold below.
The following task should be added to the Session Manager database.
-
Send Session to Field
Database: enterprise
Node Type: session
Assign Subtasks: (in order as shown)
-
Is Mobile Solution Enabled?
-
Change Session Owner to Mobile
-
Create Packet
-
Send Session to Field
-
Update Tasks
The following task should already exist in the Session Manager databases. It requires the updates shown in red. If you have added custom subtasks, your task will look different.
-
Open Redline Session
Database: field, enterprise
Node Type: session
Add Subtasks Shown in Red: (in order as shown)
-
Open Graphic Session
-
Append Sketch Layers
-
Set Active Graphics Layer
-
Note: If you have assigned custom subtasks to this task, add the new subtasks to the end.