Busbars
Object Model names: SPLITTARGET
ELECTRICNETWORKEDGE: You must assign this model name to any edge features in your electric network that will participate in the ArcFM Electric Next Upstream Protective Device and Isolation Protective Device traces.
Field Model names:
|
Field |
Field Model Name |
Properties |
|---|---|---|
|
FeederID |
FEEDERID |
Field Info Tab: Reset After Create = Yes |
|
FeederID2 |
FEEDERID2 |
Field Info Tab: Reset After Create = Yes |
|
FeederInfo |
FEEDERINFO |
Field Info Tab: Editable = No Reset After Create = Yes |
|
FdrMgrNonTraceable |
FDRMGRNONTRACEABLE |
|
|
ElectricTraceWeight |
MMELECTRICTRACEWEIGHT |
Field Info Tab: Reset After Create = Yes |
|
OperatingVoltage |
OPERATINGVOLTAGE |
|
|
PhaseDesignation |
PHASEDESIGNATION |
|
|
Optional: The following field is required only if you have a multi-tiered network. The ParentCircuitSourceID field should exist on every feature class that participates in the multi-tiered network. |
||
|
ParentCircuitSourceGUID |
PARENTCIRCUITSOURCEGUID |
Field Info Tab: Visible = Yes Editable = No Reset After Create = Yes |
|
Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager. |
||
|
ParentCircuitSourceID |
PARENTCIRCUITSOURCEID |
Field Info Tab: Visible = Yes Editable = No Reset After Create = Yes |
|
FacilityID |
FACILITYID |
Field Info Tab: Visible = Yes Editable = Yes Reset After Create = No |