Upgrade Session Manager to 8.3.1
Use these upgrade instructions if you are:
-
Using a version of Session Manager older than 8.3.1
-
Upgrading to a version of Session Manager that is 8.3.1 or higher
These instructions are intended for GIS administrators who currently are in production with a previous version of Session Manager and who want to upgrade to the most recent version of the ArcFM Solution. This document does not apply if you are not currently using Session Manager and will be implementing it with the latest release of ArcFM (i.e., you are new to ArcFM and are starting with the current release). If this is the case, refer to Set Up Session Manager.
If you are upgrading your Process Framework, you may also need to use the Process Framework Database Upgrade tool.
Upgrade to 8.3.1
With release 8.3.1, the tools included with ArcFM’s Session Manager were retrofitted to use the new Task/Subtask architecture provided with the Process Framework. Since the tools now depend on new tasks, they will be disabled if the tasks do not exist. All tools in Session Manager are affected by this change.
You will need to create the following tasks using the Process Framework Administration Tool. The Task Name must appear exactly as shown in bold below.
-
Open Session
Node Type: Session
Assign Subtasks: (in order as shown)
-
Open Session
-
-
Save Session
Node Type: Session
Assign Subtasks: (in order as shown)
-
Does user own session node?
-
Save Session
-
-
Close Session
Node Type: Session
Assign Subtasks: (in order as shown)
-
Close Session
-
Switch To Parent Version
-
-
Submit Session
Node Type: Session
Assign Subtasks: (in order as shown)
-
Does user own session node?
-
Submit Session
Mobile Note: If you're setting up this task for use in the field with Mobile, use the Mobile Submit Session subtask instead of the Submit Session subtask.
-
-
Change Session Owner
Node Type: Session
Assign Subtasks: (in order as shown)
-
Change Session Owner
-
-
Reject Session
Node Type: Session
Assign Subtasks: (in order as shown)
-
Does user own session node?
-
Reject Session
-
-
Delete Session
Node Type: Session
Assign Subtasks: (in order as shown)
-
Does user own session node?
-
Delete Session
-
-
Reconcile Session
Node Type: Session
Assign Subtasks: (in order as shown)
-
Does user own session node?
-
Reconcile Session
-
-
Post Session
Node Type: Session
Assign Subtasks: (in order as shown)
-
Does user own session node?
-
Post Session
-
-
Unlock Session
This task is optional.
Node Type: Session
Assign Subtasks: (in order as shown)
-
Unlock Node
-
-
Create Session
The Create Session task must be created for each filter node in your database.
Node Type: AllSessionsFilter, UserSessionsFilter, UserStatusSessionsFilter, and any other custom filters
Assign Subtasks: (in order as shown)
-
Create Session
-