Configure Water Tracing
The steps for configuring water tracing assume that you are configuring a new geodatabase. If you are adding water tracing functionality to an existing geodatabase, you may be able to skip some steps such as creating domains and adding model names to them. However, you may want to ensure all of the domains and water model names have been added before continuing to the next step.
Before performing the steps below, ensure your database contains the ArcFM Solution System Tables. If not, you will need to create them.
STEP 1: Create Domains
STEP 2: Configure Domains for Cathodic Protection Systems
STEP 3: Create Feature Classes
STEP 4: Add Model Names to Domains
STEP 5: Add Fields
STEP 6: Assign Model Names
STEP 7: Initialize Water Trace Weights
STEP 8: Build Geometric Network
STEP 9: Assign Autoupdaters
STEP 10: Configure Cathodic Protection Systems
STEP 11: Convert to ArcFM Objects
STEP 12: Export XML
The Appendix also includes information about how Water Tracing works.