CircuitSourceID Object Class
Optional:
The following object class is required ONLY if you are using a multi-tiered network and Extended Feeder Manager.
CircuitSourceID Object Class
Object Model names: CIRCUITSOURCEID
Field Model names:
|
Field |
Field Model Name |
|---|---|
|
FeederLevel |
FEEDERLEVEL |
|
FeederName |
FEEDERNAME |
|
ObjectID |
CIRCUITSOURCEID |
|
ParentCircuitSourceGUID |
PARENTCIRCUITSOURCEGUID |
|
Add either ParentCircuitSourceGUID or ParentCircuitSourceID, but not both. If both are added, the feature will not work with the manager. |
|
|
ParentCircuitSourceID |
PARENTCIRCUITSOURCEID |
|
RelatedFeatureClassName |
RELATEDFEATURECLASSNAME |
|
RelatedObjectID |
RELATEDOBJECTID |