Analyze Asset Data

Data visualization is a powerful way to show the monetized risk, criticality index, and health index of installed assets. Administrators can configure asset models at the asset category level to create and modify asset models based on data availability and other requirements.

When asset category parameters are configured, it makes the health calculation for maintenance and replacement more valuable. Administrators can now configure:

  • Interventions

  • Generic parameters

  • Duty Factor

  • Location Factor

  • Measured Condition Factor

  • Observed Condition Factor

  • Reliability Factor

  • Safety Consequence of Failure

  • Environmental Consequence of Failure

  • Financial Consequence of Failure

  • Network Performance Consequence of Failure

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?