Single Line Diagram

This feature offers users a way to visualize assets in a diagram layout. This functionality is particularly valuable for visualizing and analyzing asset relationships within an electrical substation, structure, or building. The drawing follows a color and shape schema that represents the associated risk levels and asset types.

A SVG file can be uploaded so that the layout of the assets is seen, similar to a geographic map view.

The assets in the drawing behave the same as assets in a map. Click an asset and the details are seen in the new window.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?