Asset Details

The map and single line diagram (SLD) view gives you the ability to search for a specific asset, or group of assets, according to the desired filter, and enables access to its details and related information. When you click on a specific asset, a window opens at the right of the screen showing a short asset summary.

If more information is required, click to see a more detail view of the desired asset.

In the window that opens, the asset detailed page shows configured widgets of information. Different asset categories and types show different information. All assets show the health and risk indexes based on the accessible data. Here are some examples:

  • A concrete pole only shows the location map.

  • A UPS shows charts with component aging and an operations counter.

  • An oil distribution transformer shows dissolved gas analysis, component aging, and peak load.

  • A dry transformer shows temperature sensor readings and health charts.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?