Visualize Spatial Assets

When you assess the monetized risk of assets, it can be helpful to see the overall layout of specific geographic areas. These areas include physical locations on a GIS map and diagrams of complex structures that contain assets. This is where the Map and Single Line Diagram view is helpful. When you use the Global Filters, you can see at a glance the risk calculation of resource groups in a color-coded layout.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?