Map

From the main menu, click Map and gain access to detailed information about clusters of geographical assets. The average risk level and number of assets is easily seen for each cluster when looking over the selected area. The risk levels are coded by color: 1(green), 2(yellow), 3(red), 4 (dark blue).

Example: The red circle with a 9, represents a cluster of 9 assets with an average risk level of 3.

The main window is divided into two sections:

  • Global filters — The main add filter options are configured by the administrator. Some examples include Installation Date, Risk Index, Health Index, Number of customers, and Asset Category.

  • Map View — Asset locations are seen based on an interactive geographical layout.

    Users can zoom to different points on the map, select different geographic regions, directly click on an asset, or see the map from the satellite view.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?