Main Application Window

Upon successful login, the main application window opens. This window is divided into three sections:

  • Application Header — user can see the number and list of current Alerts, Manage account, see the Privacy notice, and Logout.

  • Application Menu – provides access to all application options.

  • Application main area – shows information from the selected workspace, by default, and then as each menu tab is clicked.

    NOTE: Each workspace home page can be configured with different widgets. One example is the Recent work widget. It collects a list of links to the last dashboards you edited. See more takes you to the Dashboards page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?