NVE58348-02

Installation of Supports

Introduction

The cast resin busbar trunking system must be attached using the supporting structures of the building, for example, wall beams or stands, the system-specific supports, threaded rods, and C-profiles.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?