NVE58348-02

Ceiling, Wall, and Floor Support Attachment

Mounting the Supports on the Ceiling

Follow these rules to mount the supports on the ceiling:

Ceiling mounting examples: suspended installation

1 Threaded rods suspension

2 C-profiles

3 Anchor bolts

  • Check that the ceiling and the supports are strong enough to hold the weight of the system.

  • Attach the supports to the ceiling.

  • The C-profile can be used for horizontal element installation, element in widthwise or edgewise position.

The mounting set consists of the following components:

  • Two threaded rods M10 for connecting the C-profile.

  • Two C-profiles.

  • Four lock nuts with securing washers

Elements with supports attached

Mounting the Wall Supports

Follow these rules to attach the wall supports:

Fixed wall supports (left). The elements must be installed on the wall supports using terminal clamps (right).

  • A wall support consists of a wall beam and a set of terminal clamps. The wall beams must be provided by the customer, if they have not been designed, confirmed and ordered separately from Schneider Electric

  • Attach the suspension support (wall beam) to the wall or another suitable structural support.

  • You must insert additional transverse stays when implementing fixed point supports.

Examples of wall supports.

  • The figures on the left show examples of wall supports. You must check that the minimum distances indicated in the figures are implemented.

Mounting the Floor Supports

Example of a floor mounted element: elevated installation

  • The rules for mounting the floor supports are the same as those for the ceiling and wall supports.

  • The figure on the left shows an example of a floor support installation, with the minimum dimensions that must be used during installation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.