NVE58348-02

KR / KT Adapter

The Canalis KR / KT Adapter

Canalis KR is made of copper or aluminum conductors encapsulated in epoxy resin IP68.

Canalis KT is made of copper or aluminum conductors isolated by polyester films and protected by a metallic enclosure IP55.

The KR / KT adapters enable the interconnection of the two systems. Both ranges, including adapters, are certified under the IEC 61439-1/6 standard.

The KR/KT adapter

The KR / KT adapter in use.

The design of the PE conductor is different in Canalis KR and in Canalis KT. For this reason, carefully select the correct reference as shown in the table below:

NOTE: The KR / KT adapter is not provided with Canalis KR and must be ordered separately with Canalis KT products.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.