NVE58348-02

Establishing and Testing the Electrical Connection

Safety Instructions

Preparing the Elements for Connection

Distance between busbar elements to enable proper connection

  • The distance between the conductor ends of two cast resin busbar elements (junction) should be 30 +/- 5 mm.

  • The cast resin busbar elements to be connected must be aligned and level.

The ends of the elements must be cleaned and dried

  • Clean the conductor ends with a polishing fleece and dry them with an industrial drier before inserting the junction block if:

    • The elements have been stored for long.

    • The conductor-end protective packing is damaged.

    • The conductors have become contaminated, wet, or corroded.

  • Check the insulation resistance of each element. The insulation resistance must be ≥ 1 MΩ.

Establishing the Electrical Connection

Inserting the junction block between two elements

  • Insert the junction block between the copper or aluminum conductors from above or below. Align it such that it extends equally on all sides.

  • If necessary, gently knock the junction block into place using a rubber hammer.

Tightening the connections between the junction block and the elements

  • When the junction block is aligned, tighten the connecting bolt. Tighten to 54 N.m using a torque wrench for junction blocks with bolt size 17 mm or to 84 N.m for junction blocks with bolt size 19 mm.

Testing the Electrical Connection

After connecting a subsection (maximum of 6 elements), carry out the following tests:

  • Insulation testing: Using a megohmmeter, check the insulation resistance between each phase or neutral1 and earth (the casing, if it is connected to earth). According to IEC 60364-6 (and 61.3.3) standard, the insulation values must be:

    • Rated voltage < 500 V Utest DC = 500 V Ri ≥ 1 MΩ.

    • Rated voltage > 500 V Utest DC = 1000 V Ri ≥ 1 MΩ.

  • PE protective circuit equipotential (According to ref: IEC 61439-1): Using an ohmmeter, check the PE protective circuit continuity by visual inspection and random continuity testing.

1: No neutral insulation if the neutral is connected to or used as the earth.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.