NVE58348-02

Storage of Hardware and Chemical Components

Storage Area for Chemicals and Equipment

You must ensure that the material storage area meets the following requirements:

  • It must be stable and level.

  • It must be protected against extreme temperature, water penetration, and dampness.

  • It must be protected against fire, dust, water, direct sunlight, and welding sparks.

  • It must not serve as a gangway or be used to assemble other equipment.

General Rules for Storage of Equipment and Chemicals

Stacking (top) and storage (bottom) of elements

Storage of equipment

  • It is recommended to store the material in the original transport packing.

  • Up to 2 pallets of straight elements can be stacked on top of each other.

  • The elements of the double system (aluminium conductor with more than 2500 A and copper conductor with more than 3200 A) are better stored flat on top of each other

  • Secure elements with a strap retainer.

  • Other elements like end-feed units, form parts, boxes, frames, cable connections and so on, should not be stacked.

Storage of chemicals

Storage of chemicals

  • The cast resin, hardener, and demoulding agent must not be stored below 5 °C, or above 35 °C.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?