NVE58348-02

Cast Resin

Rules For Working With Cast Resin

You must follow these rules while working with cast resin:

  • Check that the resin is clear and liquid. Do not use the resin if it is milky or crystallized.

  • Check the best-before date on the label. If it is out of date, order fresh resin. Never exceed the permissible best-before date.

  • Check that the filler material/sand is dry.

Handling and Safety Precautions

You must observe these precautions while handling the resin and other chemicals:

  • Ventilate the work site well.

  • Do not eat, drink, or smoke at the work site.

  • Use protective goggles, gloves and overalls.

  • Avoid inhaling any vapor or fumes. Wear a safety mask to prevent accidental inhalation.

  • Apply protective cream over unprotected areas of skin to avoid sensitization.

  • In the event of unintentional spillage, clean with inert absorbent material (sand) and store the contaminated material in a suitable container before disposal.

  • Filled containers of resin and hardener must be incinerated or stored according to local regulations.

  • Wash your hands with warm water and soap after work.

Material Safety Data Sheets

The material safety data sheets for the chemical products are listed here:

  • Aqua Release 1026S, Safety data sheet.

  • BKS1, Safety data sheet.

  • BKS2, Safety data sheet.

  • Quartz Sand, Safety data sheet.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.