NVE58348-02

Expansion Unit

Mounting the Expansion Unit

CAUTION
HAZARD OF IMPROPER INSTALLATION
  • Do not install supports in the expansion areas.
  • Do not attach the expansion elements to the supports, as this results in the temperature-dependent expansion of the run not fully compensated.
  • Attach one support in front of the expansion area and one behind it to ensure that the element is fixed correctly. Two support points are provided for each expansion unit.
  • Do not remove the screws without having first installed the two elements adjoining the expansion unit in their final position.
Failure to follow these instructions can result in injury or equipment damage.

Follow these instructions for mounting the expansion unit.

Step

Action

1

Before mounting, ensure that the expansion unit is blocked by the screws marked in red (delivery condition).

2

Install the expansion unit in the same way as any other cast resin busbar trunking system element in the position indicated in the installation drawing. Follow the assembly instructions for connecting elements.

3

Place the expansion unit on tow beams.

4

Without releasing the expansion unit, install the following busbar trunking system element and attach it in to the corresponding flanges.

Mounting the expansion unit.

Releasing the Expansion Unit

Remove the screws from the expansion unit to enable it to move freely.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.