NVE58348-02

Reception and Handling

Scope of Delivery

All materials are packaged and sent with a delivery note, a packing list, and short installation instructions.

Receiving the Goods

After the goods are received, do the following:

  1. Take note of the information symbols and labels on the packaging. Pay attention to safety labels.

  2. Check that the documentation and material correspond with your installation project.

  3. Make sure that the material is in proper condition and without transport damage.

  4. Make sure that all components are supplied and they function as intended and indicated in the documentation.

  5. The item number on the packaging, the element number on the elements and the project manual helps you to identify where the parts/elements have to be installed in the layout.

Proper Handling of Materials

The cast resin busbar is a piece of electrical equipment and should be handled with care by following the instructions below.

Keep the boxes in an upright position at all times. Do not stack more than two pallets.

Lifting with forklift trucks:

  • For proper loading and unloading of containers, the forklift must be able to lift a minimum of 4.5 tons.

  • To lift the pallets properly at the narrow side (0.8 m), the forklift must have a minimum fork length of 2 m.

  • Use rubber covers on the fork so that it does not scratch the surface of elements.

  • Ensure that the elements do not get damaged when you transport them with a forklift.

Lifting the elements with slings

  • Use fabric slings to suspend the cast resin busbar elements.

  • Always use straps with double noose to lift the elements. Ensure that the straps can handle the weight.

  • Ensure that the lifting slings are wrapped around all the conductors, as shown in the figure on the left.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.