NVE58348-02

Connection to Switchboards and Transformers

Feed Units

These are of two types: type ER and type EL

  • Type ER feed units allow the busbar trunking to be connected to a switchboard busbar, or to the terminals of an oil-immersed transformer or generator.

  • Type EL feed units allow optimal connection to the busbar trunking.

These units can be connected:

  • Either directly to the busbar.

  • By flexible bars and connection plates.

  • By braids.

  • By cables.

Feed units can either be standard or made to measure. Consult the Canalis KR Catalogue for more information about feed units.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.