NVE58348-02

Supports for Vertical Installation on Walls

Mounting the Supports for Vertical Installations

Follow these rules for mounting vertical supports

Mounting the spring support ZA6 on the floor

  • Vertical runs must be supported by dedicated supports supplied by Schneider Electric

  • Depending on the building configuration, supports can be mounted on the floor or on the wall.

  • Supports must be mounted at distances of 3 m (maximum).

  • The first support of the run must be a fixed point, others must be with springs.

  • Intermediary guides can be used to avoid lateral displacements.

Mounting a fixed-point support ZA7 on the wall

  • Mount all supports in the corresponding locations before installing the cast resin busbar trunking system.

  • Mark the anchorage holes on the wall, using the support as a template.

  • Use the appropriate anchor bolts for the weight to be supported.

  • Extract the mounting studs held by nuts that hold the cast resin busbar trunking system.

Mounting a fixed-point support ZA8 on the floor.

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?