IO Module Registers
Introduction
This section describes the IO module registers.
Registers 13824 to 15719 are held by the IO 1.
Registers 16824 to 18719 are held by the IO 2:
-
The registers of the parameters of IO 2 are equal to the registers of the parameters of IO 1 plus 3000.
Example:
-
Register 14599 holds the digital input status register of the IO 1.
-
Register 17599 holds the digital input status register of the IO 2.
-
-
The order of the registers is the same as that of the IO 1.
-
The characteristics (access type, size, range, and unit) are the same as those of the registers of IO 1.
-
Registers 15360 to 16109 containing the predefined application are specific to the IO 1 because they hold the predefined applications.