Schematics With ComPact NSX Circuit Breakers
General Description
Depending on the type of circuit breaker used, the user must connect the IFM interface using one of the following configurations:
-
Connection of the IFM interface to the MicroLogic trip unit.
-
Connection of the IFM interface to the BSCM module.
-
Connection of the IFM interface to the BSCM module or the MicroLogic trip unit.
For more information, refer to the ULP System User Guide.
ULP Connection
NOTICE |
---|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All the connection configurations require the NSX cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac.