DOCA0091EN-08

Analog Inputs

Analog Input Register Mapping

The following table describes the analog inputs and corresponding registers and addresses of the IO module.

IO Module

Analog Input Addresses

Analog Input Registers

IO 1

0x35FF–0x3668

13824–13929

IO 2

0x41B7–0x4220

16824–16929

Analog Input Registers of IO 1

The order and the description of the analog input registers of IO 2 are the same as those of IO 1.

Address

Register

RW

Unit

Type

Range

Description

0x35FF–0x3600

13824–13825

Reserved

0x3601–0x3602

13826–13827

R

°C

FLOAT32

-50–250

Analog input sensor Pt100 temperature value (updated once every 1 s)

0x3603

13828

R

INT16U

0–1

Data quality of the analog input

  • 0 = Valid

  • 1 = Invalid

0x3604

13829

Reserved

0x3605–0x3608

13830–13833

R

DATETIME

Timestamp of the last change of +/- 1 °C of the analog data value

0x3609–0x360C

13834–13837

Reserved

0x360D–0x360E

13838–13839

R

°C

FLOAT32

-50–250

Analog input Pt100 maximum value

0x360F–0x3610

13840–13841

R

°C

FLOAT32

-50–250

Analog input Pt100 minimum value

0x3611–0x3614

13842–13845

R

DATETIME

Timestamp of minimum value of analog input value recorded

0x3615–0x3618

13846–13849

R

DATETIME

Timestamp of maximum value of analog input value recorded

0x3619–0x361C

13850–13853

R

DATETIME

Timestamp of last reset of min/max values of analog input value recorded

0x361D–0x361E

13854–13855

R

INT32U

0–65534

Switchboard temperature threshold 1 counter

This counter increments every time threshold 1 is exceeded.

0x361F–0x3620

13856–13857

R

INT32U

0–65534

Switchboard temperature threshold 2 counter

This counter increments every time threshold 2 is exceeded.

0x3621–0x3622

13858–13859

R

INT32U

0–65534

Switchboard temperature threshold 3 counter

This counter increments every time threshold 3 is exceeded.

0x3623–0x363A

13860–13883

R

OCTET STRING

Analog input identification coded over 45 ASCII characters(1)

0x363B

13884

R

INT16U

0–2

Analog input type(1)

  • 0 = Analog input is not valid (factory setting)

  • 1 = Not applicable

  • 2 = Pt100

0x363C

13885

Reserved

0x363D–0x363E

13886–13887

R

°C

FLOAT32

-50–250

Switchboard temperature threshold 1 pick-up value (Pt100) (1)

Factory setting = 50 °C

0x363F–0x3640

13888–13889

R

s

FLOAT32

1–3600

Switchboard temperature threshold 1 pick-up time delay (Pt100)(1)

Factory setting = 10 s

0x3641–0x3642

13890–13891

R

°C

FLOAT32

-50–250

Switchboard temperature threshold 1 drop-out value (Pt100)(1)

Factory setting = 45 °C

0x3643–0x3644

13892–13893

R

s

FLOAT32

1–3600

Switchboard temperature threshold 1 drop-out time delay (Pt100)(1)

Factory setting = 10 s

0x3645–0x3646

13894–13895

R

°C

FLOAT32

-50–250

Switchboard temperature threshold 2 pick-up value (Pt100)(1)

Factory setting = 60 °C

0x3647–0x3648

13896–13897

R

s

FLOAT32

1–3600

Switchboard temperature threshold 2 pick-up time delay (Pt100)(1)

Factory setting = 10 s

0x3649–0x364A

13898–13899

R

°C

FLOAT32

-50–250

Switchboard temperature threshold 2 drop-out value (Pt100)(1)

Factory setting = 55 °C

0x364B–0x364C

13900–13901

R

s

FLOAT32

1–3600

Switchboard temperature threshold 2 drop-out time delay (Pt100)(1)

Factory setting = 10 s

0x364D–0x364E

13902–13903

R

°C

FLOAT32

-50–250

Switchboard temperature threshold 3 pick-up value (Pt100)(1)

Factory setting = 70 °C

0x364F–0x3650

13904–13905

R

s

FLOAT32

1–3600

Switchboard temperature threshold 3 pick-up time delay (Pt100)(1)

Factory setting = 10 s

0x3651–0x3652

13906–13907

R

°C

FLOAT32

-50–250

Switchboard temperature threshold 3 drop-out value (Pt100)(1)

Factory setting = 65 °C

0x3653–0x3654

13908–13909

R

s

FLOAT32

1–3600

Switchboard temperature threshold 3 drop-out time delay (Pt100)(1)

Factory setting = 10 s

0x3655–0x3656

13910–13911

R

Ω

FLOAT32

200–650

Motor temperature sensor fault threshold

0x3657–0x3668

13912–13929

Reserved

(1) Value set using the EcoStruxure Power Commission software.