List of BSCM Module Commands and Error Codes
List of Commands
The following table lists the available BSCM module commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly Executing a Command.
|
Command |
Command code |
User profile |
|---|---|---|
|
Open circuit breaker Open Circuit Breaker |
904 |
Administrator or Operator |
|
Close circuit breaker Close Circuit Breaker |
905 |
Administrator or Operator |
|
Reset circuit breaker Reset Circuit Breaker |
906 |
Administrator or Operator |
|
Enable/Inhibit close order Enable/Inhibit a Circuit Breaker Close Order |
910 |
Administrator or Operator |
|
Enable/disable automatic reset Enable/Disable Automatic Reset |
42636 |
Administrator |
|
Enable/disable reset even if SDE Enable/Disable Reset even if SDE |
42637 |
Administrator |
|
Preset counters Preset Counters |
42638 |
Administrator |
|
Set up thresholds Set Up Thresholds |
42639 |
Administrator |
Error Codes
In addition to generic error codes Result of the Command, the BSCM module commands generate the following error codes returned in register 8021:
|
Error Code |
Description |
|---|---|
|
4363 (0x110B) |
BSCM module is out of order. |
|
4503 (0x1197) |
Circuit breaker is tripped. It must be reset before the command. |
|
4504 (0x1198) |
Circuit breaker is already closed. |
|
4505 (0x1199) |
Circuit breaker is already open. |
|
4506 (0x119A) |
Circuit breaker is already reset. |
|
4507 (0x119B) |
Actuator is in manual mode. Remote commands are not allowed. |
|
4508 (0x119C) |
Actuator is not present. |
|
4510 (0x119E) |
A previous command is still in progress. |
|
4511 (0x119F) |
Reset command is forbidden when SDE is set. |
|
4512 (0x11A0) |
Inhibit close order is enabled. |
Any other positive error code means an internal error.