DOCA0091EN-08

Communication Test

Introduction

The use of the EcoStruxure Power Commission software is recommended to test the serial line communication on the various circuit breakers.

If the laptop or PC installed with the EcoStruxure Power Commission software and connected on the Modbus network is able to read data from the IMU, the communication is established. Refer to the EcoStruxure Power Commission Online Help.