Schematics with ComPact NSX Circuit Breakers
General Description
Depending on the configuration of the ComPact NSX circuit breaker, connect the IFE interface to the circuit breaker using one of the following configurations:
-
Connection of the IFE interface to the MicroLogic trip unit
-
Connection of the IFE interface to the BSCM module
-
Connection of the IFE interface to the BSCM module and to the MicroLogic trip unit
For more information, refer to the ULP System User Guide.
ULP Connection
NOTICE |
---|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All connection configurations require the NSX cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac.