DOCA0091EN-08

Application Commands

Preset Cradle/Drawer Counters

The cradle/drawer counter values can be read from the cradle management registers.

To preset the cradle or drawer counters, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41352

Command code = 41352

0x1F40

8001

INT16U

16

Number of parameters (bytes) = 16

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

0–65535

Connected counter reset/preset:

  • 0–65534 = preset value of the connected counter

  • 65535 (0xFFFF) = do not preset the connected counter

0x1F46

8007

INT16U

0–65535

Disconnected counter reset/preset:

  • 0–65534 = preset value of the disconnected counter

  • 65535 (0xFFFF) = do not preset the disconnected counter

0x1F47

8008

INT16U

0–65535

Test counter reset/preset:

  • 0–65534 = preset value of the test counter

  • 65535 (0xFFFF) = do not preset the test counter

Preset Regrease Timers

To preset regrease timers, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41353

Command code = 41353

0x1F40

8001

INT16U

18

Number of parameters (bytes) = 18

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45–0x1F46

8006–8007

INT16U

Operating time since last grease maintenance

  • 0–157766400 = preset value of regrease timer counter

  • 4294967295 (0xFFFFFFFF) = No preset

0x1F47–0x1F48

8008–8009

 

INT32U

Operating time since last move in rack in position (delay from last disconnection)

  • 0–28944000 = preset value of remove timer

  • 4294967295 (0xFFFFFFFF) = No preset

Light Control

The light command status can be read from the light control registers.

To control the light, set the command registers in the following way:

Address

Register

Unit

Type

Range

Bit

Description

0x1F3F

8000

INT16U

42120

Command code = 42120

0x1F40

8001

INT16U

13

Number of parameters (bytes) = 13

0x1F41

8002

INT16U

Destination = IO 1: 8193 (0x2001)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

MSB: State

0

  • 0 = Light OFF

  • 1 = Light ON

1

  • 0 = without time delay

  • 1 = with time delay

LSB = Timer (MSB)

1–54000 seconds (if bit 1 in set state)

Any value 0-0xffff (if bit 1 in reset state)

0x1F46

8007

INT16U

MSB = Timer (LSB)

1 to 54000 seconds (if bit 1 is in set state)

Any value 0-0xffff (if bit 1 is in reset state)

LSB = 0 (not used)

Load Control

The load command status can be read from the load control registers.

To control the load, set the command registers in the following way:

Address

Register

Unit

Type

Range

Bit

Description

0x1F3F

8000

INT16U

42376

Command code = 42376

0x1F40

8001

INT16U

13

Number of parameters (bytes) = 13

0x1F41

8002

INT16U

Destination = IO 1: 8193 (0x2001)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

MSB: State

0

  • 0 = Load OFF

  • 1= Load ON

1

  • 0 = without time delay

  • 1= with time delay

LSB = Timer (MSB)

1–54000 seconds (if bit 1 in set state)

Any value 0-0xffff (if bit 1 in reset state)

0x1F46

8007

INT16U

MSB = Timer (LSB)

1–54000 seconds (if bit 1 in set state)

Any value 0-0xffff (if bit 1 in reset state)

LSB = 0 (not used)

Preset Input Pulse Counters

To preset pulse counters, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

42888

Command code = 42888

0x1F40

8001

INT16U

34

Number of parameters (bytes) = 34

NOTE: The number of parameters corresponds to the number of bytes of the 17 registers 8001–8015 and 8022–8023. The bytes of the registers 8016–8021 are not counted as command parameters.

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45–

0x1F46

8006–

8007

INT32U

0–4294967295

I1 pulse counter reset/preset:

  • 0–4294967294 = preset value of the I1 pulse counter

  • 4294967295 (0xFFFFFFFF) = do not preset the I1 pulse counter

0x1F47–

0x1F48

8008–

8009

INT32U

0–4294967295

I2 pulse counter reset/preset:

  • 0–4294967294 = preset value of the I2 pulse counter

  • 4294967295 (0xFFFFFFFF) = do not preset the I2 pulse counter

0x1F49–

0x1F4A

8010–

8011

INT32U

0–4294967295

I3 pulse counter reset/preset:

  • 0–4294967294 = preset value of the I3 pulse counter

  • 4294967295 (0xFFFFFFFF) = do not preset the I3 pulse counter

0x1F4B–

0x1F4C

8012–

8013

INT32U

0–4294967295

I4 pulse counter reset/preset:

  • 0–4294967294 = preset value of the I4 pulse counter

  • 4294967295 (0xFFFFFFFF) = do not preset the I4 pulse counter

0x1F4D–

0x1F4E

8014–

8015

INT32U

0–4294967295

I5 pulse counter reset/preset:

  • 0–4294967294 = preset value of the I5 pulse counter

  • 4294967295 (0xFFFFFFFF) = do not preset the I5 pulse counter

0x1F4F

8016

Must be set to 0 (factory setting).

0x1F50

8017

Must be set to 8019 (factory setting).

0x1F51

8018

Must be set to 8020 (factory setting).

0x1F52

8019

Must be set to 8021 (factory setting).

0x1F53

8020

Must be set to 0.

0x1F54

8021

Must be set to 0.

0x1F55–

0x1F56

8022–

8023

INT32U

0–4294967295

I6 pulse counter reset/preset:

  • 0–4294967294 = preset value of the I6 pulse counter

  • 4294967295 (0xFFFFFFFF) = do not preset the I6 pulse counter

Preset Switchboard Temperature Threshold Counters

To preset switchboard temperature threshold counters, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

42889

Command code = 42889

0x1F40

8001

INT16U

16

Number of parameters (bytes) = 16

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

0–65535

Switchboard temperature threshold 1 counter reset/preset:

  • 0–65534 = preset value of the switchboard temperature threshold 1 counter

  • 65535 (0xFFFF) = do not preset the counter

0x1F46

8007

INT16U

0–65535

Switchboard temperature threshold 2 counter reset/preset:

  • 0–65534 = preset value of the switchboard temperature threshold 2 counter

  • 65535 (0xFFFF) = do not preset the counter

0x1F47

8008

INT16U

0–65535

Switchboard temperature threshold 3 counter reset/preset:

  • 0–65534 = preset value of the switchboard temperature threshold 3 counter

  • 65535 (0xFFFF) = do not preset the counter