About the Book
Document Scope
The aim of this guide is to provide users, installers, and maintenance personnel with the technical information needed to operate the Modbus protocol on:
-
ComPact™ NSX 100-630 circuit breakers and switch-disconnectors.
-
ComPact™ NSX 100-1200 DC circuit breakers and switch-disconnectors.
Validity Note
This document is valid for:
-
ComPact™ NSX 100-630 circuit breakers and switch-disconnectors
-
with the BSCM circuit breaker status control module and with the communicating motor mechanism, and/or
-
with MicroLogic™ 5, 6, or 7 trip unit.
-
-
ComPact™ NSX 100-1200 DC circuit breakers and switch-disconnectors with the BSCM circuit breaker status control module and with the communicating motor mechanism;
and connected
-
either to an RS485 serial line Modbus network using an IFM Modbus-SL interface for one circuit breaker
-
or to an Ethernet network using an IFE Ethernet interface for one circuit breaker or an IFE Ethernet switchboard server.
This document describes the registers and commands available for the IMU modules with the following firmware version
IMU module |
Part number |
Firmware version |
---|---|---|
MicroLogic 5 and 6 trip units |
– |
≥ V001.003.000 |
MicroLogic 7 trip unit |
– |
≥ V002.001.001 |
IO module |
LV434063 |
≥ V003.004.005 |
IFM interface |
LV434000 |
≥ V003.001.012 |
IFE Ethernet interface |
LV434001 |
≥ V004.007.000 |
LV434010 |
||
IFE Server |
LV434002 |
≥ V003.016.000 |
LV434011 |
Online Information
The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download.
The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric home page at www.se.com.
Related Documents
Title of Documentation |
Reference Number |
---|---|
ComPact NSX Circuit Breakers and Switch-Disconnectors - User Guide |
|
ComPact NSX MicroLogic 5/6/7 Trip Units - User Guide |
|
ComPact NSX DC Circuit Breakers and Switch-Disconnectors - User Guide |
|
ULP (Universal Logic Plug) System - User Guide |
|
Enerlin’X IO Input/Output Application Module for One Circuit Breaker - User Guide |
|
Enerlin’X IFE - Ethernet Switchboard Server - User Guide |
|
Enerlin’X IFE - Ethernet Interface for One Circuit Breaker - User Guide |
|
Enerlin’X IO Input/Output Application Module for One Circuit Breaker - Instruction Sheet |
|
Enerlin’X IFE - Ethernet Interface / Ethernet Server - Instruction Sheet |
|
Enerlin’X IFM - Modbus-SL Interface for One Circuit Breaker - Instruction Sheet |
You can download these technical publications and other technical information from our website at https://www.se.com/en/download.